Cluster Commands: Messaging#

This group describes the CLI commands for the Messaging cluster. Listed below is a description of the cluster: This cluster provides an interface for passing text messages between SE devices.

Macros#

#define

zcl msg disp [messageId:4] [messageControl:1] [startTime:4] [durationInMinutes:2] [message:-1] [optionalExtendedMessageControl:1]

#define

zcl msg cancel [messageId:4] [messageControl:1]

#define

zcl msg disp-protd [messageId:4] [messageControl:1] [startTime:4] [durationInMinutes:2] [message:-1] [optionalExtendedMessageControl:1]

#define

zcl msg x-all [implementationDateTime:4]

#define

zcl msg confirm [messageId:4] [confirmationTime:4] [messageConfirmationControl:1] [messageResponse:-1]

#define

zcl msg get-msg-x [earliestImplementationTime:4]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_DISP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_DISP

zcl msg disp [messageId:4] [messageControl:1] [startTime:4] [durationInMinutes:2] [message:-1] [optionalExtendedMessageControl:1]

  • Command description for DisplayMessage

    • messageId - INT32U

    • messageControl - MessagingControlMask [BITMAP8]

    • startTime - UTC_TIME

    • durationInMinutes - INT16U

    • message - CHAR_STRING

    • optionalExtendedMessageControl - MessagingExtendedControlMask [BITMAP8]


Definition at line 9265 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_CANCEL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_CANCEL

zcl msg cancel [messageId:4] [messageControl:1]

  • The CancelMessage command provides the ability to cancel the sending or acceptance of previously sent messages.

    • messageId - INT32U

    • messageControl - MessagingControlMask [BITMAP8]


Definition at line 9272 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_DISP_PROTD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_DISP_PROTD

zcl msg disp-protd [messageId:4] [messageControl:1] [startTime:4] [durationInMinutes:2] [message:-1] [optionalExtendedMessageControl:1]

  • The DisplayProtected Message command is for use with messages that are protected by a password or PIN.

    • messageId - INT32U

    • messageControl - MessagingControlMask [BITMAP8]

    • startTime - UTC_TIME

    • durationInMinutes - INT16U

    • message - CHAR_STRING

    • optionalExtendedMessageControl - MessagingExtendedControlMask [BITMAP8]


Definition at line 9283 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_X_ALL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_X_ALL

zcl msg x-all [implementationDateTime:4]

  • The CancelAllMessages command indicates to a client device that it should cancel all display messages currently held by it.

    • implementationDateTime - UTC_TIME


Definition at line 9289 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_GET#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_GET

zcl msg get

  • Command description for GetLastMessage


Definition at line 9294 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_CONFIRM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_CONFIRM

zcl msg confirm [messageId:4] [confirmationTime:4] [messageConfirmationControl:1] [messageResponse:-1]

  • The Message Confirmation command provides an indication that a Utility Customer has acknowledged and/or accepted the contents of a previously sent message. Enhanced Message Confirmation commands shall contain an answer of 'NO', 'YES' and/or a message confirmation string.

    • messageId - INT32U

    • confirmationTime - UTC_TIME

    • messageConfirmationControl - BITMAP8

    • messageResponse - OCTET_STRING


Definition at line 9303 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_GET_MSG_X#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_MESSAGING_GET_MSG_X

zcl msg get-msg-x [earliestImplementationTime:4]

  • This command initiates the return of the first (and maybe only) Cancel All Messages command held on the associated server, and which has an implementation time equal to or later than the value indicated in the payload.

    • earliestImplementationTime - UTC_TIME


Definition at line 9309 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc