Plugin Commands: Messaging Server#
The messaging-server plugin contributes CLI commands to the application framework to be used for manipulating messages in a server context.
Macros#
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_APPEND
plugin messaging-server append [message:-1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CANCEL
plugin messaging-server cancel [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_NOT
plugin messaging-server confirm not
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_CONFIRM_REQ
plugin messaging-server confirm req
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_DISPLAY
plugin messaging-server display [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_ID
plugin messaging-server id [messageId:4]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_CRITICAL
plugin messaging-server importance critical
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_HIGH
plugin messaging-server importance high
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_LOW
plugin messaging-server importance low
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_IMPORTANCE_MEDIUM
plugin messaging-server importance medium
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_INVALID
plugin messaging-server invalid [endpoint:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_MESSAGE
plugin messaging-server message [message:-1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_PRINT
plugin messaging-server print [endpoint:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_RELATIVE_TIME
plugin messaging-server relative-time [time:4] [duration:4]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TIME
plugin messaging-server time [time:4] [duration:2]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_BOTH
plugin messaging-server transmission both
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_IPAN
plugin messaging-server transmission ipan
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_TRANSMISSION_NORMAL
plugin messaging-server transmission normal
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_SERVER_PLUGIN_MESSAGING_SERVER_VALID
plugin messaging-server valid [endpoint:1]