Plugin Commands: Throughput Legacy#
The throughput commands allow you to test your application's network throughput by measuring how many packets are able to be sent.
Macros#
#define
plugin throughput duration [Time:4]
#define
plugin throughput end
#define
plugin throughput inflight [Count:1]
#define
plugin throughput result
#define
plugin throughput start
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_DURATION#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_DURATION
plugin throughput duration [Time:4]
Set the duration in ms for the test.
Time - INT32U - Duration in ms
Definition at line
6963
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_END#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_END
plugin throughput end
Abort the test while running.
Definition at line
6968
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_INFLIGHT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_INFLIGHT
plugin throughput inflight [Count:1]
Set the number of packets in flight during the test.
Count - INT8U - Number of packets
Definition at line
6974
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_RESULT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_RESULT
plugin throughput result
Show the results of the last test.
Definition at line
6979
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_THROUGHPUT_LEGACY_PLUGIN_THROUGHPUT_START
plugin throughput start
Start the throughput test.
Definition at line
6984
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc