Plugin Commands: Concentrator#
The Concentrator plugin contributes several CLI commands to the application framework for controlling the sending of MTORRs.
Macros#
plugin concentrator agg
plugin concentrator print-table
plugin concentrator set-router-behavior [behavior:1]
plugin concentrator start
plugin concentrator status
plugin concentrator stop
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_AGG
plugin concentrator agg
(Requires Concentrator Support to be enabled on this device.) Schedules a ZigBee PRO Many To One Route Request (MTORR) to be sent out at next opportunity, which will cause aggregation (many-to-one) routes to be created towards this concentrator.
2199
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_PRINT_TABLE
plugin concentrator print-table
Print the SOC/NCP source route table.
2204
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_SET_ROUTER_BEHAVIOR
plugin concentrator set-router-behavior [behavior:1]
This command allows the user to set the router behavior for this plugin. The argument values come from concentrator-support.h in the enum with members starting with EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_.
behavior - INT8U - The value of a EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_ enum member.
2210
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_START
plugin concentrator start
Starts the periodic broadcast of MTORRs
2215
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STATUS
plugin concentrator status
Prints current status and configured parameters of the concentrator
2220
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONCENTRATOR_PLUGIN_CONCENTRATOR_STOP
plugin concentrator stop
Stops the periodic broadcast of MTORRs
2225
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc