Plugin Commands: Mac address filtering#
Commands to manipulate the MAC address filtering tables.
Macros#
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_CLEAR_STATS
plugin mac-address-filtering clear-stats
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_ADD
plugin mac-address-filtering long-address-list add [eui64:8]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_CLEAR
plugin mac-address-filtering long-address-list clear
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_DELETE
plugin mac-address-filtering long-address-list delete [index:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_SET_BLACKLIST
plugin mac-address-filtering long-address-list set-blacklist
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_SET_WHITELIST
plugin mac-address-filtering long-address-list set-whitelist
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_ADD
plugin mac-address-filtering pan-id-list add [pan-id:2]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_CLEAR
plugin mac-address-filtering pan-id-list clear
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_DELETE
plugin mac-address-filtering pan-id-list delete [index:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_SET_BLACKLIST
plugin mac-address-filtering pan-id-list set-blacklist
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_SET_WHITELIST
plugin mac-address-filtering pan-id-list set-whitelist
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PRINT_CONFIG
plugin mac-address-filtering print-config
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_RESET
plugin mac-address-filtering reset
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SET_CONFIG_NO_ADDRESS_FILTER
plugin mac-address-filtering set-config no-address-filter [enable:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_ADD
plugin mac-address-filtering short-address-list add [node-id:2]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_CLEAR
plugin mac-address-filtering short-address-list clear
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_DELETE
plugin mac-address-filtering short-address-list delete [index:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_SET_BLACKLIST
plugin mac-address-filtering short-address-list set-blacklist
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_SET_WHITELIST
plugin mac-address-filtering short-address-list set-whitelist