Plugin Commands: Messaging Client#

The messaging-client plugin contributes CLI commands to the application framework to be used for manipulating messages in a client context.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_CLEAR

plugin messaging-client clear [endpoint:1]

  • Clear the message.

    • endpoint - INT8U - The relevant endpoint.


Definition at line 4044 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_CONFIRM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_CONFIRM

plugin messaging-client confirm [endpoint:1]

  • Send the message confirmation.

    • endpoint - INT8U - The relevant endpoint.


Definition at line 4050 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MESSAGING_CLIENT_PLUGIN_MESSAGING_CLIENT_PRINT

plugin messaging-client print [endpoint:1]

  • Print the message info.

    • endpoint - INT8U - The relevant endpoint.


Definition at line 4056 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc