Cluster Commands: Identify#
This group describes the CLI commands for the Identify cluster. Listed below is a description of the cluster: Attributes and commands for putting a device into Identification mode (e.g. flashing a light).
Macros#
zcl identify off [endpoint:1]
zcl identify on [endpoint:1] [time:2]
zcl identify id [identifyTime:2]
zcl identify query
zcl identify ez-mode [action:1]
zcl identify trigger [effectId:1] [effectVariant:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF
zcl identify off [endpoint:1]
Writes the IdentifyTime attribute
endpoint - INT8U - The endpoint on which to stop identifying
1060
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON
zcl identify on [endpoint:1] [time:2]
Writes the IdentifyTime attribute
endpoint - INT8U - The endpoint on the device which should begin identifying
time - INT16U - The number of seconds to spend identifying
1067
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID
zcl identify id [identifyTime:2]
Command description for Identify
identifyTime - INT16U
9098
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY
zcl identify query
Command description for IdentifyQuery
9103
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE
zcl identify ez-mode [action:1]
Invoke EZMode on an Identify Server
action - BITMAP8
9109
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER
zcl identify trigger [effectId:1] [effectVariant:1]
Command description for TriggerEffect
effectId - IdentifyEffectIdentifier [ENUM8]
effectVariant - IdentifyEffectVariant [ENUM8] See Also
9119
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc