Plugin Commands: Relay Control Server#
The relay control plugin provides the functionality to enable or disable the stack's relay capabilities, and also to view the relay state.
Macros#
plugin relay-control-server get [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
plugin relay-control-server set [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [isEnabled:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_GET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_GET
plugin relay-control-server get [nodeId:2] [srcEndpoint:1] [dstEndpoint:1]
Get the relay state
nodeId - INT16U - the destination node id
srcEndpoint - INT8U - the source endpoint
dstEndpoint - INT8U - the destination endpoint
5895
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_RELAY_CONTROL_SERVER_PLUGIN_RELAY_CONTROL_SERVER_SET
plugin relay-control-server set [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [isEnabled:1]
Set the relay state
nodeId - INT16U - the destination node id
srcEndpoint - INT8U - the source endpoint
dstEndpoint - INT8U - the destination endpoint
isEnabled - INT8U - state value to be set
5904
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc