Plugin Commands: Partner Link Key Exchange#

The partner link key exchange plugin contributes CLI commands to the application framework to be used for controlling facets of link key exchanges among partners.

Macros#

#define
#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER

plugin partner-link-key-exchange allow-partner [allowPartner:1]

  • Set the allow partner flag within the device for Certificate Based Key Exchange

    • allowPartner - INT8U - Boolean value to allow or disallow partner based key exchange


Definition at line 4789 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER

plugin partner-link-key-exchange partner [nodeId:2] [endpoint:1]

  • Initiate partner link key exchange.

    • nodeId - INT16U - The 2 byte short address of the node

    • endpoint - INT8U - The endpoint of the device with whom ot start cbke.


Definition at line 4796 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc