Plugin Commands: Sleepy Message Queue#
The sleepy-message-queue plugin provides a means to store packets up to a specified period of time.
Macros#
plugin sleepy-message-queue getNumMsg [dstEui64:-1]
plugin sleepy-message-queue getPendingMsg [msgId:1]
plugin sleepy-message-queue getPendingMsgId [dstEui64:-1]
plugin sleepy-message-queue init
plugin sleepy-message-queue remainTime [msgId:1]
plugin sleepy-message-queue remove [msgId:1]
plugin sleepy-message-queue removeAll [dstEui64:-1]
plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]
plugin sleepy-message-queue timestamp
plugin sleepy-message-queue unusedCnt
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG
plugin sleepy-message-queue getNumMsg [dstEui64:-1]
Get the number of pending messages for a given destination EUI64.
dstEui64 - OCTET_STRING - The EUI64 of the device for which the number of pending messages is being queried
6211
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG
plugin sleepy-message-queue getPendingMsg [msgId:1]
Get the first pending message ID for a given destination EUI64.
msgId - INT8U - The messageID of the message to be retrieved.
6217
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID
plugin sleepy-message-queue getPendingMsgId [dstEui64:-1]
Get the first pending message ID for a given destination EUI64.
dstEui64 - OCTET_STRING - The EUI64 of the device for which the first pending message ID is being queried
6223
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT
plugin sleepy-message-queue init
Initialize the sleepy message queue.
6228
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME
plugin sleepy-message-queue remainTime [msgId:1]
Report the remaining timeout on the message specified by the message ID.
msgId - INT8U - The messageID of the message whose remaining time will be reported.
6234
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE
plugin sleepy-message-queue remove [msgId:1]
Remove the message from the queue with the given messageID.
msgId - INT8U - The messageID of the message to be removed.
6240
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL
plugin sleepy-message-queue removeAll [dstEui64:-1]
Remove all messages from the queue with the given EUI64.
dstEui64 - OCTET_STRING - The EUI64 of the device whose messages should be removed.
6246
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE
plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]
Store a message into the sleepy message queue.
timeoutSec - INT32U - Message timeout, in seconds
payloadPtr - INT32U - Pointer to (address of) the message payload
payloadLength - INT16U - The length of the message payload
payloadId - INT16U - The payload ID of this message
dstEui64 - OCTET_STRING - The EUI64 of the device to which the message is being sent
6256
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP
plugin sleepy-message-queue timestamp
Retrieve the current value of halCommonGetInt32uMillisecondTick().
6261
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT
plugin sleepy-message-queue unusedCnt
Reads the number of unused queue entries.
6266
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc