Plugin Commands: Key Establishment#
The Key Establishment commands provide commands to initiate key establishment with a remote target.
Macros#
#define
plugin key-establishment interpan [panId:2] [eui64:-1]
#define
plugin key-establishment start [nodeId:2] [endpoint:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_INTERPAN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_INTERPAN
plugin key-establishment interpan [panId:2] [eui64:-1]
Initiate key establishment with the target device over interpan.
panId - INT16U - The PAN ID that the target is located on.
eui64 - OCTET_STRING - The target's EUI64 (big endian)
Definition at line
3753
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_KEY_ESTABLISHMENT_PLUGIN_KEY_ESTABLISHMENT_START
plugin key-establishment start [nodeId:2] [endpoint:1]
Initiates key establishment with the target node ID.
nodeId - INT16U - Target node ID.
endpoint - INT8U - Target node's endpoint.
Definition at line
3760
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc