Plugin Commands: Reporting#
The reporting plugin contributes several CLI commands to the application framework to be used in creating and managing reporting table entries directly on the device.
Macros#
plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]
plugin reporting clear
plugin reporting clear-last-report-time
plugin reporting print
plugin reporting remove [index:1]
plugin reporting test-timing
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD
plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]
Add a new entry to the report table.
endpoint - INT8U - The local endpoint from which the attribute is reported.
clusterId - INT16U - The cluster where the attribute is located.
attributeId - INT16U - The id of the attribute being reported.
mask - INT8U - 0 for client-side attributes or 1 for server-side attributes.
minInterval - INT16U - The minimum reporting interval, measured in seconds.
maxInterval - INT16U - The maximum reporting interval, measured in seconds.
reportableChange - INT32U - The minimum change to the attribute that will result in a report being sent.
5927
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR
plugin reporting clear
Clear all entries from the report table.
5932
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME
plugin reporting clear-last-report-time
Clear last report time of attributes.
5937
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT
plugin reporting print
Print the report table.
5942
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE
plugin reporting remove [index:1]
Remove an entry from the report table.
index - INT8U - The index of the report to be removed.
5948
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_TEST_TIMING#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_TEST_TIMING
plugin reporting test-timing
FOR TESTING PURPOSES - gather timing metrics for reporting table operations
5953
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc