Data Structures#
Here are the data structures with brief descriptions:
128-bit AES key | |
|---|---|
Bluetooth address | |
Variable-length int8_t array. Maximum length: 65535 | |
Data structure of the scan_request event | |
Data structure of the timeout event | |
Data structure of the closed event | |
Data structure of the get_remote_tx_power_completed event | |
Data structure of the opened event | |
Data structure of the parameters event | |
Data structure of the phy_status event | |
Data structure of the remote_tx_power event | |
Data structure of the remote_used_features event | |
Data structure of the rssi event | |
Data structure of the tx_power event | |
Data structure of the connection_iq_report event | |
Data structure of the connectionless_iq_report event | |
Data structure of the dtm_iq_report event | |
Data structure of the silabs_iq_report event | |
Data structure of the boot_failure event | |
Data structure of the boot event | |
Data structure of the characteristic event | |
Data structure of the characteristic_value event | |
Data structure of the descriptor event | |
Data structure of the descriptor_value event | |
Data structure of the mtu_exchanged event | |
Data structure of the procedure_completed event | |
Data structure of the attribute_value event | |
Data structure of the characteristic_status event | |
Data structure of the execute_write_completed event | |
Data structure of the indication_timeout event | |
Data structure of the user_read_request event | |
Data structure of the user_write_request event | |
Data structure of the service event | |
Data structure of the scan_report event | |
Data structure of the bonded event | |
Data structure of the bonding_failed event | |
Data structure of the confirm_bonding event | |
Data structure of the confirm_passkey event | |
Data structure of the list_bonding_entry event | |
Data structure of the passkey_display event | |
Data structure of the passkey_request event | |
Data structure of the closed event | |
Data structure of the data event | |
Data structure of the opened event | |
Data structure of the boot event | |
Data structure of the error event | |
Data structure of the external_signal event | |
Data structure of the hardware_error event | |
Data structure of the soft_timer event | |
Data structure of the dtm_completed event | |
Data structure of the message_to_host event | |
Data structure of BT API messages | |
... | |
16-bit UUID | |
64-bit UUID | |
Variable-length uint8_t array. Maximum length: 255 | |
128-bit UUID |