RMUEMLIB
Detailed Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Macros | |
#define | RMU_LockupResetDisable(A) RMU_ResetControl(rmuResetLockUp, A) |
Enumerations | |
enum | RMU_Reset_TypeDef { rmuResetWdog0 = _EMU_RSTCTRL_WDOG0RMODE_MASK, rmuResetWdog1 = _EMU_RSTCTRL_WDOG1RMODE_MASK, rmuResetSys = _EMU_RSTCTRL_SYSRMODE_MASK, rmuResetCoreLockup = _EMU_RSTCTRL_LOCKUPRMODE_MASK, rmuResetAVDD = _EMU_RSTCTRL_AVDDBODRMODE_MASK, rmuResetIOVDD0 = _EMU_RSTCTRL_IOVDD0BODRMODE_MASK, rmuResetDecouple = _EMU_RSTCTRL_DECBODRMODE_MASK } |
enum | RMU_ResetMode_TypeDef { rmuResetModeDisabled = 0, rmuResetModeEnabled = 1 } |
Functions | |
void | RMU_ResetCauseClear (void) |
Clear the reset cause register. | |
uint32_t | RMU_ResetCauseGet (void) |
Get the cause of the last reset. | |
void | RMU_ResetControl (RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) |
Disable/enable reset for various peripherals and signal sources. | |
Macro Definition Documentation
#define RMU_LockupResetDisable | ( | A | ) | RMU_ResetControl(rmuResetLockUp, A) |
RMU_LockupResetDisable kept for backwards compatibility.
Definition at line 132
of file em_rmu.h
.
Enumeration Type Documentation
enum RMU_Reset_TypeDef |
RMU controlled peripheral reset control and reset source control.
Definition at line 76
of file em_rmu.h
.
RMU reset modes.
Definition at line 60
of file em_rmu.h
.
Function Documentation
void RMU_ResetCauseClear | ( | void |
| ) |
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet().
Definition at line 274
of file em_rmu.c
.
References BUS_RegBitWrite(), EMU_Lock(), and EMU_Unlock().
Referenced by SLEEP_Init().
uint32_t RMU_ResetCauseGet | ( | void |
| ) |
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear(). This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Definition at line 317
of file em_rmu.c
.
Referenced by SLEEP_Init().
void RMU_ResetControl | ( | RMU_Reset_TypeDef | reset, |
RMU_ResetMode_TypeDef | mode |
||
) |
Disable/enable reset for various peripherals and signal sources.
- Parameters
-
[in] reset
Reset types to enable/disable.s [in] mode
Reset mode.
Definition at line 246
of file em_rmu.c
.
References BUS_RegBitWrite(), and SL_CTZ().