SE_Command_t Struct ReferenceEMLIB > SE
SE Command structure to which all commands to the SE must adhere.
Definition at line 325
of file em_se.h
.
#include <
em_se.h
>
Data Fields | |
uint32_t | command |
SE_DataTransfer_t * | data_in |
SE_DataTransfer_t * | data_out |
size_t | num_parameters |
uint32_t | parameters [SE_MAX_PARAMETERS] |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_se.h