EZRADIODRV_FieldLength Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin
EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.
Definition at line 69
of file ezradio_transmit_plugin.h
.
#include <
ezradio_transmit_plugin.h
>
Data Fields | |
uint8_t | f1 |
Field 1 length. | |
uint8_t | f2 |
Field 2 length. | |
uint8_t | f3 |
Field 3 length. | |
uint8_t | f4 |
Field 4 length. | |
uint8_t | f5 |
Field 5 length. | |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/
ezradio_transmit_plugin.h