MSC_EccConfig_TypeDef Struct ReferenceEMLIB > MSC
ECC configuration.
Definition at line 232
of file em_msc.h
.
#include <
em_msc.h
>
Data Fields | |
uint32_t | dmaChannels [2] |
bool | enableEccBank [MSC_ECC_BANKS] |
Field Documentation
uint32_t MSC_EccConfig_TypeDef::dmaChannels[2] |
Array of 2 DMA channel numbers to use for ECC initialization.
Definition at line 237
of file em_msc.h
.
Referenced by MSC_EccConfigSet().
bool MSC_EccConfig_TypeDef::enableEccBank[MSC_ECC_BANKS] |
Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.
Definition at line 233
of file em_msc.h
.
Referenced by MSC_EccConfigSet().
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_msc.h