BATTERY_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields for Battery (suited for Anim)

Definition at line 115 of file segmentlcd.c.

Data Fields

uint8_t bit [4]
 
uint8_t com [4]
 

Field Documentation

uint8_t BATTERY_TypeDef::bit[4]

LCD bit number

Definition at line 117 of file segmentlcd.c.

uint8_t BATTERY_TypeDef::com[4]

LCD COM line (for multiplexing)

Definition at line 116 of file segmentlcd.c.


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/segmentlcd.c