CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
Definition at line
549
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
| uint8_t | coreBiasAna |
| uint8_t | coreBiasStartup |
| CMU_HfxoCoreDegen_TypeDef | coreDegenAna |
| CMU_HfxoCtuneFixCap_TypeDef | ctuneFixAna |
| uint8_t | ctuneXiAna |
| uint8_t | ctuneXiStartup |
| uint8_t | ctuneXoAna |
| uint8_t | ctuneXoStartup |
| bool | disOnDemand |
| bool | enXiDcBiasAna |
| bool | forceEn |
| bool | forceXi2GndAna |
| bool | forceXo2GndAna |
| uint8_t | imCoreBiasStartup |
| CMU_HfxoOscMode_TypeDef | mode |
| bool | regLock |
| CMU_HfxoCbLsbTimeout_TypeDef | timeoutCbLsb |
| CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteady |
| CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteadyFirstLock |
Field Documentation
| uint8_t CMU_HFXOInit_TypeDef::coreBiasAna |
| uint8_t CMU_HFXOInit_TypeDef::coreBiasStartup |
| CMU_HfxoCoreDegen_TypeDef CMU_HFXOInit_TypeDef::coreDegenAna |
| CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna |
Fixed tuning capacitance on XI/XO.
Definition at line
558
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXiAna |
Tuning capacitance on XI.
Definition at line
560
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXiStartup |
XI pin startup tuning capacitance.
Definition at line
554
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXoAna |
Tuning capacitance on XO.
Definition at line
559
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXoStartup |
XO pin startup tuning capacitance.
Definition at line
553
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::disOnDemand |
Disable on-demand requests.
Definition at line
566
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::enXiDcBiasAna |
Enable XI internal DC bias.
Definition at line
562
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::forceEn |
| bool CMU_HFXOInit_TypeDef::forceXi2GndAna |
| bool CMU_HFXOInit_TypeDef::forceXo2GndAna |
| uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup |
Core bias intermediate startup current.
Definition at line
556
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| CMU_HfxoOscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
| bool CMU_HFXOInit_TypeDef::regLock |
| CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb |
| CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady |
Steady state timeout duration.
Definition at line
552
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock |
Steady state timeout duration for first lock.
Definition at line
551
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_cmu.h