NUMBER_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields numeric display.

Definition at line 91 of file segmentlcd.c .

Data Fields

uint8_t bit [7]
uint8_t com [7]

Field Documentation

uint8_t NUMBER_TypeDef::bit[7]

LCD bit number

Definition at line 93 of file segmentlcd.c .

uint8_t NUMBER_TypeDef::com[7]

LCD COM line (for multiplexing)

Definition at line 92 of file segmentlcd.c .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/ segmentlcd.c