IADC_InitSingle_t Struct ReferenceEMLIB > IADC
IADC single init structure
Definition at line 722
of file em_iadc.h
.
#include <
em_iadc.h
>
Data Fields | |
IADC_Alignment_t | alignment |
uint8_t | dataValidLevel |
bool | fifoDmaWakeup |
bool | showId |
bool | singleTailgate |
bool | start |
IADC_TriggerAction_t | triggerAction |
IADC_TriggerSel_t | triggerSelect |
Field Documentation
IADC_Alignment_t IADC_InitSingle_t::alignment |
Alignment of data in FIFO.
Definition at line 723
of file em_iadc.h
.
Referenced by IADC_initSingle().
uint8_t IADC_InitSingle_t::dataValidLevel |
Data valid level before requesting DMA transfer.
Definition at line 725
of file em_iadc.h
.
Referenced by IADC_initSingle().
bool IADC_InitSingle_t::fifoDmaWakeup |
Wake-up DMA when FIFO reaches data valid level.
Definition at line 726
of file em_iadc.h
.
Referenced by IADC_initSingle().
bool IADC_InitSingle_t::showId |
Tag FIFO entry with single indicator (0x20).
Definition at line 724
of file em_iadc.h
.
Referenced by IADC_initSingle().
bool IADC_InitSingle_t::singleTailgate |
If true, wait until end of SCAN queue before single queue warmup and conversion.
Definition at line 729
of file em_iadc.h
.
Referenced by IADC_initSingle().
bool IADC_InitSingle_t::start |
IADC_TriggerAction_t IADC_InitSingle_t::triggerAction |
IADC_TriggerSel_t IADC_InitSingle_t::triggerSelect |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_iadc.h