SYSTEM_CalAddrVal_TypeDef Struct ReferenceEMLIB > SYSTEM

DEVINFO calibration address/value pair.

Definition at line 293 of file em_system.h.

#include <em_system.h>

Data Fields

uint32_t address
 
uint32_t calValue
 

Field Documentation

uint32_t SYSTEM_CalAddrVal_TypeDef::address

Peripheral calibration register address.

Definition at line 294 of file em_system.h.

Referenced by SYSTEM_GetCalibrationValue().

uint32_t SYSTEM_CalAddrVal_TypeDef::calValue

Calibration value for register at address.

Definition at line 295 of file em_system.h.

Referenced by SYSTEM_GetCalibrationValue().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/em_system.h