Sample API functions for using USB.

Data Structures

struct USB_Setup_TypeDef
USB Setup request package.
struct USB_DeviceDescriptor_TypeDef
USB Device Descriptor.
struct USB_ConfigurationDescriptor_TypeDef
USB Configuration Descriptor.
struct USB_InterfaceDescriptor_TypeDef
USB Interface Descriptor.
struct USB_EndpointDescriptor_TypeDef
USB Endpoint Descriptor.
struct USB_StringDescriptor_TypeDef
USB String Descriptor.

Macros

#define USB_SETUP_DIR_OUT 0
#define USB_SETUP_DIR_IN 1
#define USB_SETUP_DIR_MASK 0x80
#define USB_SETUP_DIR_D2H 0x80
#define USB_SETUP_DIR_H2D 0x00
#define USB_SETUP_TYPE_STANDARD 0
#define USB_SETUP_TYPE_CLASS 1
#define USB_SETUP_TYPE_VENDOR 2
#define USB_SETUP_TYPE_STANDARD_MASK 0x00
#define USB_SETUP_TYPE_CLASS_MASK 0x20
#define USB_SETUP_TYPE_VENDOR_MASK 0x40
#define USB_SETUP_RECIPIENT_DEVICE 0
#define USB_SETUP_RECIPIENT_INTERFACE 1
#define USB_SETUP_RECIPIENT_ENDPOINT 2
#define USB_SETUP_RECIPIENT_OTHER 3
#define GET_STATUS 0
#define CLEAR_FEATURE 1
#define SET_FEATURE 3
#define SET_ADDRESS 5
#define GET_DESCRIPTOR 6
#define SET_DESCRIPTOR 7
#define GET_CONFIGURATION 8
#define SET_CONFIGURATION 9
#define GET_INTERFACE 10
#define SET_INTERFACE 11
#define SYNCH_FRAME 12
#define USB_HID_GET_REPORT 0x01
#define USB_HID_GET_IDLE 0x02
#define USB_HID_SET_REPORT 0x09
#define USB_HID_SET_IDLE 0x0A
#define USB_HID_SET_PROTOCOL 0x0B
#define USB_CDC_SETLINECODING 0x20
#define USB_CDC_GETLINECODING 0x21
#define USB_CDC_SETCTRLLINESTATE 0x22
#define USB_MSD_BOTRESET 0xFF
#define USB_MSD_GETMAXLUN 0xFE
#define USB_DEVICE_DESCRIPTOR 1
#define USB_CONFIG_DESCRIPTOR 2
#define USB_STRING_DESCRIPTOR 3
#define USB_INTERFACE_DESCRIPTOR 4
#define USB_ENDPOINT_DESCRIPTOR 5
#define USB_DEVICE_QUALIFIER_DESCRIPTOR 6
#define USB_OTHER_SPEED_CONFIG_DESCRIPTOR 7
#define USB_INTERFACE_POWER_DESCRIPTOR 8
#define USB_HUB_DESCRIPTOR 0x29
#define USB_HID_DESCRIPTOR 0x21
#define USB_HID_REPORT_DESCRIPTOR 0x22
#define USB_CS_INTERFACE_DESCRIPTOR 0x24
#define USB_DEVICE_DESCSIZE 18
#define USB_CONFIG_DESCSIZE 9
#define USB_INTERFACE_DESCSIZE 9
#define USB_ENDPOINT_DESCSIZE 7
#define USB_DEVICE_QUALIFIER_DESCSIZE 10
#define USB_OTHER_SPEED_CONFIG_DESCSIZE 9
#define USB_HID_DESCSIZE 9
#define USB_CDC_HEADER_FND_DESCSIZE 5
#define USB_CDC_CALLMNG_FND_DESCSIZE 5
#define USB_CDC_ACM_FND_DESCSIZE 4
#define USB_EP0_SIZE 8
#define USB_EP1_SIZE 8
#define USB_EP2_SIZE 8
#define USB_EP3_SIZE 64
#define USB_EP4_SIZE 32
#define USB_EP5_SIZE 64
#define USB_EP6_SIZE 512
#define USB_MAX_EP_SIZE 64
#define USB_EPTYPE_CTRL 0
#define USB_EPTYPE_ISOC 1
#define USB_EPTYPE_BULK 2
#define USB_EPTYPE_INTR 3
#define USB_EP_DIR_IN 0x80
#define USB_SETUP_PKT_SIZE 8
#define USB_EPNUM_MASK 0x0F
#define USB_LANGID_ENUS 0x0409
#define USB_MAX_DEVICE_ADDRESS 127
#define CONFIG_DESC_BM_REMOTEWAKEUP 0x20
#define CONFIG_DESC_BM_SELFPOWERED 0x40
#define CONFIG_DESC_BM_RESERVED_D7 0x80
#define CONFIG_DESC_BM_TRANSFERTYPE 0x03
#define CONFIG_DESC_MAXPOWER_mA (x)   (((x) + 1) / 2)
#define DEVICE_IS_SELFPOWERED 0x0001
#define REMOTE_WAKEUP_ENABLED 0x0002
#define USB_FEATURE_ENDPOINT_HALT 0
#define USB_FEATURE_DEVICE_REMOTE_WAKEUP 1
#define HUB_FEATURE_PORT_RESET 4
#define HUB_FEATURE_PORT_POWER 8
#define HUB_FEATURE_C_PORT_CONNECTION 16
#define HUB_FEATURE_C_PORT_RESET 20
#define HUB_FEATURE_PORT_INDICATOR 22
#define USB_CLASS_CDC 2
#define USB_CLASS_CDC_DATA 0x0A
#define USB_CLASS_CDC_ACM 2
#define USB_CLASS_CDC_HFN 0
#define USB_CLASS_CDC_CMNGFN 1
#define USB_CLASS_CDC_ACMFN 2
#define USB_CLASS_CDC_UNIONFN 6
#define USB_CLASS_HID 3
#define USB_CLASS_HID_KEYBOARD 1
#define USB_CLASS_HID_MOUSE 2
#define USB_CLASS_HUB 9
#define USB_CLASS_MSD 8
#define USB_CLASS_MSD_BOT_TRANSPORT 0x50
#define USB_CLASS_MSD_SCSI_CMDSET 6
#define USB_CLASS_MSD_CSW_CMDPASSED 0
#define USB_CLASS_MSD_CSW_CMDFAILED 1
#define USB_CLASS_MSD_CSW_PHASEERROR 2
#define PORT_FULL_SPEED 1
#define PORT_LOW_SPEED 2
#define nibble2Ascii (n)   ((n) + (((n) < 10) ? '0' : 'A' - 10));
#define STATIC_CONST_STRING_DESC (_name, ...)
#define STATIC_CONST_STRING_DESC_LANGID (_name, x, y)
#define UBUF (x, y)   EFM32_ALIGN(4) uint8_t x[((y) + 3) & ~3]
#define STATIC_UBUF (x, y)   EFM32_ALIGN(4) static uint8_t x[((y) + 3) & ~3]

Typedefs

typedef int(* USB_XferCompleteCb_TypeDef ) ( USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining)
USB transfer callback function.
typedef void(* USBTIMER_Callback_TypeDef ) (void)
USBTIMER callback function.

Enumerations

enum USB_Status_TypeDef {
USB_STATUS_OK = 0,
USB_STATUS_REQ_ERR = -1,
USB_STATUS_EP_BUSY = -2,
USB_STATUS_REQ_UNHANDLED = -3,
USB_STATUS_ILLEGAL = -4,
USB_STATUS_EP_STALLED = -5,
USB_STATUS_EP_ABORTED = -6,
USB_STATUS_EP_ERROR = -7,
USB_STATUS_EP_NAK = -8,
USB_STATUS_DEVICE_UNCONFIGURED = -9,
USB_STATUS_DEVICE_SUSPENDED = -10,
USB_STATUS_DEVICE_RESET = -11,
USB_STATUS_TIMEOUT = -12,
USB_STATUS_DEVICE_REMOVED = -13,
USB_STATUS_HC_BUSY = -14,
USB_STATUS_DEVICE_MALFUNCTION = -15,
USB_STATUS_PORT_OVERCURRENT = -16
}
USB transfer status enumerator.

Functions

void USBTIMER_DelayMs (uint32_t msec)
void USBTIMER_DelayUs (uint32_t usec)
void USBTIMER_Init (void)
void USBTIMER_Start (uint32_t id, uint32_t timeout, USBTIMER_Callback_TypeDef callback)
void USBTIMER_Stop (uint32_t id)

Detailed Description

See em_usb.h for source code.

Macro Definition Documentation

#define CLEAR_FEATURE   1

Standard setup request CLEAR_FEATURE.

#define CONFIG_DESC_BM_REMOTEWAKEUP   0x20

Configuration descriptor attribute macro.

#define CONFIG_DESC_BM_RESERVED_D7   0x80

Configuration descriptor attribute macro.

#define CONFIG_DESC_BM_SELFPOWERED   0x40

Configuration descriptor attribute macro.

#define CONFIG_DESC_BM_TRANSFERTYPE   0x03

Configuration descriptor transfer type bitmask.

Referenced by USBD_Init() .

#define CONFIG_DESC_MAXPOWER_mA ( x ) (((x) + 1) / 2)

Configuration descriptor power macro.

#define DEVICE_IS_SELFPOWERED   0x0001

Standard request GET_STATUS bitmask.

#define GET_CONFIGURATION   8

Standard setup request GET_CONFIGURATION.

#define GET_DESCRIPTOR   6

Standard setup request GET_DESCRIPTOR.

#define GET_INTERFACE   10

Standard setup request GET_INTERFACE.

#define GET_STATUS   0

Standard setup request GET_STATUS.

#define HUB_FEATURE_C_PORT_CONNECTION   16

HUB class request CLEAR/SET_PORT_FEATURE feature selector.

#define HUB_FEATURE_C_PORT_RESET   20

HUB class request CLEAR/SET_PORT_FEATURE feature selector.

#define HUB_FEATURE_PORT_INDICATOR   22

HUB class request CLEAR/SET_PORT_FEATURE feature selector.

#define HUB_FEATURE_PORT_POWER   8

HUB class request CLEAR/SET_PORT_FEATURE feature selector.

#define HUB_FEATURE_PORT_RESET   4

HUB class request CLEAR/SET_PORT_FEATURE feature selector.

#define nibble2Ascii ( n ) ((n) + (((n) < 10) ? '0' : 'A' - 10));
#define PORT_FULL_SPEED   1

Full speed return value for USBH_GetPortSpeed().

#define PORT_LOW_SPEED   2

Low speed return value for USBH_GetPortSpeed().

#define REMOTE_WAKEUP_ENABLED   0x0002

Standard request GET_STATUS bitmask.

#define SET_ADDRESS   5

Standard setup request SET_ADDRESS.

#define SET_CONFIGURATION   9

Standard setup request SET_CONFIGURATION.

#define SET_DESCRIPTOR   7

Standard setup request SET_DESCRIPTOR.

#define SET_FEATURE   3

Standard setup request SET_FEATURE.

#define SET_INTERFACE   11

Standard setup request SET_INTERFACE.

#define STATIC_CONST_STRING_DESC ( _name,
...
)
Value:
EFM32_PACK_START(1) \
typedef struct \
{ \
uint8_t len; \
uint8_t type; \
char16_t name[1 + sizeof ((char16_t[]){ __VA_ARGS__ }) / 2]; \
} __attribute__ ((packed)) _ ##_name; \
EFM32_PACK_END() \
EFM32_ALIGN(4) \
EFM32_PACK_START(1) \
static const _##_name _name = \
{ \
.len = sizeof(_##_name) - 2, \
.type = USB_STRING_DESCRIPTOR, \
.name = { __VA_ARGS__ }, \
.name[((sizeof(_##_name) - 2) / 2) - 1] = '\0' \
} \
EFM32_PACK_END()
#define __attribute__(...)
Define attribute to nothing since it isn&#39;t handled by IAR.
Definition: iar.h:221
#define STATIC_CONST_STRING_DESC_LANGID ( _name,
x,
y
)
Value:
EFM32_PACK_START(1) \
typedef struct \
{ \
uint8_t len; \
uint8_t type; \
uint8_t name[2]; \
} _##_name; \
EFM32_PACK_END() \
EFM32_ALIGN(4) \
EFM32_PACK_START(1) \
static const _##_name _name __attribute__ ((aligned(4))) = \
{ \
.len = 4, \
.name = { y, x } \
} \
EFM32_PACK_END()
#define USB_STRING_DESCRIPTOR
Definition: em_usb.h:135
#define __attribute__(...)
Define attribute to nothing since it isn&#39;t handled by IAR.
Definition: iar.h:221

Macro for creating USB compliant language string descriptors.
Example: STATIC_CONST_STRING_DESC_LANGID( langID, 0x04, 0x09 ) ;

#define STATIC_UBUF ( x,
y
) EFM32_ALIGN(4) static uint8_t x[((y) + 3) & ~3]
#define SYNCH_FRAME   12

Standard setup request SYNCH_FRAME.

#define UBUF ( x,
y
) EFM32_ALIGN(4) uint8_t x[((y) + 3) & ~3]

Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
Example:
UBUF( rxBuffer, 37 ) ; => uint8_t rxBuffer[ 40 ];

#define USB_CDC_ACM_FND_DESCSIZE   4

CDC Abstract Control Management functional descriptor size.

#define USB_CDC_CALLMNG_FND_DESCSIZE   5

CDC Call Management functional descriptor size.

#define USB_CDC_GETLINECODING   0x21

CDC class setup request GET_LINE_CODING.

#define USB_CDC_HEADER_FND_DESCSIZE   5

CDC Header functional descriptor size.

#define USB_CDC_SETCTRLLINESTATE   0x22

CDC class setup request SET_CONTROL_LINE_STATE.

#define USB_CDC_SETLINECODING   0x20

CDC class setup request SET_LINE_CODING.

#define USB_CLASS_CDC   2

CDC device/interface class code.

#define USB_CLASS_CDC_ACM   2

CDC Abstract Control Model interface subclass code.

#define USB_CLASS_CDC_ACMFN   2

CDC class Abstract Control Management Functional Descriptor subtype.

#define USB_CLASS_CDC_CMNGFN   1

CDC class Call Management Functional Descriptor subtype.

#define USB_CLASS_CDC_DATA   0x0A

CDC Data interface class code.

#define USB_CLASS_CDC_HFN   0

CDC class Header Functional Descriptor subtype.

#define USB_CLASS_CDC_UNIONFN   6

CDC class Union Functional Descriptor subtype.

#define USB_CLASS_HID   3

HID device/interface class code.

#define USB_CLASS_HID_KEYBOARD   1

HID keyboard interface protocol code.

#define USB_CLASS_HID_MOUSE   2

HID mouse interface protocol code.

#define USB_CLASS_HUB   9

HUB device/interface class code.

#define USB_CLASS_MSD   8

MSD device/interface class code.

#define USB_CLASS_MSD_BOT_TRANSPORT   0x50

MSD Bulk Only Transport protocol.

#define USB_CLASS_MSD_CSW_CMDFAILED   1

MSD BOT Command status wrapper command failed code.

#define USB_CLASS_MSD_CSW_CMDPASSED   0

MSD BOT Command status wrapper command passed code.

#define USB_CLASS_MSD_CSW_PHASEERROR   2

MSD BOT Command status wrapper cmd phase error code.

#define USB_CLASS_MSD_SCSI_CMDSET   6

MSD Subclass SCSI transparent command set.

#define USB_CONFIG_DESCRIPTOR   2

CONFIGURATION descriptor value.

#define USB_CONFIG_DESCSIZE   9

Configuration descriptor size.

#define USB_CS_INTERFACE_DESCRIPTOR   0x24

Audio Class-specific Descriptor Type.

#define USB_DEVICE_DESCRIPTOR   1

DEVICE descriptor value.

#define USB_DEVICE_DESCSIZE   18

Device descriptor size.

#define USB_DEVICE_QUALIFIER_DESCRIPTOR   6

DEVICE_QUALIFIER descriptor value.

#define USB_DEVICE_QUALIFIER_DESCSIZE   10

Device qualifier descriptor size.

#define USB_ENDPOINT_DESCRIPTOR   5

ENDPOINT descriptor value.

Referenced by USBD_Init() .

#define USB_ENDPOINT_DESCSIZE   7

Endpoint descriptor size.

#define USB_EP0_SIZE   8

The size of endpoint 0.

Referenced by USBD_Init() .

#define USB_EP1_SIZE   8

The size of endpoint 1.

#define USB_EP2_SIZE   8

The size of endpoint 2.

#define USB_EP3_SIZE   64

The size of endpoint 3.

#define USB_EP4_SIZE   32

The size of endpoint 4.

#define USB_EP5_SIZE   64

The size of endpoint 5.

#define USB_EP6_SIZE   512

The size of endpoint 6.

#define USB_EP_DIR_IN   0x80

Endpoint direction mask.

#define USB_EPNUM_MASK   0x0F

Endpoint number mask.

Referenced by USBD_Init() .

#define USB_EPTYPE_BULK   2

Endpoint type bulk.

#define USB_EPTYPE_CTRL   0

Endpoint type control.

Referenced by USBD_Init() .

#define USB_EPTYPE_INTR   3

Endpoint type interrupt.

#define USB_EPTYPE_ISOC   1

Endpoint type isochron.

#define USB_FEATURE_DEVICE_REMOTE_WAKEUP   1

Standard request CLEAR/SET_FEATURE bitmask.

#define USB_FEATURE_ENDPOINT_HALT   0

Standard request CLEAR/SET_FEATURE bitmask.

#define USB_HID_DESCRIPTOR   0x21

HID descriptor value.

#define USB_HID_DESCSIZE   9

HID descriptor size.

#define USB_HID_GET_IDLE   0x02

HID class setup request GET_IDLE.

#define USB_HID_GET_REPORT   0x01

HID class setup request GET_REPORT.

#define USB_HID_REPORT_DESCRIPTOR   0x22

HID REPORT descriptor value.

#define USB_HID_SET_IDLE   0x0A

HID class setup request SET_IDLE.

#define USB_HID_SET_PROTOCOL   0x0B

HID class setup request SET_PROTOCOL.

#define USB_HID_SET_REPORT   0x09

HID class setup request SET_REPORT.

#define USB_HUB_DESCRIPTOR   0x29

HUB descriptor value.

#define USB_INTERFACE_DESCRIPTOR   4

INTERFACE descriptor value.

#define USB_INTERFACE_DESCSIZE   9

Interface descriptor size.

#define USB_INTERFACE_POWER_DESCRIPTOR   8

INTERFACE_POWER descriptor value.

#define USB_LANGID_ENUS   0x0409

English-United States language id.

#define USB_MAX_DEVICE_ADDRESS   127

Maximum allowable device address.

#define USB_MAX_EP_SIZE   64

The max size of any full speed endpoint.

#define USB_MSD_BOTRESET   0xFF

MSD class setup request Bulk only transfer reset.

#define USB_MSD_GETMAXLUN   0xFE

MSD class setup request Get Max LUN.

#define USB_OTHER_SPEED_CONFIG_DESCRIPTOR   7

OTHER_SPEED_CONFIGURATION descriptor value.

#define USB_OTHER_SPEED_CONFIG_DESCSIZE   9

Device other speed configuration descriptor size.

#define USB_SETUP_DIR_D2H   0x80

Setup request data stage IN direction mask.

#define USB_SETUP_DIR_H2D   0x00

Setup request data stage OUT direction mask.

#define USB_SETUP_DIR_IN   1

Setup request data stage IN direction value.

#define USB_SETUP_DIR_MASK   0x80

Setup request data stage direction mask.

Referenced by USBD_Init() .

#define USB_SETUP_DIR_OUT   0

Setup request data stage OUT direction value.

#define USB_SETUP_PKT_SIZE   8

Setup request packet size.

#define USB_SETUP_RECIPIENT_DEVICE   0

Setup request device recipient value.

#define USB_SETUP_RECIPIENT_ENDPOINT   2

Setup request endpoint recipient value.

#define USB_SETUP_RECIPIENT_INTERFACE   1

Setup request interface recipient value.

#define USB_SETUP_RECIPIENT_OTHER   3

Setup request other recipient value.

#define USB_SETUP_TYPE_CLASS   1

Class setup request value.

#define USB_SETUP_TYPE_CLASS_MASK   0x20

Class setup request mask.

#define USB_SETUP_TYPE_STANDARD   0

Standard setup request value.

#define USB_SETUP_TYPE_STANDARD_MASK   0x00

Standard setup request mask.

#define USB_SETUP_TYPE_VENDOR   2

Vendor setup request value.

#define USB_SETUP_TYPE_VENDOR_MASK   0x40

Vendor setup request mask.

#define USB_STRING_DESCRIPTOR   3

STRING descriptor value.

Typedef Documentation

typedef int(* USB_XferCompleteCb_TypeDef) ( USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining)

The callback function is called when a transfer has completed. An application should check the status, xferred and optionally the remaining parameters before deciding if the transfer is usable. In the case where the transfer is part of a control request data stage, the callback function should return an appropriate USB_Status_TypeDef status.

Parameters
[in] status The transfer status. See USB_Status_TypeDef .
[in] xferred Number of bytes actually transferred.
[in] remaining Number of bytes not transferred.
Returns
USB_STATUS_OK on success, else an appropriate error code.
typedef void(* USBTIMER_Callback_TypeDef) (void)

The callback function is called when an USBTIMER has expired. The callback is done with interrupts disabled.

Enumeration Type Documentation

Enumerator
USB_STATUS_OK

No errors detected.

USB_STATUS_REQ_ERR

Setup request error.

USB_STATUS_EP_BUSY

Endpoint is busy.

USB_STATUS_REQ_UNHANDLED

Setup request not handled.

USB_STATUS_ILLEGAL

Illegal operation attempted.

USB_STATUS_EP_STALLED

Endpoint is stalled.

USB_STATUS_EP_ABORTED

Endpoint transfer was aborted.

USB_STATUS_EP_ERROR

Endpoint transfer error.

USB_STATUS_EP_NAK

Endpoint NAK'ed transfer request.

USB_STATUS_DEVICE_UNCONFIGURED

Device is unconfigured.

USB_STATUS_DEVICE_SUSPENDED

Device is suspended.

USB_STATUS_DEVICE_RESET

Device is/was reset.

USB_STATUS_TIMEOUT

Transfer timeout.

USB_STATUS_DEVICE_REMOVED

Device was removed.

USB_STATUS_HC_BUSY

Host channel is busy.

USB_STATUS_DEVICE_MALFUNCTION

Malfunctioning device attached.

USB_STATUS_PORT_OVERCURRENT

VBUS shortcircuit/overcurrent failure.

Function Documentation

void USBTIMER_DelayMs ( uint32_t msec )
void USBTIMER_DelayUs ( uint32_t usec )
void USBTIMER_Init ( void )

Referenced by USBD_Init() .

void USBTIMER_Start ( uint32_t id,
uint32_t timeout,
USBTIMER_Callback_TypeDef callback
)
void USBTIMER_Stop ( uint32_t id )