DTLS API
Macros | |
#define | EMBER_DTLS_MODE_CERT 0x01 |
Define the various modes of a DTLS connection. | |
#define | EMBER_DTLS_MODE_PSK 0x02 |
#define | EMBER_DTLS_MODE_PKEY 0x04 |
Typedefs | |
typedef uint8_t | EmberDtlsMode |
Functions | |
void | emberSetDtlsDeviceCertificate (const CertificateAuthority **certAuthority, const DeviceCertificate *deviceCert) |
Set a device certificate to be used to create a certificate based secure session on the application. The expected arguments are DER encoded X.509 certificates. If this succeeds, emberSetDtlsDeviceCertificateReturn should return 0. | |
void | emberSetDtlsDeviceCertificateReturn (uint32_t result) |
Provides the result of a call to emberSetDtlsDeviceCertificate(). | |
void | emberSetDtlsPresharedKey (const uint8_t *key, uint8_t keyLength, const uint8_t *identity, uint8_t identityLength, const EmberIpv6Address *remoteAddress) |
Set a key to be used to create a PSK based secure session on the application. The maximum length of the key is 32 bytes. | |
void | emberSetDtlsPresharedKeyReturn (EmberStatus status) |
Provides the result of a call to emberSetDtlsPresharedKey(). | |
void | emberOpenDtlsConnection (EmberDtlsMode dtlsMode, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Establish a DTLS connection with a peer on the Thread network. When established, this session can be used to send secure CoAP data. The device requesting the connection acts as a DTLS client. | |
void | emberOpenDtlsConnectionReturn (uint32_t result, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Provides the result of a call to emberOpenDtlsConnection(). | |
void | emberDtlsSecureSessionEstablished (uint8_t flags, uint8_t sessionId, const EmberIpv6Address *localAddress, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Indicates to the application that a secure connection was successfully established. | |
uint8_t | emberGetSecureDtlsSessionId (const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Request the session ID given connection parameters. | |
uint8_t | emberGetDtlsConnectionNextSessionId (uint8_t sessionId) |
Request the next session ID following the given one. If EMBER_NULL_SESSION_ID is passed, then the first session ID is returned. | |
EmberStatus | emberGetDtlsConnectionPeerAddressBySessionId (const uint8_t sessionId, EmberIpv6Address *remoteAddress) |
Request the address associated with a particular session. | |
EmberStatus | emberGetDtlsConnectionPeerPortBySessionId (const uint8_t sessionId, uint16_t *remotePort) |
Request the port associated with a particular session. | |
EmberStatus | emberGetDtlsConnectionPeerPublicKeyBySessionId (const uint8_t sessionId, uint8_t *publicKey, const uint16_t publicKeyMaxSize, uint16_t *publicKeySize) |
Request the public key associated with a particular session. | |
void | emberCloseDtlsConnection (uint8_t sessionId) |
Close a currently active secure session on the application. When successful, emberCloseDtlsConnectionReturn should be called on both ends of the connection with EMBER_SUCCESS. | |
void | emberCloseDtlsConnectionReturn (uint8_t sessionId, EmberStatus status) |
Provides the result of a call to emberCloseDtlsConnection(), or indicates that the connection was closed on the other end. | |
bool | emberDtlsTransmitHandler (const uint8_t *payload, uint16_t payloadLength, const EmberIpv6Address *localAddress, uint16_t localPort, const EmberIpv6Address *remoteAddress, uint16_t remotePort, void *transmitHandlerData) |
Public DTLS transmit handler to be set in emberCoapSend. The secure payload is delivered via emberProcessCoap on the other end, with a matching session ID in the transmitHandlerData of its CoapRequestInfo. See emberProcessCoap (stack/include/coap.h ) |
Detailed Description
See dtls.h
for source code.
Macro Definition Documentation
#define EMBER_DTLS_MODE_CERT 0x01 |
Note: Please configure either the CERT or PSK modes, as the public key option is currently unavailable.
#define EMBER_DTLS_MODE_PKEY 0x04 |
#define EMBER_DTLS_MODE_PSK 0x02 |
Typedef Documentation
typedef uint8_t EmberDtlsMode |
Function Documentation
void emberCloseDtlsConnection | ( | uint8_t | sessionId | ) |
- Parameters
-
sessionId
sessionId used for secure CoAP transport.
void emberCloseDtlsConnectionReturn | ( | uint8_t | sessionId, |
EmberStatus | status |
||
) |
- Parameters
-
sessionId
sessionId used for secure CoAP transport. status
- EMBER_SUCCESS - Successfully closed the connection
- EMBER_INVALID_CALL - Invalid session ID
- EMBER_ERR_FATAL - Fatal error closing the connection
void emberDtlsSecureSessionEstablished | ( | uint8_t | flags, |
uint8_t | sessionId, |
||
const EmberIpv6Address * | localAddress, |
||
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
- Parameters
-
flags
1 = server, 0 = client (possibly other info later) sessionId
sessionId used for secure CoAP transport localAddress
local IPv6 address remoteAddress
remote IPv6 address localPort
local port remotePort
remote port
bool emberDtlsTransmitHandler | ( | const uint8_t * | payload, |
uint16_t | payloadLength, |
||
const EmberIpv6Address * | localAddress, |
||
uint16_t | localPort, |
||
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | remotePort, |
||
void * | transmitHandlerData |
||
) |
- Parameters
-
payload
CoAP payload to be sent securely payloadLength
payload length localAddress
local IPv6 address localPort
local port remoteAddress
remote IPv6 address remotePort
remote port transmitHandlerData
session ID of the secure connection (see emberDtlsSecureSessionEstablished or emberGetSecureDtlsSessionId above)
uint8_t emberGetDtlsConnectionNextSessionId | ( | uint8_t | sessionId | ) |
- Parameters
-
sessionId
session ID to be followed
EmberStatus emberGetDtlsConnectionPeerAddressBySessionId | ( | const uint8_t | sessionId, |
EmberIpv6Address * | remoteAddress |
||
) |
- Parameters
-
sessionId
session ID of interest remoteAddress
remote address used in session
EmberStatus emberGetDtlsConnectionPeerPortBySessionId | ( | const uint8_t | sessionId, |
uint16_t * | remotePort |
||
) |
- Parameters
-
sessionId
session ID of interest remotePort
remote port used in session
EmberStatus emberGetDtlsConnectionPeerPublicKeyBySessionId | ( | const uint8_t | sessionId, |
uint8_t * | publicKey, |
||
const uint16_t | publicKeyMaxSize, |
||
uint16_t * | publicKeySize |
||
) |
- Parameters
-
sessionId
session ID of interest publicKey
Array that will store the public key publicKeyMaxSize
Maximum size of the array publickeySize
Size of the array in use
uint8_t emberGetSecureDtlsSessionId | ( | const EmberIpv6Address * | remoteAddress, |
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
- Parameters
-
remoteAddress
remote IPv6 address localPort
local port remotePort
remote port
void emberOpenDtlsConnection | ( | EmberDtlsMode | dtlsMode, |
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
(For DotDot applications, the local port and remote port are both EMBER_COAP_SECURE_PORT)
- Parameters
-
dtlsMode
DTLS connection mode (see EMBER_DTLS_MODE_* above) remoteAddress
IPv6 address of the server localPort
local port remotePort
remote port
void emberOpenDtlsConnectionReturn | ( | uint32_t | result, |
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
- Parameters
-
result
error code - an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
remoteAddress
IPv6 address of the server localPort
local port remotePort
remote port
void emberSetDtlsDeviceCertificate | ( | const CertificateAuthority ** | certAuthority, |
const DeviceCertificate * | deviceCert |
||
) |
- Parameters
-
certAuthority
the certificate authority deviceCert
the certificate
void emberSetDtlsDeviceCertificateReturn | ( | uint32_t | result | ) |
- Parameters
-
result
- ::0 The certificate was set successfully.
- ::result error code
- an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
void emberSetDtlsPresharedKey | ( | const uint8_t * | key, |
uint8_t | keyLength, |
||
const uint8_t * | identity, |
||
uint8_t | identityLength, |
||
const EmberIpv6Address * | remoteAddress |
||
) |
Note: Up to 32 pre-shared keys can be stored.
If this succeeds, emberSetDtlsPresharedKeyReturn will return EMBER_SUCCESS. Otherwise, a failure status is indicated.
- Parameters
-
key
the pre-shared key keyLength
key length key
the pre-shared identity keyLength
identity length remoteAddress
IPv6 address of peer
void emberSetDtlsPresharedKeyReturn | ( | EmberStatus | status | ) |
- Parameters
-
result
- ::status An EmberStatus value