Additional information about an incoming response.

#include < coap.h >

Data Fields

EmberIpv6Address localAddress
EmberIpv6Address remoteAddress
uint16_t localPort
uint16_t remotePort
void * applicationData
uint16_t applicationDataLength

Field Documentation

void* EmberCoapResponseInfo::applicationData

The value passed to emberCoapSend() .

uint16_t EmberCoapResponseInfo::applicationDataLength

The value passed to emberCoapSend() .

EmberIpv6Address EmberCoapResponseInfo::localAddress
uint16_t EmberCoapResponseInfo::localPort
EmberIpv6Address EmberCoapResponseInfo::remoteAddress
uint16_t EmberCoapResponseInfo::remotePort

The documentation for this struct was generated from the following file:
  • coap.h