Microphone Codec MSADPCM Callbacks
Functions |
|
void | halMicrophoneCodecMsadpcmDataReadyCallback (uint8_t *data, uint8_t length) |
Called when new microphone data is ready.
|
Detailed Description
These callbacks are contributed by the Microphone Codec MSADPCM plugin.
Function Documentation
void halMicrophoneCodecMsadpcmDataReadyCallback | ( | uint8_t * |
data,
|
uint8_t |
length
|
||
) |
This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.
- Parameters
-
data
Pointer to the data that is ready. length
Length of the data.