network-management API Callbacks
Functions |
|
| void | emberActiveScanHandler (const EmberMacBeaconData *beaconData) |
|
Reports an incoming beacon during an active scan.
|
|
| void | emberAddressConfigurationChangeHandler (const EmberIpv6Address *address, uint32_t preferredLifetime, uint32_t validLifetime, uint8_t addressFlags) |
|
This is called when a new address is configured on the application.
|
|
| void | emberAttachToNetworkReturn ( EmberStatus status) |
|
A callback that indicates whether the attach process was successfully initiated via a prior call to
emberAttachToNetwork()
. The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if attach was called when the network status was not EMBER_JOINED_NETWORK_NO_PARENT, or while an attach was underway.
|
|
| void | emberBecomeCommissionerReturn ( EmberStatus status) |
|
Return call for
emberBecomeCommissioner()
. The status is EMBER_SUCCESS if a petition was sent or EMBER_ERR_FATAL if some temporary resource shortage prevented doing so.
|
|
| void | emberChangeNodeTypeReturn ( EmberStatus status) |
|
Provides the result of a call to
emberChangeNodeType()
: either EMBER_SUCCESS, or EMBER_INVALID_CALL.
|
|
| void | emberAllowNativeCommissionerReturn ( EmberStatus status) |
|
Provides the result of a call to
emberAllowNativeCommissioner()
: either EMBER_SUCCESS or EMBER_INVALID_CALL.
|
|
| void | emberSetCommissionerKeyReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetCommissionerKey()
: either EMBER_SUCCESS or EMBER_INVALID_CALL.
|
|
| void | emberSetPskcHandler (const uint8_t *pskc) |
|
Handler to let application know that a PSKc TLV was successfully set.
|
|
| void | emberSetJoinKeyReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetJoinKey()
: either EMBER_SUCCESS or EMBER_BAD_ARGUMENT.
|
|
| void | emberSetParentPriorityReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetParentPriority()
: either EMBER_SUCCESS or EMBER_INVALID_CALL.
|
|
| void | emberGetParentPriorityReturn (const int8_t parentPriority) |
|
Provides the result of a call to
emberGetParentPriority()
:
|
|
| void | emberCommissionNetworkReturn ( EmberStatus status) |
|
Provides the result of a call to emberCommissionNetwork.
|
|
| void | emberCommissionerStatusHandler (uint16_t flags, const uint8_t *commissionerName, uint8_t commissionerNameLength) |
|
Reports on the current commissioner state.
|
|
| void | emberConfigureGatewayReturn ( EmberStatus status) |
|
Provides the result of a call to
emberConfigureGateway
.
|
|
| void | emberSetNdDataReturn ( EmberStatus status, uint16_t length) |
|
Provides the result of a call to
emberSetNdData
.
|
|
| void | emberSetLocalNetworkDataReturn ( EmberStatus status, uint16_t length) |
|
Provides the result of a call to
emberSetLocalNetworkData
.
|
|
| void | emberConfigureExternalRouteReturn ( EmberStatus status) |
|
Provides the result of a call to
emberConfigureExternalRoute
.
|
|
| void | emberCounterHandler ( EmberCounterType type, uint16_t increment) |
|
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
|
|
| uint16_t | emberCounterValueHandler ( EmberCounterType type) |
|
A callback invoked to query the application for the countervalue of an event defined by EmberCounterType.
|
|
| void | emberResetCounterHandler ( EmberCounterType type) |
|
A callback invoked to the application to reset the countervalue of an event defined by EmberCounterType.
|
|
| void | emberCustomHostToNcpMessageHandler (const uint8_t *message, uint16_t messageLength) |
|
NCP handler called to process a custom message from the Host.
|
|
| void | emberCustomNcpToHostMessageHandler (const uint8_t *message, uint16_t messageLength) |
|
Host handler called to process a custom message from the NCP.
|
|
| void | emberDhcpServerChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
|
This is called when the stack knows about a new dhcp server or if a dhcp server has become unavailable.
|
|
| void | emberEnergyScanHandler (uint8_t channel, int8_t maxRssiValue) |
|
Reports the maximum RSSI value measured on the channel.
|
|
| void | emberEventDelayUpdatedFromIsrHandler ( Event *event) |
|
This method is called any time an event is scheduled from within an ISR context. It can be used to determine when to stop a long running sleep to see what application or stack events now need to be processed.
|
|
| void | emberExternalRouteChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
|
This is called when the stack knows about a border router that has an external route to a prefix.
|
|
| void | emberForceTxAfterFailedCcaReturn ( EmberStatus status) |
|
Provides the result of a call to
emberForceTxAfterFailedCca
.
|
|
| void | emberFormNetworkReturn ( EmberStatus status) |
|
A callback that indicates whether a prior call to
emberFormNetwork()
successfully initiated the form process. The status argument is either EMBER_SUCCSS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_NO_NETWORK, or a scan was underway.
|
|
| void | emberGetAntennaModeReturn ( EmberStatus status, uint8_t mode) |
|
Provides the result of a call to
emberGetAntennaMode
.
|
|
| void | emberGetAntennaRxModeReturn ( EmberStatus status, uint8_t mode) |
|
Provides the result of a call to
emberGetAntennaRxMode
.
|
|
| void | emberGetCcaThresholdReturn (int8_t threshold) |
|
Provides the result of a call to
emberGetCcaThreshold()
.
|
|
| void | emberGetChannelCalDataTokenReturn (uint8_t lna, int8_t tempAtLna, uint8_t modDac, int8_t tempAtModDac) |
|
Gets the token information for tokenId = EMBER_CHANNEL_CAL_DATA_TOKEN.
|
|
| void | emberGetChildEntryReturn (uint8_t status, uint8_t index, uint8_t childTableSize, const EmberChildEntry *entry, const EmberIpv6Address *addresses, uint8_t addressCount) |
|
This callback returns the results of a call to
emberGetChildEntry()
. A status of EMBER_GET_CHILD_ENTRY_SUCCESS indicates a valid entry is being returned in the
EmberChildEntry
argument, located at the supplied index in the child table of size childTableSize. Note that the index returned is the smallest index not less than the index that was supplied to
emberGetChildEntry()
, which contains a valid child entry.
|
|
| void | emberGetCounterReturn ( EmberCounterType type, uint16_t value) |
|
Provides the result of a call to
emberGetCounter()
.
|
|
| void | emberGetCtuneReturn (uint16_t tune, EmberStatus status) |
|
Provides the result of a call to
emberGetCtune
.
|
|
| void | emberGetGlobalAddressReturn (const EmberIpv6Address *address, uint32_t preferredLifetime, uint32_t validLifetime, uint8_t addressFlags) |
|
Provides the result of a call to
emberGetGlobalAddresses
.
|
|
| void | emberGetGlobalPrefixReturn (uint8_t flags, bool isStable, const uint8_t *prefix, uint8_t prefixLengthInBits, uint8_t domainId, uint32_t preferredLifetime, uint32_t validLifetime) |
|
Provides the result of a call to ::emberGetGlobalPrefix.
|
|
| void | emberLinkMetricsMgmtHandler ( EmberLinkMetricsStatus status, const uint8_t *remoteAddress) |
|
This function is called when the link metrics initiator gets a link management response message.
|
|
| void | emberLinkMetricsResponseHandler ( EmberLinkMetricsStatus status, const uint8_t *remoteAddress, const uint8_t *reportTlvValue, uint8_t reportTlvLength) |
|
This function is called when the link metrics initiator gets an MLE Data Response message in response to a link metrics query.
|
|
| void | emberGetMfgTokenReturn ( EmberMfgTokenId tokenId, EmberStatus status, const uint8_t *tokenData, uint8_t tokenDataLength) |
|
Provides the result of a call to
emberGetMfgToken
.
|
|
| void | emberGetNetworkDataReturn ( EmberStatus status, uint8_t *networkData, uint16_t bufferLength) |
|
Provides the result of a call to
emberGetNetworkData
.
|
|
| void | emberGetNetworkDataTlvReturn (uint8_t typeByte, uint8_t index, uint8_t versionNumber, const uint8_t *tlv, uint8_t tlvLength) |
|
Provides the result of a call to
emberGetNetworkDataTlv()
.
|
|
| void | emberGetPtaDirectionalPriorityPulseWidthReturn (uint8_t pulseWidthUs) |
|
Provides the result of a call to
emberGetPtaDirectionalPriorityPulseWidth
.
|
|
| void | emberGetPtaEnableReturn (bool enabled) |
|
Provides the result of a call to
emberGetPtaEnable
.
|
|
| void | emberGetPtaOptionsReturn (uint32_t options) |
|
Provides the result of a call to
emberGetPtaOptions
.
|
|
| void | emberGetPtaPhySelectTimeoutReturn (uint8_t timeoutMs) |
|
Provides the result of a call to
emberGetPtaPhySelectTimeout
.
|
|
| void | emberGetPtaPwmOptionsReturn (uint8_t request, uint8_t dutyCycle, uint8_t periodHalfMs) |
|
This function provides the result of a call to
emberGetPtaPwmOptions
.
|
|
| void | emberGetRadioPowerReturn (int8_t power) |
|
Provides the result of a call to
emberGetRadioPower()
on the host.
|
|
| void | emberGetRipEntryReturn (uint8_t index, const EmberRipEntry *entry) |
|
Provides the result of a call to
emberGetRipEntry()
.
|
|
| void | emberGetRoutingLocatorReturn (const EmberIpv6Address *rloc) |
|
Provides the result of a call to
emberGetRoutingLocator
.
|
|
| void | emberGetStandaloneBootloaderInfoReturn (uint16_t version, uint8_t platformId, uint8_t microId, uint8_t phyId) |
|
Provides the result of a call to
emberGetStandaloneBootloaderInfo
.
|
|
| void | emberGetTxPowerModeReturn (uint16_t txPowerMode) |
|
Provides the result of a call to
emberGetTxPowerMode()
on the host.
|
|
| void | emberGetVersionsReturn (const uint8_t *versionName, uint16_t managementVersionNumber, uint16_t stackVersionNumber, uint16_t stackBuildNumber, EmberVersionType versionType, const uint8_t *buildTimestamp) |
|
Provides the result of a call to
emberGetVersions()
.
|
|
| void | emberSetAddressHandler (const uint8_t *address) |
|
In a host/NCP setup, notifies the host to set the new mesh local address.
|
|
| void | emberHostStateHandler (const EmberNetworkParameters *parameters, const EmberEui64 *localEui64, const EmberEui64 *macExtendedId, EmberNetworkStatus networkStatus) |
|
In a host/NCP setup, notifies the host to changes in the network parameters.
|
|
| void | emberInitReturn ( EmberStatus status) |
|
Provides the result of a call to
emberInit()
.
|
|
| void | emberInitiateLinkMetricsProbingReturn ( EmberStatus status) |
|
Provides the result of a call to
emberInitiateLinkMetricsProbing()
:
|
|
| void | emberJoinNetworkReturn ( EmberStatus status) |
|
A callback that indicates whether the join process was successfully initiated via a prior call to
emberJoinNetwork()
or
emberJoinCommissioned()
. The possible EmberStatus values are: EMBER_SUCCESS, EMBER_BAD_ARGUMENT, or EMBER_INVALID_CALL (if join was called when the network status was something other than EMBER_NO_NETWORK).
|
|
| void | emberLaunchStandaloneBootloaderReturn ( EmberStatus status) |
|
Provides the result of a call to
emberLaunchStandaloneBootloader
.
|
|
| void | emberLeaderDataHandler (const uint8_t *leaderData) |
|
A callback invoked when the leader data changes.
|
|
| bool | emberMacPassthroughFilterHandler (uint8_t *macHeader) |
|
Application handler to define "passthrough" packets.
|
|
| void | emberMacPassthroughMessageHandler ( PacketHeader header) |
|
Application handler to intercept "passthrough" packets and handle them at the application.
|
|
| bool | emberMacRssiFilterHandler (uint8_t *macHeader) |
|
Application handler to filter 802.15.4 packets to be observed for signal strength.
|
|
| void | emberMacRssiHandler (int8_t currentRssi) |
|
Gets the received signal strength indication (RSSI) for the last 802.15.4 packet received by the stack.
|
|
| void | emberNetworkDataChangeHandler (const uint8_t *networkData, uint16_t length) |
|
This is called when the stack receives new Thread Network Data.
|
|
| void | emberNetworkStatusHandler ( EmberNetworkStatus newNetworkStatus, EmberNetworkStatus oldNetworkStatus, EmberJoinFailureReason reason) |
|
Reports a change to the network status. For example, the network status changes while going through the joining process, or while reattaching to the network, which can happen for a variety of reasons. In particular, after issuing a form, join, resume, or attach command, the application knows that the device is on the network and ready to communicate when this handler is called with a newNetworkStatus of EMBER_JOINED_NETWORK_ATTACHED.
|
|
| void | emberOkToNapReturn (uint8_t stateMask) |
|
If implementing event-driven sleep on an NCP host, this method will return the bitmask indicating the stack's current tasks. (see enum above)
|
|
| void | emberPollForDataReturn ( EmberStatus status) |
|
Provides the result of a call to
emberPollForData()
.
|
|
| void | emberRadioGetRandomNumbersReturn ( EmberStatus status, const uint16_t *rn, uint8_t count) |
|
Provides the result of a call to
emberRadioGetRandomNumbers
.
|
|
| void | emberRequestDhcpAddressReturn ( EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
|
Provides the result of a call to
emberRequestDhcpAddress
.
|
|
| void | emberRequestSlaacAddressReturn ( EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
|
Provides the result of a call to
emberRequestSlaacAddress
.
|
|
| void | emberRequestDomainUniqueAddressReturn ( EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
|
This function provides the result of a call to
emberRequestDomainUniqueAddress
.
|
|
| void | emberRequestMulticastListenerReturn ( EmberStatus status, const EmberIpv6Address *address) |
|
This function provides the result of a call to
emberRequestMulticastListener
. This call only indicates the status of the request.
|
|
| void | emberMulticastListenerHandler (const EmberIpv6Address *multicastGroupAddress) |
|
This function is called when a multicast group listener registration was successful, indicating that multicast packets coming from non-Thread IPv6 hosts can be sent to this device by the (primary) BBR.
|
|
| void | emberAddMeshDuaEntryReturn ( EmberStatus status, const EmberIpv6Address *dua) |
|
This function provides the result of a call to
emberAddMeshDuaEntry
.
|
|
| void | emberRemoveMeshDuaEntryReturn ( EmberStatus status, const EmberIpv6Address *dua) |
|
This function provides the result of a call to
emberRemoveMeshDuaEntry
.
|
|
| void | emberResetMicroHandler ( EmberResetCause cause) |
|
Notifies the application of a reset on the Ember chip due to the indicated cause.
|
|
| void | emberResetNetworkStateReturn ( EmberStatus status) |
|
Provides the result of a call to
emberResetNetworkState()
.
|
|
| void | emberResignGlobalAddressReturn ( EmberStatus status) |
|
Provides the result of a call to
emberResignGlobalAddress()
.
|
|
| void | emberResumeNetworkReturn ( EmberStatus status) |
|
A callback that indicates whether a prior call to
emberResumeNetwork()
successfully initiated the resume process. The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_SAVED_NETWORK, or while a scan was underway.
|
|
| void | emberScanReturn ( EmberStatus status) |
|
Provides the status upon completion of a scan.
|
|
| void | emberSendLinkMetricsQueryReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSendLinkMetricsQuery()
:
|
|
| void | emberSendLinkProbeMessagesReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSendLinkProbeMessages()
:
|
|
| void | emberSendSteeringDataReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSendSteeringData()
.
|
|
| void | emberSetAntennaModeReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetAntennaMode
.
|
|
| void | emberSetAntennaRxModeReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetAntennaRxMode
.
|
|
| void | emberSetCcaThresholdReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetCcaThreshold()
.
|
|
| void | emberSetCtuneReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetCtune
.
|
|
| void | emberSetMfgTokenReturn ( EmberMfgTokenId tokenId, EmberStatus status) |
|
Provides the result of a call to
emberSetMfgToken
.
|
|
| void | emberSetPtaDirectionalPriorityPulseWidthReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetPtaDirectionalPriorityPulseWidth
.
|
|
| void | emberSetPtaEnableReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetPtaEnable
.
|
|
| void | emberSetPtaOptionsReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetPtaOptions
.
|
|
| void | emberSetPtaPhySelectTimeoutReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetPtaPhySelectTimeout
.
|
|
| void | emberSetPtaPwmOptionsReturn ( EmberStatus status) |
|
This function provides the result of a call to
emberSetPtaPwmOptions
.
|
|
| void | emberSetRadioHoldOffReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetRadioHoldOff
.
|
|
| void | emberSetRadioPowerReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetRadioPower()
on the host.
|
|
| void | emberSetSecurityParametersReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetSecurityParameters()
.
|
|
| void | emberSetTxPowerModeReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetTxPowerMode()
on the host.
|
|
| void | emberSlaacServerChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
|
This is called when the stack knows about a new SLAAC prefix or if a SLAAC server has become unavailable.
|
|
| void | emberConfigureDefaultDomainPrefixReturn ( EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
|
This function provides the result of a call to
emberConfigureDefaultDomainPrefix
.
|
|
| void | emberBecomeBackboneRouterReturn ( EmberStatus status, bool primary) |
|
This function provides the result of a call to
emberConfigureDefaultDomainPrefix
.
|
|
| void | emberSetBbrDatasetReturn ( EmberStatus status) |
|
This function provides the result of a call to
emberSetBbrDataset
.
|
|
| void | emberBackbonePrefixHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
|
This function is called when the stack knows about a new backbone prefix or if a backbone server has become unavailable.
|
|
| void | emberStackPollForDataReturn ( EmberStatus status) |
|
Provides the result of a call to
emberStackPollForData()
.
|
|
| void | emberStartHostJoinClientHandler (const uint8_t *parentAddress) |
|
Callback to tell the host to start security commissioning.
|
|
| void | emberStateReturn (const EmberNetworkParameters *parameters, const EmberEui64 *localEui64, const EmberEui64 *macExtendedId, EmberNetworkStatus networkStatus) |
|
In a host/NCP setup, provides the result of a call to
emberState()
on the host.
|
|
| void | emberSwitchToNextNetworkKeyHandler ( EmberStatus status) |
|
This can be stubbed out on the SoC and host app. It is used by the NCP to update security on the driver when it is instructed to switch the network key by an over the air update.
|
|
| void | emberSwitchToNextNetworkKeyReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSwitchToNextNetworkKey()
.
|
|
| void | emberSetDtlsDeviceCertificateReturn (uint32_t result) |
|
Provides the result of a call to
emberSetDtlsDeviceCertificate()
.
|
|
| void | emberSetDtlsPresharedKeyReturn ( EmberStatus status) |
|
Provides the result of a call to
emberSetDtlsPresharedKey()
.
|
|
| void | emberOpenDtlsConnectionReturn (uint32_t result, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Provides the result of a call to
emberOpenDtlsConnection()
.
|
|
| void | emberDtlsSecureSessionEstablished (uint8_t flags, uint8_t sessionId, const EmberIpv6Address *localAddress, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
|
Indicates to the application that a secure connection was successfully established.
|
|
| void | emberCloseDtlsConnectionReturn (uint8_t sessionId, EmberStatus status) |
|
Provides the result of a call to
emberCloseDtlsConnection()
, or indicates that the connection was closed on the other end.
|
|
| void | emberProcessCoap (const uint8_t *message, uint16_t messageLength, EmberCoapRequestInfo *info) |
|
Process a CoAP message received over an alternate transport.
|
|
| void | emberMicroBusyHandler (bool busy) |
|
Callback informing the application running on the micro of interruptions to normal processing. If ::busy is true, the micro will be busy processing and unavailable for an indefinite period of time. If ::busy is false, the micro has resumed normal operation. The main use case is jpake crypto on EM3xx processors. This gives the application a chance to prepare for the pause in regular processing.
|
|
Detailed Description
These callbacks were contributed by the network-management API.
Function Documentation
| void emberActiveScanHandler | ( | const EmberMacBeaconData * |
beaconData
|
) |
This function reports an incoming beacon during an active scan.
| void emberAddMeshDuaEntryReturn | ( | EmberStatus |
status,
|
| const EmberIpv6Address * |
dua
|
||
| ) |
- Parameters
-
statusEMBER_SUCCESS or EMBER_TABLE_FULL
| void emberAddressConfigurationChangeHandler | ( | const EmberIpv6Address * |
address,
|
| uint32_t |
preferredLifetime,
|
||
| uint32_t |
validLifetime,
|
||
| uint8_t |
addressFlags
|
||
| ) |
This function is called when a new address is configured on the application.
If addressFlags is EMBER_LOCAL_ADDRESS, it means that the address configured is a Thread-local address.
Otherwise, it means that the address assigned is a global address (DHCP or SLAAC).
In either case, if the valid lifetime is zero, then the address is no longer available.
- Parameters
-
addressthe address preferredLifetimethe preferred lifetime of the address (in seconds) validLifetimethe valid lifetime of the address (in seconds) addressFlagsaddress configuration flags (see LocalServerFlag_e)
| void emberAllowNativeCommissionerReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberAllowNativeCommissioner() : either EMBER_SUCCESS or EMBER_INVALID_CALL.
| void emberAttachToNetworkReturn | ( | EmberStatus |
status
|
) |
| void emberBackbonePrefixHandler | ( | const uint8_t * |
prefix,
|
| uint8_t |
prefixLengthInBits,
|
||
| bool |
available
|
||
| ) |
"available" means we can configure a DUA address.
- Parameters
-
prefixDUA prefix prefixLengthInBitslength in bits of the prefix availablewhether we can configure a DUA address
| void emberBecomeBackboneRouterReturn | ( | EmberStatus |
status,
|
| bool |
primary
|
||
| ) |
- Parameters
-
statusEMBER_SUCCESS or EMBER_INVALID_CALL primarytrue indicates that we are active in a primary BBR role.
| void emberBecomeCommissionerReturn | ( | EmberStatus |
status
|
) |
| void emberChangeNodeTypeReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberChangeNodeType() : either EMBER_SUCCESS, or EMBER_INVALID_CALL.
| void emberCloseDtlsConnectionReturn | ( | uint8_t |
sessionId,
|
| EmberStatus |
status
|
||
| ) |
- Parameters
-
sessionIdsessionId used for secure CoAP transport. status- EMBER_SUCCESS - Successfully closed the connection
- EMBER_INVALID_CALL - Invalid session ID
- EMBER_ERR_FATAL - Fatal error closing the connection
| void emberCommissionerStatusHandler | ( | uint16_t |
flags,
|
| const uint8_t * |
commissionerName,
|
||
| uint8_t |
commissionerNameLength
|
||
| ) |
This function reports on the current commissioner state.
- Parameters
-
flagsA combination of zero or more of the following: - EMBER_HAVE_COMMISSIONER a commissioner is active in the network
- EMBER_AM_COMMISSIONER this device is the active commissioner if emberStopCommissioning is called, then this flag is not returned as we are open to commissioner petitions
- EMBER_JOINING_ENABLED joining is enabled
- EMBER_JOINING_WITH_EUI_STEERING steering data restricts which devices can join. if not set, no restriction, any device can join (significant only when EMBER_JOINING_ENABLED is set)
commissionerNameThe name of the active commissioner, or NULL if there is none or the name is not known. commissionerNameLengthThe length of commissonerName.
| void emberCommissionNetworkReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberCommissionNetwork.
Returns EMBER_SUCCESS if successful EMBER_BAD_ARGUMENT if any of the options are wrong EMBER_INVALID_CALL if the node is already on a network
- Parameters
-
statusWhether the call to emberCommissionNetwork was successful
| void emberConfigureDefaultDomainPrefixReturn | ( | EmberStatus |
status,
|
| const uint8_t * |
prefix,
|
||
| uint8_t |
prefixLengthInBits
|
||
| ) |
- Parameters
-
statusEMBER_SUCCESS or EMBER_BAD_ARGUMENT prefixDefault domain prefix prefixLengthInBitsLength in bits of the prefix
| void emberConfigureExternalRouteReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberConfigureExternalRoute .
| void emberConfigureGatewayReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberConfigureGateway .
| void emberCounterHandler | ( | EmberCounterType |
type,
|
| uint16_t |
increment
|
||
| ) |
The application must define EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
- Parameters
-
typeThe type of the event. incrementSpecify the increase in the counter's tally.
| uint16_t emberCounterValueHandler | ( | EmberCounterType |
type
|
) |
The application must define EMBER_APPLICATION_HAS_COUNTER_VALUE_HANDLER in its CONFIGURATION_HEADER to use this.
- Parameters
-
typeThe type of the event.
- Returns
- The counter's tally.
| void emberCustomHostToNcpMessageHandler | ( | const uint8_t * |
message,
|
| uint16_t |
messageLength
|
||
| ) |
- Parameters
-
messagemessage received messageLengthlength of message
| void emberCustomNcpToHostMessageHandler | ( | const uint8_t * |
message,
|
| uint16_t |
messageLength
|
||
| ) |
- Parameters
-
messagemessage received messageLengthlength of message
| void emberDhcpServerChangeHandler | ( | const uint8_t * |
prefix,
|
| uint8_t |
prefixLengthInBits,
|
||
| bool |
available
|
||
| ) |
This function is called when the stack knows about a new dhcp server or if a dhcp server has become unavailable.
"available" means the DHCP server can offer us an address if requested.
- Parameters
-
prefixdhcp server prefix prefixLengthInBitslength in bits of the prefix availablewhether this dhcp server is available
| void emberDtlsSecureSessionEstablished | ( | uint8_t |
flags,
|
| uint8_t |
sessionId,
|
||
| const EmberIpv6Address * |
localAddress,
|
||
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
- Parameters
-
flags1 = server, 0 = client (possibly other info later) sessionIdsessionId used for secure CoAP transport localAddresslocal IPv6 address remoteAddressremote IPv6 address localPortlocal port remotePortremote port
| void emberEnergyScanHandler | ( | uint8_t |
channel,
|
| int8_t |
maxRssiValue
|
||
| ) |
This function reports the maximum RSSI value measured on the channel.
- Parameters
-
channelThe 802.15.4 channel on which the RSSI value was measured. maxRssiValueThe maximum RSSI value measured (in units of dBm).
| void emberEventDelayUpdatedFromIsrHandler | ( | Event * |
event
|
) |
- Parameters
-
eventThe event that was scheduled by the ISR.
| void emberExternalRouteChangeHandler | ( | const uint8_t * |
prefix,
|
| uint8_t |
prefixLengthInBits,
|
||
| bool |
available
|
||
| ) |
This function is called when the stack knows about a border router that has an external route to a prefix.
- Parameters
-
prefixexternal route prefix prefixLengthInBitslength in bits of the prefix availablewhether this external route is available.
| void emberForceTxAfterFailedCcaReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberForceTxAfterFailedCca .
- Parameters
-
statusEMBER_BAD_ARGUMENT if csmaAttempts is out of range, EMBER_SUCCESS otherwise.
| void emberFormNetworkReturn | ( | EmberStatus |
status
|
) |
| void emberGetAntennaModeReturn | ( | EmberStatus |
status,
|
| uint8_t |
mode
|
||
| ) |
This function provides the result of a call to emberGetAntennaMode .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure. modethe current antenna mode 0-don't alter antenna selection, 1-antenna 1, 2-antenna 2, 3-TX antenna diversity
| void emberGetAntennaRxModeReturn | ( | EmberStatus |
status,
|
| uint8_t |
mode
|
||
| ) |
This function provides the result of a call to emberGetAntennaRxMode .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure. modethe current RX antenna mode 0-don't alter antenna selection, 1-antenna 1, 2-antenna 2, 3-RX antenna diversity
| void emberGetCcaThresholdReturn | ( | int8_t |
threshold
|
) |
This function provides the result of a call to emberGetCcaThreshold() .
| void emberGetChannelCalDataTokenReturn | ( | uint8_t |
lna,
|
| int8_t |
tempAtLna,
|
||
| uint8_t |
modDac,
|
||
| int8_t |
tempAtModDac
|
||
| ) |
This function gets the token information for tokenId = EMBER_CHANNEL_CAL_DATA_TOKEN.
- Parameters
-
lna[msb: cal needed? | bit 0-5: lna tune value] tempAtLna[the temp (degC) when the LNA was calibrated] #param modDac [msb: cal needed? | bit 0-5: modulation DAC tune value] tempAtModDac[the temp (degC) when the mod DAC was calibrated]
| void emberGetChildEntryReturn | ( | uint8_t |
status,
|
| uint8_t |
index,
|
||
| uint8_t |
childTableSize,
|
||
| const EmberChildEntry * |
entry,
|
||
| const EmberIpv6Address * |
addresses,
|
||
| uint8_t |
addressCount
|
||
| ) |
If the child is not a Full Thread Device (as indicated in the EmberChildEntry flags field), the parent stores the child's ipv6 addresses, which are then returned by this callback as well.
A status of EMBER_GET_CHILD_ENTRY_FAILURE indicates that no valid child entry was found at or above the requested index.
| void emberGetCounterReturn | ( | EmberCounterType |
type,
|
| uint16_t |
value
|
||
| ) |
This function provides the result of a call to emberGetCounter() .
| void emberGetCtuneReturn | ( | uint16_t |
tune,
|
| EmberStatus |
status
|
||
| ) |
This function provides the result of a call to emberGetCtune .
- Parameters
-
tuneThe current CTUNE value. statusAn EmberStatus value indicating success or the reason for failure.
| void emberGetGlobalAddressReturn | ( | const EmberIpv6Address * |
address,
|
| uint32_t |
preferredLifetime,
|
||
| uint32_t |
validLifetime,
|
||
| uint8_t |
addressFlags
|
||
| ) |
This function provides the result of a call to emberGetGlobalAddresses .
- Parameters
-
addressIPv6 global address preferredLifetimePreferred lifetime (in seconds) validLifetimeValid lifetime (in seconds) addressFlagsAddress configuration flags (EMBER_GLOBAL_ADDRESS_*)
| void emberGetGlobalPrefixReturn | ( | uint8_t |
flags,
|
| bool |
isStable,
|
||
| const uint8_t * |
prefix,
|
||
| uint8_t |
prefixLengthInBits,
|
||
| uint8_t |
domainId,
|
||
| uint32_t |
preferredLifetime,
|
||
| uint32_t |
validLifetime
|
||
| ) |
This function provides the result of a call to ::emberGetGlobalPrefix.
- Parameters
-
flagsPlease ignore this param, it is currently unused. (returns 0) isStableStable or temporary prefix prefixBorder router prefix prefixLengthInBitsPrefix length in bits domainIdProvisioning domain ID preferredLifetimePreferred lifetime (in seconds) validLifetimeValid lifetime (in seconds)
| void emberGetMfgTokenReturn | ( | EmberMfgTokenId |
tokenId,
|
| EmberStatus |
status,
|
||
| const uint8_t * |
tokenData,
|
||
| uint8_t |
tokenDataLength
|
||
| ) |
This function provides the result of a call to emberGetMfgToken .
- Parameters
-
tokenIdWhich manufacturing token read. statusAn EmberStatus value indicating success or the tokenDataThe manufacturing token data. tokenDataLengthThe length of the tokenData parameter in bytes.
| void emberGetNetworkDataReturn | ( | EmberStatus |
status,
|
| uint8_t * |
networkData,
|
||
| uint16_t |
bufferLength
|
||
| ) |
This function provides the result of a call to emberGetNetworkData .
The status value is one of:
- EMBER_SUCCESS
- EMBER_NETWORK_DOWN
- EMBER_BAD_ARGUMENT (the supplied buffer was too small)
- Parameters
-
statusnetworkDatalocation of the Network Data dataLengthlength in bytes of the Network Data
| void emberGetNetworkDataTlvReturn | ( | uint8_t |
typeByte,
|
| uint8_t |
index,
|
||
| uint8_t |
versionNumber,
|
||
| const uint8_t * |
tlv,
|
||
| uint8_t |
tlvLength
|
||
| ) |
This function provides the result of a call to emberGetNetworkDataTlv() .
- Parameters
-
typethe type of TLV returned. This is the same value as the value specified in the emberGetNetworkDataTlv() call. indexthe instance number of the TLV. This is the same value as the value specified in the emberGetNetworkDataTlv() call. versionNumberthe network data version tlvthe TLV corresponding to type or NULL. tlvLengthlength of tlv
| void emberGetParentPriorityReturn | ( | const int8_t |
parentPriority
|
) |
In a host/NCP setup, provides the result of a call to emberGetParentPriority() on the host.
- Parameters
-
parentPriorityParent Priority
| void emberGetPtaDirectionalPriorityPulseWidthReturn | ( | uint8_t |
pulseWidthUs
|
) |
This function provides the result of a call to emberGetPtaDirectionalPriorityPulseWidth . (Only valid on EFR32)
- Parameters
-
pulseWidthUsDirectional priority pulse width in microseconds
| void emberGetPtaEnableReturn | ( | bool |
enabled
|
) |
This function provides the result of a call to emberGetPtaEnable .
- Parameters
-
enabledWhen true, indicates packet traffic arbitration is enabed. When false, indicates packet traffic arbitration is disabled.
| void emberGetPtaOptionsReturn | ( | uint32_t |
options
|
) |
This function provides the result of a call to emberGetPtaOptions .
- Parameters
-
indicatespacket traffic arbitration options bit field. Field Bit Position Size(bits) RX retry timeout ms 0 8 Enable ack radio holdoff 8 1 Abort mid TX if grant is lost 9 1 TX request is high priority 10 1 RX request is high prioirity 11 1 RX retry request is high priority 12 1 RX retry request is enabled 13 1 Radio holdoff is enabled 14 1 Toggle request on mac retransmit 15 1 Force holdoff by disabling request 16 1 Hold off transmit in the mac layer 17 1 Delay asserting request until 18 1 address filtering passes Assert request with high priority 19 1 after address filtering passes CCA failure counter threshold 20 3 MAC retry counter threshold 23 2 MAC failure counter threshold 25 2 Reserved 27 4 Hold request across CCA failures 31 1
| void emberGetPtaPhySelectTimeoutReturn | ( | uint8_t |
timeoutMs
|
) |
This function provides the result of a call to emberGetPtaPhySelectTimeout . (Only valid on EFR32)
- Parameters
-
timeoutMsPacket traffic arbitration PHY select timeout in milliseconds.
| void emberGetPtaPwmOptionsReturn | ( | uint8_t |
request,
|
| uint8_t |
dutyCycle,
|
||
| uint8_t |
periodHalfMs
|
||
| ) |
- Parameters
-
requestPTA PWM bit field Field Bit Position Size(bits) Request enabled 0 1 Priority enabled 1 1 dutyCyclePTA PWM duty cycle percentage(0-100) periodHalfMsPTA PWM request period in half milliseconds
| void emberGetRadioPowerReturn | ( | int8_t |
power
|
) |
This function provides the result of a call to emberGetRadioPower() on the host.
| void emberGetRipEntryReturn | ( | uint8_t |
index,
|
| const EmberRipEntry * |
entry
|
||
| ) |
This function provides the result of a call to emberGetRipEntry() .
| void emberGetRoutingLocatorReturn | ( | const EmberIpv6Address * |
rloc
|
) |
This function provides the result of a call to emberGetRoutingLocator .
- Parameters
-
rlocThe Routing Locator as a full IPv6 address.
| void emberGetStandaloneBootloaderInfoReturn | ( | uint16_t |
version,
|
| uint8_t |
platformId,
|
||
| uint8_t |
microId,
|
||
| uint8_t |
phyId
|
||
| ) |
This function provides the result of a call to emberGetStandaloneBootloaderInfo .
- Parameters
-
versionBOOTLOADER_INVALID_VERSION if the standalone bootloader is not present, or the version of the installed standalone bootloader. platformIdThe value of PLAT on the node. microIdThe value of MICRO on the node. phyIdThe value of PHY on the node.
| void emberGetTxPowerModeReturn | ( | uint16_t |
txPowerMode
|
) |
This function provides the result of a call to emberGetTxPowerMode() on the host.
- Returns
- the current tx power mode.
| void emberGetVersionsReturn | ( | const uint8_t * |
versionName,
|
| uint16_t |
managementVersionNumber,
|
||
| uint16_t |
stackVersionNumber,
|
||
| uint16_t |
stackBuildNumber,
|
||
| EmberVersionType |
versionType,
|
||
| const uint8_t * |
buildTimestamp
|
||
| ) |
| void emberHostStateHandler | ( | const EmberNetworkParameters * |
parameters,
|
| const EmberEui64 * |
localEui64,
|
||
| const EmberEui64 * |
macExtendedId,
|
||
| EmberNetworkStatus |
networkStatus
|
||
| ) |
- Parameters
-
parametersCurrent network parameters localEui64The EUI64 of the Ember chip macExtendedIdThe extended MAC ID of the Ember chip networkStatusThe current status of the network
| void emberInitiateLinkMetricsProbingReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSendLinkMetricsProbing().
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberInitReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberInit() .
| void emberJoinNetworkReturn | ( | EmberStatus |
status
|
) |
| void emberLaunchStandaloneBootloaderReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberLaunchStandaloneBootloader .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberLeaderDataHandler | ( | const uint8_t * |
leaderData
|
) |
The format of the leader data is as follows (Thread spec section 4.5.12):
| octets: | 4 | 1 | 1 | 1 | 1 |
| | Partition ID | Weight | Data Ver. | Stable Data Ver. | Router ID |
- Parameters
-
leaderDatathe leader data
| void emberLinkMetricsMgmtHandler | ( | EmberLinkMetricsStatus |
status,
|
| const uint8_t * |
remoteAddress
|
||
| ) |
This function is called when the Probing Initiator gets an MLE Link Management Response message.
- Parameters
-
statuslink metrics request status remoteAddressIPv6 address of the subject
| void emberLinkMetricsResponseHandler | ( | EmberLinkMetricsStatus |
status,
|
| const uint8_t * |
remoteAddress,
|
||
| const uint8_t * |
reportTlvValue,
|
||
| uint8_t |
reportTlvLength
|
||
| ) |
This function is called when a Probing Initiator gets an MLE Data Response message in response to an MLE Data Request Message making a Link Metrics Query.
- Parameters
-
statuslink metrics status remoteAddressIPv6 address of the subject reportTlvValueLink Metrics Report TLV Value field (Applicable only when status is Success(0), NULL otherwise) reportTlvLengthLink Metrics Report TLV Length field (Applicable only when status is Success(0), 0 otherwise)
| bool emberMacPassthroughFilterHandler | ( | uint8_t * |
macHeader
|
) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_MAC_PASSTHROUGH_FILTER_HANDLER
- Parameters
-
macHeaderA pointer to the initial portion of the incoming MAC header, in the standard 802.15.4 format. The first two bytes comprise the frame control, which dictates source / destination PAN and addressing formats. (See the MAC sublayer definition in the standards definition 802.15.4e/2012)
The relevant bytes of the header are:
| octets: | 2 | 1 | 0/2 | 0/2/8 | 0/2 | 0/2/8 |
| | ctl | seq | dst.pan | dst.addr | src.pan | src.addr | ...
Note that subsequent MAC fields, and the MAC payload, may not yet be present at this point.
- Returns
- true if the message is an application MAC passthrough message.
| void emberMacPassthroughMessageHandler | ( | PacketHeader |
header
|
) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_MAC_PASSTHROUGH_MESSAGE_HANDLER
- Parameters
-
headerThe message buffer pointing to the full 802.15.4 frame to be handled by the application.
| bool emberMacRssiFilterHandler | ( | uint8_t * |
macHeader
|
) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_RSSI_FILTER_HANDLER
- Parameters
-
macHeaderA pointer to the initial portion of the incoming MAC header, in the standard 802.15.4 format. The first two bytes comprise the frame control, which dictates source / destination PAN and addressing formats. (See the MAC sublayer definition in the standards definition 802.15.4e/2012)
The relevant bytes of the header are:
| octets: | 2 | 1 | 0/2 | 0/2/8 | 0/2 | 0/2/8 |
| | ctl | seq | dst.pan | dst.addr | src.pan | src.addr | ...
Note that subsequent MAC fields, and the MAC payload, may not yet be present at this point.
- Returns
- true if the application wants to peek at the RSSI for this message.
| void emberMacRssiHandler | ( | int8_t |
currentRssi
|
) |
- Note
- This is called on the application for all packets that match the rule defined in emberMacRssiFilterHandler()
The quantity referenced by currentRssi will contain the energy level (in units of dBm) observed during the last 802.15.4 packet received in that handler.
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_RSSI_FILTER_HANDLER
- This functionality is not available for packets such as 802.15.4 data requests or acknowledgements. Data requests must be handled quickly due to strict 15.4 timing requirements, and so the RSSI information is not recorded. Similarly, 802.15.4 ACKs are handled by the hardware and the information does not make it up to the stack.
- Parameters
-
currentRssiThe RSSI for the last incoming message processed.
| void emberMicroBusyHandler | ( | bool |
busy
|
) |
This callback is not available on a host processor. Note that if ::busy is true, the micro may become busy as soon as this handler exits. In a host/ncp setup, one solution for informing the host is to implement this handler in your own xNCP image and use it to toggle the serial CTS line.
| void emberMulticastListenerHandler | ( | const EmberIpv6Address * |
multicastGroupAddress
|
) |
The off-mesh multicasts are sent to the Thread network in MPL packets, via IPv6-in-IPv6 encapsulation.
On a BBR, this handler can be used to configure the multicast groups on the backbone link. The application must use MLDv2 to communicate to the wider IPv6 LAN/WAN about the groups it needs to listen to.
- Parameters
-
multicastGroupAddressIPv6 address representing the multicast group
| void emberNetworkDataChangeHandler | ( | const uint8_t * |
networkData,
|
| uint16_t |
length
|
||
| ) |
This function is called when the stack receives new Thread Network Data. The networkData argument may be NULL, in which case emberGetNetworkData can be used to obtain the new Thread Network Data.
- Parameters
-
networkDatathe Network Data lengthlength in bytes of the Network Data
| void emberNetworkStatusHandler | ( | EmberNetworkStatus |
newNetworkStatus,
|
| EmberNetworkStatus |
oldNetworkStatus,
|
||
| EmberJoinFailureReason |
reason
|
||
| ) |
This function reports a change to the network status. For example, the network status changes while going through the joining process, or while reattaching to the network, which can happen for a variety of reasons. In particular, after issuing a form, join, resume, or attach command, the application knows that the device is on the network and ready to communicate when this handler is called with a newNetworkStatus of EMBER_JOINED_NETWORK_ATTACHED.
If the status handler is reporting a join failure, then the newNetworkStatus argument will have a value of EMBER_NO_NETWORK and the reason argument will contain an appropriate value. For other network status reports, the reason argument does not apply and is set to EMBER_JOIN_FAILURE_REASON_NONE.
| void emberOkToNapReturn | ( | uint8_t |
stateMask
|
) |
The mask EMBER_HIGH_PRIORITY_TASKS defines which tasks are high priority. Devices should not sleep if any high priority tasks are active. Active tasks that are not high priority are waiting for messages to arrive from other devices. If there are active tasks, but no high priority ones, the device may sleep but should periodically wake up and call emberPollForData() in order to receive messages. Parents will hold messages for EMBER_INDIRECT_TRANSMISSION_TIMEOUT (in quarter seconds) before discarding them.
- Returns
- A bitmask of the stack's active tasks.
| void emberOpenDtlsConnectionReturn | ( | uint32_t |
result,
|
| const EmberIpv6Address * |
remoteAddress,
|
||
| uint16_t |
localPort,
|
||
| uint16_t |
remotePort
|
||
| ) |
- Parameters
-
resulterror code - an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
remoteAddressIPv6 address of the server localPortlocal port remotePortremote port
| void emberPollForDataReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberPollForData() .
- Parameters
-
AnEmberStatus value: - EMBER_SUCCESS - The poll message has been submitted for transmission
- EMBER_INVALID_CALL - The node is not a sleepy end device.
- EMBER_NOT_JOINED - The node is not part of a network.
| void emberProcessCoap | ( | const uint8_t * |
message,
|
| uint16_t |
messageLength,
|
||
| EmberCoapRequestInfo * |
info
|
||
| ) |
This function processes a CoAP message received over an alternate transport.
Called to process a CoAP message that arrived via DTLS or other alternative transport. Only the address, port and transmit handler fields of
info
are used. The token and ackData fields are ignored.
| void emberRadioGetRandomNumbersReturn | ( | EmberStatus |
status,
|
| const uint16_t * |
rn,
|
||
| uint8_t |
count
|
||
| ) |
This function provides the result of a call to emberRadioGetRandomNumbers .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure. When EMBER_SUCCESS is returned ::rn and ::count will contain valid data. ::rn and ::count are undefined when EMBER_SUCCESS is not returned. rnthe uint16_t random values count- the count of uint16_t values located at ::rn
| void emberRemoveMeshDuaEntryReturn | ( | EmberStatus |
status,
|
| const EmberIpv6Address * |
dua
|
||
| ) |
- Parameters
-
statusEMBER_SUCCESS or EMBER_BAD_ARGUMENT
| void emberRequestDhcpAddressReturn | ( | EmberStatus |
status,
|
| const uint8_t * |
prefix,
|
||
| uint8_t |
prefixLengthInBits
|
||
| ) |
This function provides the result of a call to emberRequestDhcpAddress .
This call only indicates the status of the request (EMBER_ERR_FATAL if no DHCP server is found, and EMBER_SUCCESS otherwise). The assigned IPv6 address is returned via emberAddressConfigurationChangeHandler
- Parameters
-
statusStatus of DHCP Address Request prefixPrefix requested in emberRequestDhcpAddress prefixLengthInBitsPrefix length in bits requested in emberRequestDhcpAddress
| void emberRequestDomainUniqueAddressReturn | ( | EmberStatus |
status,
|
| const uint8_t * |
prefix,
|
||
| uint8_t |
prefixLengthInBits
|
||
| ) |
This call only indicates the status of the request (EMBER_ERR_FATAL if no PBBR is found, and EMBER_SUCCESS otherwise). The assigned IPv6 address is returned via emberAddressConfigurationChangeHandler
- Parameters
-
statusStatus of DUA Request prefixPrefix requested in emberRequestDomainUniqueAddress prefixLengthInBitsPrefix length in bits requested in emberRequestDomainUniqueAddress
| void emberRequestMulticastListenerReturn | ( | EmberStatus |
status,
|
| const EmberIpv6Address * |
address
|
||
| ) |
- Parameters
-
statusStatus of MLR Request multicastGroupAddressIPv6 address representing the multicast group
| void emberRequestSlaacAddressReturn | ( | EmberStatus |
status,
|
| const uint8_t * |
prefix,
|
||
| uint8_t |
prefixLengthInBits
|
||
| ) |
This function provides the result of a call to emberRequestSlaacAddress .
This call only indicates the status of the request (EMBER_ERR_FATAL if no SLAAC server is found, and EMBER_SUCCESS otherwise). The assigned IPv6 address is returned via emberAddressConfigurationChangeHandler
- Parameters
-
statusStatus of SLAAC Address Request prefixPrefix requested in emberRequestSlaacAddress prefixLengthInBitsPrefix length in bits requested in emberRequestSlaacAddress
| void emberResetCounterHandler | ( | EmberCounterType |
type
|
) |
The application must define EMBER_APPLICATION_HAS_COUNTER_VALUE_HANDLER in its CONFIGURATION_HEADER to use this.
- Parameters
-
typeThe type of the event.
| void emberResetMicroHandler | ( | EmberResetCause |
cause
|
) |
This function notifies the application of a reset on the Ember chip due to the indicated cause.
| void emberResetNetworkStateReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberResetNetworkState() .
| void emberResignGlobalAddressReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberResignGlobalAddress() .
| void emberResumeNetworkReturn | ( | EmberStatus |
status
|
) |
| void emberScanReturn | ( | EmberStatus |
status
|
) |
This function provides the status upon completion of a scan.
| void emberSendLinkMetricsQueryReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSendLinkMetricsQuery() .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSendLinkProbeMessagesReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSendLinkProbeMessages() .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSendSteeringDataReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSendSteeringData() .
| void emberSetAddressHandler | ( | const uint8_t * |
address
|
) |
A callback that is generated when the host's address changes.
- Parameters
-
addressIP address, 16 bytes
| void emberSetAntennaModeReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetAntennaMode .
- Parameters
-
EMBER_SUCCESSif antenna mode is configured as desired or EMBER_BAD_ARGUMENT if antenna mode is not supported.
| void emberSetAntennaRxModeReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetAntennaRxMode .
- Parameters
-
EMBER_SUCCESSif RX antenna mode is configured as desired or EMBER_BAD_ARGUMENT if RX antenna mode is not supported.
| void emberSetBbrDatasetReturn | ( | EmberStatus |
status
|
) |
- Parameters
-
statusEMBER_SUCCESS
| void emberSetCcaThresholdReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetCcaThreshold() .
| void emberSetCommissionerKeyReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetCommissionerKey() : either EMBER_SUCCESS or EMBER_INVALID_CALL.
| void emberSetCtuneReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetCtune .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetDtlsDeviceCertificateReturn | ( | uint32_t |
result
|
) |
- Parameters
-
result- ::0 The certificate was set successfully.
-
::result error code
- an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
| void emberSetDtlsPresharedKeyReturn | ( | EmberStatus |
status
|
) |
- Parameters
-
result- ::status An EmberStatus value
| void emberSetJoinKeyReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetJoinKey() .
| void emberSetLocalNetworkDataReturn | ( | EmberStatus |
status,
|
| uint16_t |
length
|
||
| ) |
Provides the result of a call to ::emberSetServerNetworkData.
| void emberSetMfgTokenReturn | ( | EmberMfgTokenId |
tokenId,
|
| EmberStatus |
status
|
||
| ) |
This function provides the result of a call to emberSetMfgToken .
- Parameters
-
tokenIdWhich manufacturing token set. statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetNdDataReturn | ( | EmberStatus |
status,
|
| uint16_t |
length
|
||
| ) |
This function provides the result of a call to emberSetNdData .
| void emberSetParentPriorityReturn | ( | EmberStatus |
status
|
) |
A callback to indicate if the call to emberSetParentPriority() was successful.
| void emberSetPskcHandler | ( | const uint8_t * |
pskc
|
) |
- Parameters
-
pskcPSKc: 16 bytes in length
| void emberSetPtaDirectionalPriorityPulseWidthReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetPtaDirectionalPriorityPulseWidth . (Only valid on EFR32)
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetPtaEnableReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetPtaEnable .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetPtaOptionsReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetPtaOptions .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetPtaPhySelectTimeoutReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetPtaPhySelectTimeout . (Only valid on EFR32)
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetPtaPwmOptionsReturn | ( | EmberStatus |
status
|
) |
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure.
| void emberSetRadioHoldOffReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetRadioHoldOff .
- Parameters
-
statusAn EmberStatus value indicating success or the reason for failure. EMBER_SUCCESS if Radio HoldOff was configured as desired or EMBER_BAD_ARGUMENT if requesting it be enabled but RHO has not been configured by the BOARD_HEADER.
| void emberSetRadioPowerReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetRadioPower() on the host.
| void emberSetSecurityParametersReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetSecurityParameters() .
| void emberSetTxPowerModeReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSetTxPowerMode() on the host.
| void emberSlaacServerChangeHandler | ( | const uint8_t * |
prefix,
|
| uint8_t |
prefixLengthInBits,
|
||
| bool |
available
|
||
| ) |
This function is called when the stack knows about a new SLAAC prefix or if a SLAAC server has become unavailable.
"available" means we can configure a SLAAC address.
- Parameters
-
prefixSLAAC prefix prefixLengthInBitslength in bits of the prefix availablewhether we can configure an address
| void emberStackPollForDataReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberStackPollForData() .
| void emberStartHostJoinClientHandler | ( | const uint8_t * |
parentAddress
|
) |
A callback to tell the host to start security commissioning.
- Parameters
-
addressparent IP address, 16 bytes
| void emberStateReturn | ( | const EmberNetworkParameters * |
parameters,
|
| const EmberEui64 * |
localEui64,
|
||
| const EmberEui64 * |
macExtendedId,
|
||
| EmberNetworkStatus |
networkStatus
|
||
| ) |
- Parameters
-
parametersCurrent network parameters localEui64The EUI64 of the Ember chip macExtendedIdThe extended MAC ID of the Ember chip networkStatusThe current status of the network
| void emberSwitchToNextNetworkKeyHandler | ( | EmberStatus |
status
|
) |
This function can be stubbed out on the SoC and host app. It is used by the NCP to update security on the driver when it is instructed to switch the network key by an over the air update.
| void emberSwitchToNextNetworkKeyReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberSwitchToNextNetworkKey() .