Functions

bool emberZclClusterTimeServerInitCallback ( EmberZclEndpointId_t endpointId)
Initialises the Time Server.
bool emberZclClusterTimeServerTickCallback ( EmberZclEndpointId_t endpointId)
Handle the Time Server tick.
uint32_t emberZclClusterTimeServerGetCurrentTimeCallback (void)
Calls the user to get the real time.

Detailed Description

These callbacks are contributed by the Time Server plugin.

Function Documentation

uint32_t emberZclClusterTimeServerGetCurrentTimeCallback ( void )

The user is able to provide the real time to the server through this call back.

bool emberZclClusterTimeServerInitCallback ( EmberZclEndpointId_t endpointId )

This function is called from the time server during its initialisation.

Parameters
endpointId The endpoint that holds the time server Ver.: always
Returns
FALSE if the application is not handling the Time Server initialisation.

References FALSE .

bool emberZclClusterTimeServerTickCallback ( EmberZclEndpointId_t endpointId )

This function is called when the Time Server tick event expires.

Parameters
endpointId The endpoint that holds the time server Ver.: always
Returns
FALSE if the application is not handling the Time Server tick.

References FALSE .