EmberZclGroupEntry_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields |
|
| EmberZclGroupId_t | groupId |
| EmberZclEndpointId_t | endpointId |
| uint8_t | groupNameLength |
| uint8_t | addrAssignmentMode |
| EmberIpv6Address | groupMcastAddress |
| uint16_t | groupUdpPort |
This structure holds a group entry that represents membership of an endpoint in a group.
Field Documentation
| uint8_t EmberZclGroupEntry_t::addrAssignmentMode |
An array containing group name. Save space Address assignment mode as passed in "add group" command or 0xFF if address is not assigned
| EmberZclEndpointId_t EmberZclGroupEntry_t::endpointId |
An endpoint identifier of a group entry.
| EmberZclGroupId_t EmberZclGroupEntry_t::groupId |
A group identifier of a group entry.
| EmberIpv6Address EmberZclGroupEntry_t::groupMcastAddress |
Group IPv6 address or flag/scope bits from "add group" command
| uint8_t EmberZclGroupEntry_t::groupNameLength |
Length of group name.
| uint16_t EmberZclGroupEntry_t::groupUdpPort |
UDP port the group is listening on: EMBER_COAP_PORT or whatever was passed in "add group"
The documentation for this struct was generated from the following file:
-
zcl-core-types.h