EmberMacBeaconData Struct Reference
Structure to hold information about an 802.15.4 beacon for use on the application.
#include <
network-management.h
>
Data Fields |
|
| uint8_t | networkId [16] |
| uint8_t | extendedPanId [8] |
| uint8_t | macExtendedId [8] |
| uint16_t | panId |
| uint8_t | protocolId |
| uint8_t | channel |
| bool | allowingJoin |
| uint8_t | lqi |
| int8_t | rssi |
| uint8_t | version |
| uint16_t | shortId |
| uint8_t | steeringData [16] |
| uint8_t | steeringDataLength |
The documentation for this struct was generated from the following file:
-
network-management.h