Functions

void emberZclIdentifyServerStartIdentifyingCallback ( EmberZclEndpointId_t endpointId, uint16_t identifyTimeS)
Start Identifying.
void emberZclIdentifyServerStopIdentifyingCallback ( EmberZclEndpointId_t endpointId)
Stop Identifying.

Detailed Description

These callbacks are contributed by the Identify Server plugin.

Function Documentation

void emberZclIdentifyServerStartIdentifyingCallback ( EmberZclEndpointId_t endpointId,
uint16_t identifyTimeS
)

This function is called when the device should start identifying. The device should continue to identify until emberZclIdentifyServerStopIdentifyingCallback is called.

void emberZclIdentifyServerStopIdentifyingCallback ( EmberZclEndpointId_t endpointId )

This function is called when the device should stop identifying.