USB_DeviceDescriptor_TypeDef Struct Reference
USB Device Descriptor.
#include <
em_usb.h
>
Data Fields | |
uint8_t | bLength |
uint8_t | bDescriptorType |
uint16_t | bcdUSB |
uint8_t | bDeviceClass |
uint8_t | bDeviceSubClass |
uint8_t | bDeviceProtocol |
uint8_t | bMaxPacketSize0 |
uint16_t | idVendor |
uint16_t | idProduct |
uint16_t | bcdDevice |
uint8_t | iManufacturer |
uint8_t | iProduct |
uint8_t | iSerialNumber |
uint8_t | bNumConfigurations |
Field Documentation
uint16_t USB_DeviceDescriptor_TypeDef::bcdDevice |
Device release number in binary-coded decimal
uint16_t USB_DeviceDescriptor_TypeDef::bcdUSB |
USB Specification Release Number in Binary-Coded Decimal
uint8_t USB_DeviceDescriptor_TypeDef::bDescriptorType |
Constant DEVICE Descriptor Type
uint8_t USB_DeviceDescriptor_TypeDef::bDeviceClass |
Class code (assigned by the USB-IF)
uint8_t USB_DeviceDescriptor_TypeDef::bDeviceProtocol |
Protocol code (assigned by the USB-IF)
uint8_t USB_DeviceDescriptor_TypeDef::bDeviceSubClass |
Subclass code (assigned by the USB-IF)
uint8_t USB_DeviceDescriptor_TypeDef::bLength |
Size of this descriptor in bytes
uint8_t USB_DeviceDescriptor_TypeDef::bMaxPacketSize0 |
Maximum packet size for endpoint zero
uint8_t USB_DeviceDescriptor_TypeDef::bNumConfigurations |
Number of possible configurations
uint16_t USB_DeviceDescriptor_TypeDef::idProduct |
Product ID (assigned by the manufacturer)
uint16_t USB_DeviceDescriptor_TypeDef::idVendor |
Vendor ID (assigned by the USB-IF)
uint8_t USB_DeviceDescriptor_TypeDef::iManufacturer |
Index of string descriptor describing manufacturer
uint8_t USB_DeviceDescriptor_TypeDef::iProduct |
Index of string descriptor describing product
uint8_t USB_DeviceDescriptor_TypeDef::iSerialNumber |
Index of string descriptor describing the device serialnumber
The documentation for this struct was generated from the following file:
em_usb.h