EmberCommissionData Struct Reference

#include < network-diagnostics.h >

Data Fields

uint32_t tlvMask
const uint8_t * provisioningUrl
const uint8_t * vendorName
const uint8_t * vendorModel
const uint8_t * swVersion
const uint8_t * vendorData
const uint8_t * vendorStackVersion

Field Documentation

const uint8_t* EmberCommissionData::provisioningUrl
const uint8_t* EmberCommissionData::swVersion
uint32_t EmberCommissionData::tlvMask
const uint8_t* EmberCommissionData::vendorData
const uint8_t* EmberCommissionData::vendorModel
const uint8_t* EmberCommissionData::vendorName
const uint8_t* EmberCommissionData::vendorStackVersion

The documentation for this struct was generated from the following file:
  • network-diagnostics.h