OTA Bootload Server Callbacks
Functions | |
bool | emberZclOtaBootloadServerGetImageNotifyInfoCallback (EmberIpv6Address *address, EmberZclOtaBootloadFileSpec_t *fileSpec) |
EmberZclStatus_t | emberZclOtaBootloadServerGetNextImageCallback (const EmberIpv6Address *source, const EmberZclOtaBootloadFileSpec_t *currentFileSpec, EmberZclOtaBootloadFileSpec_t *nextFileSpec) |
uint32_t | emberZclOtaBootloadServerUpgradeEndRequestCallback (const EmberIpv6Address *source, const EmberZclOtaBootloadFileSpec_t *fileSpec, EmberZclStatus_t status) |
Detailed Description
These callbacks are contributed by the OTA Bootload Server plugin.
Function Documentation
bool emberZclOtaBootloadServerGetImageNotifyInfoCallback | ( | EmberIpv6Address * | address, |
EmberZclOtaBootloadFileSpec_t * | fileSpec |
||
) |
Get the information needed to send an ImageNotify command.
- Parameters
-
address
Address to which to send the ImageNotify command fileSpec
The OTA file specification data contained in the ImageNotify command payload. See OTA specification for more details.
- Returns
true
if the ImageNotify command should be sent,false
otherwise.
- Note
- If
false
is returned, then the ImageNotify command will be rescheduled to be sent at a later time.
EmberZclStatus_t emberZclOtaBootloadServerGetNextImageCallback | ( | const EmberIpv6Address * | source, |
const EmberZclOtaBootloadFileSpec_t * | currentFileSpec, |
||
EmberZclOtaBootloadFileSpec_t * | nextFileSpec |
||
) |
Get the next OTA file to send in response to a QueryNextImage command.
- Parameters
-
currentFileSpec
The current file spec from the QueryNextImage command nextFileSpec
The next file spec to be downloaded by the client
- Returns
- One of the following EmberZclStatus_t values.
- EMBER_ZCL_STATUS_SUCCESS if the server should tell the client to start downloading the OTA file described by the nextFileSpec data
- EMBER_ZCL_STATUS_NO_IMAGE_AVAILABLE if there is no image available for the client to download
- EMBER_ZCL_STATUS_NOT_AUTHORIZED if the client is not authorized to download the next image
References EMBER_ZCL_STATUS_NO_IMAGE_AVAILABLE.
uint32_t emberZclOtaBootloadServerUpgradeEndRequestCallback | ( | const EmberIpv6Address * | source, |
const EmberZclOtaBootloadFileSpec_t * | fileSpec, |
||
EmberZclStatus_t | status |
||
) |
Get the status to send to an OTA client after a download has completed.
- Parameters
-
source
The source address of the OTA client that has completed a download fileSpec
The file specification of the OTA file that the client has downloaded status
The status reported by the client upon completing the download
- Returns
- The time at which the client should upgrade to the newly downloaded image.
- Note
- This callback is called regardless of whether or not the client completed the download successfully. If the status parameter is not equal to EMBER_ZCL_STATUS_SUCCESS, then the server will not tell the client to proceed with the upgrade.