Discovery
Enumerations |
|
| enum |
EmberZclDiscoveryRequestMode
{
EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY = 0, EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY = 1, EMBER_ZCL_DISCOVERY_REQUEST_MODE_MAX = 2 } |
Functions |
|
| void | emberZclDiscInit (void) |
| bool | emberZclDiscSetMode ( EmberZclDiscoveryRequestMode mode) |
| bool | emberZclDiscSend ( EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscCoreRd ( EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByClusterId (const EmberZclClusterSpec_t *clusterSpec, EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByEndpoint ( EmberZclEndpointId_t endpointId, EmberZclDeviceId_t deviceId, EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByUid (const EmberZclUid_t *uid, uint16_t uidBits, EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByClusterRev ( EmberZclClusterRevision_t version, EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByDeviceId ( EmberZclDeviceId_t deviceId, EmberCoapResponseHandler responseHandler) |
| bool | emberZclDiscByResourceVersion ( EmberZclClusterRevision_t version, EmberCoapResponseHandler responseHandler) |
Detailed Description
See
zcl-core-types.h
for source code.
See
zcl-core-well-known.h
for source code.
Enumeration Type Documentation
Function Documentation
| bool emberZclDiscByClusterId | ( | const EmberZclClusterSpec_t * |
clusterSpec,
|
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends a cluster ID query to the discovery request string.
- Parameters
-
clusterSpecA structure for cluster ID / role / manufacture code responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
Referenced by emberZclOtaBootloadClientServerHasDiscByClusterId() .
| bool emberZclDiscByClusterRev | ( | EmberZclClusterRevision_t |
version,
|
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends a cluster revision query to the discovery request string.
- Parameters
-
versionThe version responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| bool emberZclDiscByDeviceId | ( | EmberZclDeviceId_t |
deviceId,
|
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends a device ID query to the discovery request string.
- Parameters
-
deviceIdThe device identifier responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| bool emberZclDiscByEndpoint | ( | EmberZclEndpointId_t |
endpointId,
|
| EmberZclDeviceId_t |
deviceId,
|
||
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends an endpoint query to the Discovery request string.
- Parameters
-
endpointIdThe endpoint identifier deviceIdThe device identifier responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| bool emberZclDiscByResourceVersion | ( | EmberZclClusterRevision_t |
version,
|
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends a resource version query to the discovery request string.
- Parameters
-
versionThe version responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| bool emberZclDiscByUid | ( | const EmberZclUid_t * |
uid,
|
| uint16_t |
uidBits,
|
||
| EmberCoapResponseHandler |
responseHandler
|
||
| ) |
This function appends a UID query to the discovery request string.
- Parameters
-
uidThe uid uidBitsThe uid bits responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| bool emberZclDiscCoreRd | ( | EmberCoapResponseHandler |
responseHandler
|
) |
This function appends a core.rd query to the discovery request string.
- Parameters
-
responseHandlerThe response handler
- Returns
- in EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode: True if the command was sent or false otherwise. in EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode: True if the command was appended or false otherwise.
| void emberZclDiscInit | ( | void |
|
) |
Initialization for sending Discovery command.
| bool emberZclDiscSend | ( | EmberCoapResponseHandler |
responseHandler
|
) |
This function broadcasts a GET using the Discovery request string.
- Parameters
-
responseHandlerThe response handler
- Returns
- True if the message was sent or false otherwise.
| bool emberZclDiscSetMode | ( | EmberZclDiscoveryRequestMode |
mode
|
) |
This function sets mode to create a query.
- Parameters
-
modeEMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY - single query EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY - multiple queries
- Returns
- True if mode was set or false otherwise.
Under EMBER_ZCL_DISCOVERY_REQUEST_SINGLE_QUERY mode, appending one query string automatically triggers the Discovery command to be broadcast. Under EMBER_ZCL_DISCOVERY_REQUEST_MULTIPLE_QUERY mode, appended query strings is accumulated. The accumulated query string will not be broadcast until emberZclDiscSend() is called.