EmberNetworkDebugParameters Struct Reference
An application structure to hold useful network debug parameters.
#include <
network-management.h
>
Data Fields |
|
| uint8_t | ripId |
| EmberNodeId | nodeId |
| uint8_t | parentRipId |
| EmberNodeId | parentId |
| EmberNodeId | leaderNodeId |
| uint8_t | networkFragmentIdentifier [5] |
| uint32_t | networkFrameCounter |
Meant for use with the ::emberGetNodeStatus debug API. (Access to these parameters is only available with debugging symbols enabled)
. rip id . short id . parent's rip id . parent's short id . network fragment identifier . network frame counter
The documentation for this struct was generated from the following file:
-
network-management.h