USBD_Init_TypeDef Struct Reference
USB Device stack initialization structure.
#include <
em_usb.h
>
Data Fields | |
const USB_DeviceDescriptor_TypeDef * | deviceDescriptor |
const uint8_t * | configDescriptor |
const void *const * | stringDescriptors |
const uint8_t | numberOfStrings |
const uint8_t * | bufferingMultiplier |
USBD_Callbacks_TypeDef_Pointer | callbacks |
const uint32_t | reserved |
This structure is passed to USBD_Init() when starting up the device.
Field Documentation
const uint8_t* USBD_Init_TypeDef::bufferingMultiplier |
Pointer to an array defining the size of the endpoint buffers. The size is given in multiples of endpoint size. Generally a value of 1 (single) or 2 (double) buffering should be used.
Referenced by USBD_Init().
USBD_Callbacks_TypeDef_Pointer USBD_Init_TypeDef::callbacks |
Pointer to struct with callbacks (USBD_Callbacks_TypeDef). These callbacks are used by the device stack to signal events to or query the application.
Referenced by USBD_Init().
const uint8_t* USBD_Init_TypeDef::configDescriptor |
Pointer to a configuration descriptor.
Referenced by USBD_Init().
const USB_DeviceDescriptor_TypeDef* USBD_Init_TypeDef::deviceDescriptor |
Pointer to a device descriptor.
Referenced by USBD_Init().
const uint8_t USBD_Init_TypeDef::numberOfStrings |
Number of strings in string descriptor array.
Referenced by USBD_Init().
const uint32_t USBD_Init_TypeDef::reserved |
Reserved for future use.
const void* const* USBD_Init_TypeDef::stringDescriptors |
Pointer to an array of string descriptor pointers.
Referenced by USBD_Init().
The documentation for this struct was generated from the following file:
em_usb.h