thread-debug API Callbacks
Functions |
|
| void | emberAssertInfoReturn (const uint8_t *fileName, uint32_t lineNumber) |
|
Callback for a debug command. Provides the result of ::emberAssertInfo.
|
|
| void | emberConfigUartReturn (void) |
|
Callback for a debug command. Provides the result of ::emberConfigUart.
|
|
| void | emberEchoReturn (const uint8_t *data, uint8_t length) |
|
Callback for a debug command. Provides the result of
emberEcho
.
|
|
| void | emberGetMulticastEntryReturn (uint8_t lastSequence, uint8_t windowBitmask, uint8_t dwellQs, const uint8_t *seed) |
|
Callback for a debug command. Provides the result of ::emberGetMulticastEntry.
|
|
| void | emberGetNetworkKeyInfoReturn ( EmberStatus status, uint32_t sequence, uint8_t state) |
|
Callback for a debug command. Provides the result of ::emberGetNetworkKeyInfo.
|
|
| void | emberGetNodeStatusReturn ( EmberStatus status, const EmberNetworkDebugParameters *parameters) |
|
Callback for a debug command. Provides the result of ::emberGetNodeStatus.
|
|
| void | emberNcpUdpStormCompleteHandler (void) |
|
Callback for a debug command. Provides the result of ::emberNcpUdpStormComplete.
|
|
| void | emberNcpUdpStormReturn ( EmberStatus status) |
|
Callback for a debug command. Provides the result of ::emberNcpUdpStorm.
|
|
| void | emberResetNcpAshReturn (void) |
|
Callback for a debug command. Provides the result of ::emberResetNcpAsh.
|
|
| void | emberSendDoneReturn (void) |
|
Callback for a debug command. Provides the result of ::emberSendDone.
|
|
| void | emberSetRandomizeMacExtendedIdReturn (void) |
|
Callback for a debug command. Provides the result of ::emberSetRandomizeMacExtendedId.
|
|
| void | emberStartUartStormReturn (void) |
|
Callback for a debug command. Provides the result of ::emberStartUartStorm.
|
|
| void | emberStopUartStormReturn (void) |
|
Callback for a debug command. Provides the result of ::emberStopUartStorm.
|
|
| void | emberUartSpeedTestReturn (uint32_t totalBytesSent, uint32_t payloadBytesSent, uint32_t timeout) |
|
Callback for a debug command. Provides the result of ::emberUartSpeedTest.
|
|
Detailed Description
These callbacks were contributed by the thread-debug API.
Function Documentation
| void emberAssertInfoReturn | ( | const uint8_t * |
fileName,
|
| uint32_t |
lineNumber
|
||
| ) |
Sent from the NCP to the host when an assert occurs.
| void emberConfigUartReturn | ( | void |
|
) |
| void emberEchoReturn | ( | const uint8_t * |
data,
|
| uint8_t |
length
|
||
| ) |
| void emberGetMulticastEntryReturn | ( | uint8_t |
lastSequence,
|
| uint8_t |
windowBitmask,
|
||
| uint8_t |
dwellQs,
|
||
| const uint8_t * |
seed
|
||
| ) |
| void emberGetNetworkKeyInfoReturn | ( | EmberStatus |
status,
|
| uint32_t |
sequence,
|
||
| uint8_t |
state
|
||
| ) |
| void emberGetNodeStatusReturn | ( | EmberStatus |
status,
|
| const EmberNetworkDebugParameters * |
parameters
|
||
| ) |
| void emberNcpUdpStormCompleteHandler | ( | void |
|
) |
| void emberNcpUdpStormReturn | ( | EmberStatus |
status
|
) |
| void emberResetNcpAshReturn | ( | void |
|
) |
| void emberSendDoneReturn | ( | void |
|
) |
| void emberSetRandomizeMacExtendedIdReturn | ( | void |
|
) |
| void emberStartUartStormReturn | ( | void |
|
) |
| void emberStopUartStormReturn | ( | void |
|
) |
| void emberUartSpeedTestReturn | ( | uint32_t |
totalBytesSent,
|
| uint32_t |
payloadBytesSent,
|
||
| uint32_t |
timeout
|
||
| ) |