EmberRipEntry Struct Reference
Structure that holds information about a routing table entry for use on the application. See emberGetRipEntry .
#include <
network-management.h
>
Data Fields |
|
| uint8_t | macExtendedId [8] |
| EmberNodeType | type |
| int8_t | rollingRssi |
| uint8_t | nextHopIndex |
| uint8_t | ripMetric |
| uint8_t | incomingLinkQuality |
| uint8_t | outgoingLinkQuality |
| bool | mleSync |
| uint8_t | age |
| uint8_t | routeDelta |
The documentation for this struct was generated from the following file:
-
network-management.h