Direct_Transmit_Plugin
Detailed Description
Direct transmit plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
| struct | EZRADIODRV_DirectTxHandle |
|
EzRadio direct tx plug-in instance initialization and handler structure.
|
|
Macros |
|
| #define | EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
|
Configuration data for EzRadio direct tx plug-in.
|
|
Typedefs |
|
| typedef struct EZRADIODRV_DirectTxHandle | EZRADIODRV_DirectTxHandle_t |
|
EzRadio direct tx plug-in instance initialization and handler structure.
|
|
Functions |
|
| Ecode_t | ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle) |
|
Starts direct transmission with the radio configurations from the radioHandle parameter.
|
|
| Ecode_t | ezradioStopDirectTransmit (void) |
|
Stops direct transmission.
|
|
Macro Definition Documentation
| #define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct tx plug-in.
Definition at line
71
of file
ezradio_direct_transmit_plugin.h
.
Function Documentation
| Ecode_t ezradioStartDirectTransmit | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
Starts direct transmission with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
54
of file
ezradio_direct_transmit_plugin.c
.
References EZRADIODRV_DirectTxHandle::channel , EZRADIODRV_HandleData::directTx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , and ezradio_start_tx() .
| Ecode_t ezradioStopDirectTransmit | ( | void |
|
) |
Stops direct transmission.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
85
of file
ezradio_direct_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .