SensorStruct_t Struct Reference
Stores all runtime values for an enabled capacitive sensor.
Definition at line
71
of file
cslib.h
.
#include <
cslib.h
>
Data Fields |
|
| uint8_t | activeIndicator |
|
Bit array showing whether touch is qualified on sensor, uses DEBOUNCE_ACTIVE_MASK.
|
|
| signed char | baselineAccumulator |
|
Tracks trend of CS values to determine whether baseline rises or falls.
|
|
| uint32_t | currentBaseline |
|
Runtime estimate of untouched or inactive state of CS sensor input.
|
|
| uint8_t | debounceCounts |
|
Stores consecutive CS values above or below active or inactive threshold.
|
|
| SI_UU32_t | expValue |
|
Filtered CS value with 16 bits of LSBs.
|
|
| uint32_t | rawBuffer [ DEF_SENSOR_BUFFER_SIZE ] |
|
Newest sample taken from CS hardware, without any processing.
|
|
| uint8_t | touchDeltaDiv16 |
|
Describes the expected difference between untouched and touched CS value.
|
|
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/middleware/cslib/inc/
cslib.h