__HALL_Config Struct Reference
Structure to configure the Hall effect sensor device.
Definition at line
67
of file
hall.h
.
#include <
hall.h
>
Data Fields |
|
| float | hysteresis |
| bool | outputInvert |
| uint8_t | polarity |
| float | threshold |
Field Documentation
| float __HALL_Config::hysteresis |
| bool __HALL_Config::outputInvert |
The polarity of the output pin
Definition at line
71
of file
hall.h
.
Referenced by HALL_configure() .
| uint8_t __HALL_Config::polarity |
Magnetic field polarity setting
Definition at line
70
of file
hall.h
.
Referenced by HALL_configure() .
| float __HALL_Config::threshold |
Decision point for magnetic field high or low in mT
Definition at line
68
of file
hall.h
.
Referenced by HALL_configure() .
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/hardware/kit/common/bsp/thunderboard/
hall.h