Detailed Description
Graphics Library.
Silicon Labs Graphics Library. Feature rich graphics library for memory constrained applications.
Introduction
GLIB is a graphics library that can be used to draw pixels, common shapes, text or bitmaps to a display connected to an MCU. The main goal of this library is easy of use and small code and memory footprint. In this way GLIB can be used on even the smallest Cortex-M0 devices.
GLIB treats the display as a matrix of pixels which is a model of the physical display. This matrix is exposed to GLIB via an API called DMD (Dot Matrix Display). So in order to draw something on a physical display the user application needs to provide GLIB with a single implementation of the DMD interface. Sample DMD implementations are provided for the displays that are connected to the Silion Labs Starter Kits and the Silicon Labs Development Kits.
Initialization
There are two things that must be initialized before GLIB can be used to draw pixels on the display. First the user needs to initialize the DMD implementation for the actual hardware display which is used. This initialization is display hardware specific.
After the DMD is initialized the user needs to initialize a GLIB_Context_t that can be used for all the drawing operations. A GLIB_Context_t structure is initialized using the GLIB_contextInit() function.
Every GLIB drawing function will require a GLIB_Context_t as one of the functions arguments. The GBLI context contains important configuration values that all the drawing functions use. It contains the foreground and background color, and it also contains information on what font to use when rendering text on the display.
Color
GLIB represent color in a pixel as three 8 bit color values representing red, green and blue, giving the user support for a 24 bit color depth. The GLIB_rgbColor() function can be used to convert from distinct red, green and blue values to an 32-bit integer representing the color of single pixel. Similarly the GLIB_colorTranslate24bpp() function can be used to convert from the 32-bit integer representation into the 3 separate red, green and blue components. The 32-bit integer representation of a pixel color is used when configuring the foreground and background color.
GLIB also contains some common predefined colors for use in places where a 32-bit integer is used to represent the color. These predefined colors include White
, Black
, Brown
, Orange
, and many more. See the glib_color.h
file for the full list of colors.
Some displays are monochrome, meaning that they only support 2 colors. When using GLIB to draw shapes on these displays the applications should use only the 2 colors White
and Black
.
Draw Shapes
GLIB contains functions for drawing common shapes to a display. Here is a list containing all the drawing functions.
- GLIB_drawCircle(). Draw a circle outline with the foreground color.
- GLIB_drawCircleFilled(). Draw a circle filled with the foreground color.
- GLIB_drawPartialCircle(). Draw specific octants of a circle with the foreground color.
- GLIB_drawLine(). Draw line with the foreground color.
- GLIB_drawLineH(). Draw a horizontal line.
- GLIB_drawLineV(). Draw a vertical line.
- GLIB_drawRect(). Draw a rectangle outline with the foreground color.
- GLIB_drawRectFilled(). Draw a filled rectangle using the foreground color.
- GLIB_drawPolygon(). Draw lines between all the points in the given set using the foreground color.
- GLIB_drawPolygonFilled(). Draw filled polygon between points.
Draw Pixels
These are functions that GLIB provides for drawing one pixel.
- GLIB_drawPixel(). Draw a pixel using the foreground color.
- GLIB_drawPixelRGB(). Draw a single pixel using a specific color.
- GLIB_drawPixelColor(). Draw a single pixel using a specific color.
Font rendering
GLIB Supports fixed width font rendering. The functions GLIB_drawString() and GLIB_drawChar() are used to render text on the display.
GLIB provides these fonts for the user
- GLIB_FontNormal8x8 A normal 8x8 pixel font which is the defaul font if nothing else is configured.
- GLIB_FontNarrow6x8 A narrow 6x8 pixel font which can be used if the default font is to wide.
- GLIB_FontNumber16x20 A large font for use with only numbers. This font is 16x20 pixels.
To change the font the user calls GLIB_setFont() with a pointer to a GLIB_Font_t structure which describes the whole font. The GLIB_Font_t structure contains a pointer to the bitmap for each character and it describes attributes of the font like the width and height of each character and it also contains the bitmap of each character.
Draw Bitmap
To draw an image or custom bitmaps on the display the GLIB_drawBitmap() function can be used. Note that the format of the bitmap depends on the DMD implementation of the display. The color displays typically use a bitmap format where each pixel is represented by 3 consecutive bytes representing the red, green and blue color components. While a monochrome display typically use a bitmap format where 1 byte represents 8 pixels where a 0 bit is white and a 1 bit is black. Note that bitmaps are insensitive to the foreground and background color settings.
Example
This examples shows how to initialize a GLIB context and draw something on a display.
Data Structures | |
struct | __BMP_DataType |
BMP Data type structure to hold information about the bmp data returned. | |
struct | __BMP_Header |
BMP Module header structure. Must be packed to exact 54 bytes. | |
struct | __BMP_Palette |
BMP palette structure to hold palette pointer and size. | |
struct | __GLIB_Context_t |
GLIB Drawing Context (Multiple instances of GLIB_Context_t can exist) | |
struct | __GLIB_Font_t |
Font definition structure. | |
struct | __GLIB_Rectangle_t |
Rectangle structure. | |
Typedefs | |
typedef struct __BMP_DataType | BMP_DataType |
BMP Data type structure to hold information about the bmp data returned. | |
typedef struct __BMP_Header | BMP_Header |
typedef struct __BMP_Palette | BMP_Palette |
BMP palette structure to hold palette pointer and size. | |
typedef struct __GLIB_Context_t | GLIB_Context_t |
GLIB Drawing Context (Multiple instances of GLIB_Context_t can exist) | |
typedef enum __GLIB_Font_Class | GLIB_Font_Class |
Font classes. | |
typedef struct __GLIB_Font_t | GLIB_Font_t |
Font definition structure. | |
typedef struct __GLIB_Rectangle_t | GLIB_Rectangle_t |
Rectangle structure. | |
Enumerations | |
enum | __GLIB_Font_Class { InvalidFont = 0, FullFont, NumbersOnlyFont } |
Font classes. | |
Functions | |
int16_t | BMP_getBitsPerPixel (void) |
Get color depth (bits per pixel) | |
int32_t | BMP_getCompressionType (void) |
Get compression type. | |
int32_t | BMP_getDataOffset (void) |
Get the offset, i.e. starting address, of the byte where the bitmap data can be found. | |
int32_t | BMP_getFileSize (void) |
Get the fileSize in bytes. | |
int32_t | BMP_getHeight (void) |
Get height of BMP image in pixels. | |
int32_t | BMP_getImageDataSize (void) |
Get imageDataSize in bytes. | |
int32_t | BMP_getWidth (void) |
Get width of BMP image in pixels. | |
EMSTATUS | BMP_init (uint8_t *palette, uint32_t paletteSize, EMSTATUS(*fp)(uint8_t buffer[], uint32_t bufLength, uint32_t bytesToRead)) |
Initializes BMP Module. | |
EMSTATUS | BMP_readRawData (BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
Fills buffer with raw data from BMP file. | |
EMSTATUS | BMP_readRgbData (uint8_t buffer[], uint32_t bufLength, uint32_t *pixelsRead) |
Reads in data from BMP file and fills buffer with RGB values. This function terminates either when the buffer is full, end of row is reached or end of file is reached. | |
EMSTATUS | BMP_reset (void) |
Makes the module ready for new bmp file. Reads in header from file, and checks if the provided bmp file is valid and supported. It reads in palette if BMP file is 8bpp. Uses function pointer set in BMP_init(). | |
EMSTATUS | GLIB_applyClippingRegion (const GLIB_Context_t *pContext) |
Apply the clipping region from the GLIB_Context_t in the DMD driver. | |
EMSTATUS | GLIB_clear (GLIB_Context_t *pContext) |
Clears the display with the background color of the GLIB_Context_t. | |
EMSTATUS | GLIB_clearRegion (const GLIB_Context_t *pContext) |
Clears the clipping region by filling it with the background color of the GLIB_Context_t. | |
void | GLIB_colorTranslate24bpp (uint32_t color, uint8_t *red, uint8_t *green, uint8_t *blue) |
Extracts the color components from the 32-bit color passed and puts them in the passed in 8-bits ints. The color is 24-bit RGB. | |
EMSTATUS | GLIB_contextInit (GLIB_Context_t *pContext) |
Initialize the GLIB_Context_t. | |
EMSTATUS | GLIB_displaySleep (void) |
Sets the display in sleep mode. | |
EMSTATUS | GLIB_displayWakeUp (void) |
Returns the display from sleep mode. | |
EMSTATUS | GLIB_drawBitmap (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t width, uint32_t height, const uint8_t *picData) |
Draws a bitmap. | |
EMSTATUS | GLIB_drawChar (GLIB_Context_t *pContext, char myChar, int32_t x, int32_t y, bool opaque) |
Draws a char using the font supplied with the library. | |
EMSTATUS | GLIB_drawCircle (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t radius) |
Draws a circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawCircleFilled (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t radius) |
Draws a filled circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawLine (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2, int32_t y2) |
Draws a line from x1,y1 to x2, y2. | |
EMSTATUS | GLIB_drawLineH (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2) |
Draws a horizontal line from x1, y1 to x2, y2. | |
EMSTATUS | GLIB_drawLineV (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t y2) |
Draws a vertical line from x1, y1 to x1, y2. | |
EMSTATUS | GLIB_drawPartialCircle (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius, uint8_t bitMask) |
Draws a partial circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawPixel (GLIB_Context_t *pContext, int32_t x, int32_t y) |
Draws a pixel at x, y using foregroundColor defined in the GLIB_Context_t. | |
EMSTATUS | GLIB_drawPixelColor (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t color) |
Draws a pixel at x, y using the color parameter. | |
EMSTATUS | GLIB_drawPixelRGB (GLIB_Context_t *pContext, int32_t x, int32_t y, uint8_t red, uint8_t green, uint8_t blue) |
Draws a pixel at x, y with color defined by red, green and blue 1 byte per channel. | |
EMSTATUS | GLIB_drawPolygon (GLIB_Context_t *pContext, uint32_t numPoints, const int32_t *polyPoints) |
Draws a polygon using Bresnham's Midpoint Line Algorithm. | |
EMSTATUS | GLIB_drawPolygonFilled (GLIB_Context_t *pContext, uint32_t numPoints, const int32_t *polyPoints) |
Draws a filled polygon using a scan line algorithm. | |
EMSTATUS | GLIB_drawRect (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Draws a rectangle outline defined by the passed in rectangle. | |
EMSTATUS | GLIB_drawRectFilled (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Draws a filled rectangle defined by the passed in rectangle. The filled rectangle is drawn from (xMin, yMin) to (xMax, yMax), inclusive, of the rectangle passed in. | |
EMSTATUS | GLIB_drawString (GLIB_Context_t *pContext, const char *pString, uint32_t sLength, int32_t x0, int32_t y0, bool opaque) |
Draws a string using the font supplied with the library. | |
void | GLIB_invertBitmap (GLIB_Context_t *pContext, uint32_t bitmapSize, uint8_t *picData) |
Inverts each bit of the bitmap. | |
void | GLIB_normalizeRect (GLIB_Rectangle_t *pRect) |
Normalize the rectangle that is passed in. Sets yMin to the minimum value of yMin and yMax. Sets yMax to the maximum value of yMin and yMax. And the same for xMin and xMax. | |
bool | GLIB_rectContainsPoint (const GLIB_Rectangle_t *pRect, int32_t xCenter, int32_t yCenter) |
Checks if the point passed in is in the interior of the rectangle passed in. | |
EMSTATUS | GLIB_resetClippingRegion (GLIB_Context_t *pContext) |
Reset the GLIB_Context_t clipping region to the whole display. | |
EMSTATUS | GLIB_resetDisplayClippingArea (GLIB_Context_t *pContext) |
Reset the display driver clipping area to the whole display. | |
uint32_t | GLIB_rgbColor (uint8_t red, uint8_t green, uint8_t blue) |
Convert 3 uint8_t color components into a 24-bit color. | |
EMSTATUS | GLIB_setClippingRegion (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Sets the clippingRegion of the passed in GLIB_Context_t. | |
EMSTATUS | GLIB_setFont (GLIB_Context_t *pContext, GLIB_Font_t *pFont) |
Set new font for the library. Note that GLIB defines a default font in glib.c. Redefine GLIB_DEFAULT_FONT to change the default font. | |
Variables | |
const GLIB_Font_t | GLIB_FontNarrow6x8 |
Narrow 6x8 pixels font containing characters and numbers. | |
const GLIB_Font_t | GLIB_FontNormal8x8 |
Normal 8x8 pixels font containing characters and numbers. | |
const GLIB_Font_t | GLIB_FontNumber16x20 |
Large 16x20 pixels font containing only numbers. | |
Macro Definition Documentation
#define BMP_END_OF_FILE |
End of file has been reached
Definition at line 42
of file bmp.h
.
#define BMP_ERROR_BUFFER_TOO_SMALL (ECODE_BMP_BASE | 0x0020) |
Buffer provided is too small
Definition at line 64
of file bmp.h
.
Referenced by BMP_init(), and BMP_readRgbData().
#define BMP_ERROR_END_OF_FILE (ECODE_BMP_BASE | 0x0010) |
End of bmp file is reached
Definition at line 62
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRgbData(), and BMP_readRleData().
#define BMP_ERROR_ENDIAN_MISMATCH (ECODE_BMP_BASE | 0x0003) |
#define BMP_ERROR_FILE_INVALID (ECODE_BMP_BASE | 0x0005) |
#define BMP_ERROR_FILE_NOT_RESET (ECODE_BMP_BASE | 0x0009) |
File not reset. Call BMP_reset()
Definition at line 60
of file bmp.h
.
Referenced by BMP_readRawData(), and BMP_readRgbData().
#define BMP_ERROR_FILE_NOT_SUPPORTED (ECODE_BMP_BASE | 0x0004) |
#define BMP_ERROR_HEADER_SIZE_MISMATCH (ECODE_BMP_BASE | 0x0002) |
BMP_Header size in bytes is different from BMP_HEADER_SIZE
Definition at line 46
of file bmp.h
.
Referenced by BMP_init().
#define BMP_ERROR_INVALID_ARGUMENT (ECODE_BMP_BASE | 0x0006) |
Argument passed to function is invalid
Definition at line 54
of file bmp.h
.
Referenced by BMP_readRawData().
#define BMP_ERROR_INVALID_PALETTE_SIZE (ECODE_BMP_BASE | 0x0008) |
#define BMP_ERROR_IO (ECODE_BMP_BASE | 0x0001) |
General IO error
Definition at line 44
of file bmp.h
.
#define BMP_ERROR_MODULE_NOT_INITIALIZED (ECODE_BMP_BASE | 0x0007) |
BMP module is not initialized. Call BMP_init()
Definition at line 56
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRgbData(), and BMP_reset().
#define BMP_ERROR_PALETTE_NOT_READ (ECODE_BMP_BASE | 0x0030) |
Bmp palette is not read
Definition at line 66
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRgbData(), and BMP_reset().
#define BMP_HEADER_SIZE (54) |
BMP Header Size in bytes
Definition at line 71
of file bmp.h
.
Referenced by BMP_init(), and BMP_reset().
#define BMP_LOCAL_CACHE_LIMIT (3) |
#define BMP_LOCAL_CACHE_SIZE (BMP_CONFIG_LOCAL_CACHE_SIZE) |
BMP Local cache size
Definition at line 81
of file bmp.h
.
Referenced by BMP_init(), BMP_readPaddingBytes(), BMP_readRawDataRLE8(), BMP_readRgbData(), BMP_readRgbDataRLE8(), and BMP_readRleData().
#define BMP_OK 0x00000000 |
Successful call
Definition at line 40
of file bmp.h
.
Referenced by BMP_init(), BMP_readPaddingBytes(), BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), BMP_readRgbData(), BMP_readRgbDataRLE8(), BMP_readRleData(), and BMP_reset().
#define BMP_PALETTE_8BIT_SIZE (256 * 4) |
Palette size in bytes
Definition at line 69
of file bmp.h
.
#define ECODE_BMP_BASE 0x00000000 |
BMP base error code
Definition at line 36
of file bmp.h
.
#define ECODE_GLIB_BASE 0x00000000 |
GLIB Base error code
Definition at line 190
of file glib.h
.
#define GLIB_ERROR_FILE_NOT_SUPPORTED (ECODE_GLIB_BASE | 0x0007) |
File not supported
Definition at line 208
of file glib.h
.
#define GLIB_ERROR_INVALID_ARGUMENT (ECODE_GLIB_BASE | 0x0005) |
Invalid argument
Definition at line 204
of file glib.h
.
Referenced by GLIB_applyClippingRegion(), GLIB_clear(), GLIB_clearRegion(), GLIB_contextInit(), GLIB_drawChar(), GLIB_drawCircleFilled(), GLIB_drawLine(), GLIB_drawLineH(), GLIB_drawLineV(), GLIB_drawPartialCircle(), GLIB_drawPixel(), GLIB_drawPixelColor(), GLIB_drawPixelRGB(), GLIB_drawPolygon(), GLIB_drawPolygonFilled(), GLIB_drawString(), GLIB_resetClippingRegion(), GLIB_resetDisplayClippingArea(), GLIB_setClippingRegion(), and GLIB_setFont().
#define GLIB_ERROR_INVALID_CHAR (ECODE_GLIB_BASE | 0x0002) |
Invalid char
Definition at line 198
of file glib.h
.
Referenced by GLIB_drawChar(), and GLIB_drawString().
#define GLIB_ERROR_INVALID_CLIPPINGREGION (ECODE_GLIB_BASE | 0x0004) |
Invalid coordinates (ex. xMin > xMax)
Definition at line 202
of file glib.h
.
Referenced by GLIB_setClippingRegion().
#define GLIB_ERROR_INVALID_FILE (ECODE_GLIB_BASE | 0x0009) |
Invalid file
Definition at line 212
of file glib.h
.
#define GLIB_ERROR_IO (ECODE_GLIB_BASE | 0x0008) |
General IO Error
Definition at line 210
of file glib.h
.
#define GLIB_ERROR_NOTHING_TO_DRAW (ECODE_GLIB_BASE | 0x0001) |
Function did not draw
Definition at line 196
of file glib.h
.
Referenced by GLIB_drawChar(), GLIB_drawCircleFilled(), GLIB_drawLine(), GLIB_drawLineH(), GLIB_drawLineV(), GLIB_drawPartialCircle(), GLIB_drawPartialCirclePoints(), GLIB_drawPixel(), GLIB_drawPixelColor(), GLIB_drawPixelRGB(), GLIB_drawPolygon(), and GLIB_drawString().
#define GLIB_ERROR_OUT_OF_MEMORY (ECODE_GLIB_BASE | 0x0006) |
Out of memory
Definition at line 206
of file glib.h
.
#define GLIB_OK 0x00000000 |
Successful call
Definition at line 194
of file glib.h
.
Referenced by GLIB_clear(), GLIB_contextInit(), GLIB_drawChar(), GLIB_drawCircleFilled(), GLIB_drawLine(), GLIB_drawPartialCircle(), GLIB_drawPartialCirclePoints(), GLIB_drawPolygon(), GLIB_drawPolygonFilled(), GLIB_drawRect(), GLIB_drawString(), GLIB_resetClippingRegion(), and GLIB_setFont().
#define GLIB_OUT_OF_BOUNDS (ECODE_GLIB_BASE | 0x0003) |
Coordinates out of bounds
Definition at line 200
of file glib.h
.
Referenced by GLIB_setClippingRegion().
#define NO_COMPRESSION (0) |
Use no compression
Definition at line 78
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawDataRLE8(), and BMP_readRgbData().
#define RLE8_COMPRESSION (1) |
Use RLE8 compression
Definition at line 76
of file bmp.h
.
Referenced by BMP_readRawData(), BMP_readRawDataRLE8(), and BMP_readRgbData().
Enumeration Type Documentation
enum __GLIB_Font_Class |
Function Documentation
int16_t BMP_getBitsPerPixel | ( | void |
| ) |
Get color depth (bits per pixel)
- Returns
- Returns bitsPerPixel, or -1 on error
Definition at line 954
of file bmp.c
.
References __BMP_Header::bitsPerPixel.
int32_t BMP_getCompressionType | ( | void |
| ) |
Get compression type.
0 - No compression 1 - RLE 8bpp 2 - RLE 4bpp
- Returns
- Returns compressionType, or -1 on error
Definition at line 974
of file bmp.c
.
References __BMP_Header::compressionType.
int32_t BMP_getDataOffset | ( | void |
| ) |
Get the offset, i.e. starting address, of the byte where the bitmap data can be found.
- Returns
- Returns dataOffset, or -1 on error
Definition at line 1006
of file bmp.c
.
References __BMP_Header::dataOffset.
int32_t BMP_getFileSize | ( | void |
| ) |
Get the fileSize in bytes.
- Returns
- Returns fileSize, or -1 on error
Definition at line 1022
of file bmp.c
.
References __BMP_Header::fileSize.
int32_t BMP_getHeight | ( | void |
| ) |
Get height of BMP image in pixels.
- Returns
- Returns height, or -1 on error
Definition at line 938
of file bmp.c
.
References __BMP_Header::height.
int32_t BMP_getImageDataSize | ( | void |
| ) |
Get imageDataSize in bytes.
- Returns
- Returns imageDataSize, or -1 on error
Definition at line 990
of file bmp.c
.
References __BMP_Header::imageDataSize.
int32_t BMP_getWidth | ( | void |
| ) |
Get width of BMP image in pixels.
- Returns
- Returns width of image, or -1 on error
Definition at line 922
of file bmp.c
.
References __BMP_Header::width.
EMSTATUS BMP_init | ( | uint8_t * | palette, |
uint32_t | paletteSize, |
||
EMSTATUS(*)(uint8_t buffer[], uint32_t bufLength, uint32_t bytesToRead) | fp |
||
) |
Initializes BMP Module.
Support:
- 24-bit Uncompressed.
- 8-bit Uncompressed.
- 8-bit RLE compressed.
- Parameters
-
palette
Data buffer to hold palette. Required for 8bpp BMPs. paletteSize
Size of palette in bytes. If BMP is 8-bit, this potentially has to be 256 * 4 bytes. If the user knows that he only loads BMPs with N bytes, he can pass in paletteSize = N. Otherwise this value should be 256 * 4 = 1024 bytes to ensure that the palette is big enough for all 8-bits BMPs. fp
Function pointer that is used to read in bytes from BMP file. The function has to return an EMSTATUS and have the following parameter list (uint32_t buffer[], uint32_t bufLength, uint32_t bytesToRead). The function should fill (buffer) with (bytesToRead) bytes from the beginning. If it succeds it has to return BMP_OK, otherwise it should return BMP_ERROR_IO. When the function returns it should be ready to read from where it left off.
- Returns
- Returns BMP_OK on success, or else error code.
Definition at line 100
of file bmp.c
.
References BMP_ERROR_BUFFER_TOO_SMALL, BMP_ERROR_HEADER_SIZE_MISMATCH, BMP_HEADER_SIZE, BMP_LOCAL_CACHE_LIMIT, BMP_LOCAL_CACHE_SIZE, BMP_OK, __BMP_Palette::data, and __BMP_Palette::size.
EMSTATUS BMP_readRawData | ( | BMP_DataType * | dataType, |
uint8_t | buffer[], |
||
uint32_t | bufLength |
||
) |
Fills buffer with raw data from BMP file.
- If data is 24bit: Buffer is filled with RGB values till its full or end of row is reached.
- If data is 8bit: Buffer is filled with palette indicies till its full or end of row is reached.
- If data is RLE8: Buffer is filled with number of pixels, followed by palette indicies like this (N is number of pixels, P is palette index) buffer = { N P N P ... }.
- Data is 24bpp if dataType.bitsPerPixel == 24 and dataType.compressionType == NO_COMPRESSION.
- Data is 8bpp if dataType.bitsPerPixel == 8 and dataType.compressionType == NO_COMPRESSION.
- Data is RLE8 if dataType.bitsPerPixel == 8 and dataType.compressionType == RLE8_COMPRESSION.
- Parameters
-
dataType
Data type struct which holds information about the data returned buffer
Buffer to be filled with raw data bufLength
Length of buffer
- Returns
- Returns BMP_OK on success, or else error code
Definition at line 843
of file bmp.c
.
References __BMP_Header::bitsPerPixel, __BMP_DataType::bitsPerPixel, BMP_ERROR_END_OF_FILE, BMP_ERROR_FILE_NOT_RESET, BMP_ERROR_INVALID_ARGUMENT, BMP_ERROR_MODULE_NOT_INITIALIZED, BMP_ERROR_PALETTE_NOT_READ, BMP_OK, BMP_readPaddingBytes(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), __BMP_Header::compressionType, __BMP_DataType::compressionType, __BMP_DataType::endOfRow, __BMP_Header::height, __BMP_Header::imageDataSize, NO_COMPRESSION, RLE8_COMPRESSION, __BMP_DataType::size, and __BMP_Header::width.
Referenced by BMP_readRgbData().
EMSTATUS BMP_readRgbData | ( | uint8_t | buffer[], |
uint32_t | bufLength, |
||
uint32_t * | pixelsRead |
||
) |
Reads in data from BMP file and fills buffer with RGB values. This function terminates either when the buffer is full, end of row is reached or end of file is reached.
- Parameters
-
buffer
Buffer to hold RGB values. bufLength
Buffer length in bytes. pixelsRead
Pointer to a uint32_t which holds how many bytes that are read.
- Returns
- Returns BMP_OK on success
- Returns BMP_ERROR_END_OF_FILE if end of file is reached
- Returns error code otherwise.
Definition at line 248
of file bmp.c
.
References __BMP_Header::bitsPerPixel, BMP_ERROR_BUFFER_TOO_SMALL, BMP_ERROR_END_OF_FILE, BMP_ERROR_FILE_NOT_RESET, BMP_ERROR_MODULE_NOT_INITIALIZED, BMP_ERROR_PALETTE_NOT_READ, BMP_LOCAL_CACHE_SIZE, BMP_OK, BMP_readPaddingBytes(), BMP_readRawData(), BMP_readRawData8bit(), BMP_readRgbDataRLE8(), __BMP_Header::compressionType, __BMP_Palette::data, __BMP_DataType::endOfRow, __BMP_Header::height, __BMP_Header::imageDataSize, NO_COMPRESSION, RLE8_COMPRESSION, __BMP_DataType::size, and __BMP_Header::width.
EMSTATUS BMP_reset | ( | void |
| ) |
Makes the module ready for new bmp file. Reads in header from file, and checks if the provided bmp file is valid and supported. It reads in palette if BMP file is 8bpp. Uses function pointer set in BMP_init().
- Returns
- Returns BMP_OK on success, or else error code
Definition at line 136
of file bmp.c
.
References __BMP_Header::bitsPerPixel, BMP_ERROR_ENDIAN_MISMATCH, BMP_ERROR_FILE_INVALID, BMP_ERROR_FILE_NOT_SUPPORTED, BMP_ERROR_INVALID_PALETTE_SIZE, BMP_ERROR_MODULE_NOT_INITIALIZED, BMP_ERROR_PALETTE_NOT_READ, BMP_HEADER_SIZE, BMP_OK, __BMP_Header::compressionType, __BMP_Palette::data, __BMP_Header::dataOffset, __BMP_Header::fileSize, __BMP_Header::headerSize, __BMP_Header::height, __BMP_Header::imageDataSize, __BMP_Header::magic, and __BMP_Palette::size.
EMSTATUS GLIB_applyClippingRegion | ( | const GLIB_Context_t * | pContext | ) |
Apply the clipping region from the GLIB_Context_t in the DMD driver.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 303
of file glib.c
.
References __GLIB_Context_t::clippingRegion, GLIB_ERROR_INVALID_ARGUMENT, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
Referenced by GLIB_clearRegion(), GLIB_drawBitmap(), GLIB_drawLineH(), GLIB_drawLineV(), GLIB_drawRectFilled(), and GLIB_setClippingRegion().
EMSTATUS GLIB_clear | ( | GLIB_Context_t * | pContext | ) |
Clears the display with the background color of the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the background color.
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 174
of file glib.c
.
References __GLIB_Context_t::backgroundColor, GLIB_colorTranslate24bpp(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_OK, GLIB_resetDisplayClippingArea(), and __GLIB_Context_t::pDisplayGeometry.
EMSTATUS GLIB_clearRegion | ( | const GLIB_Context_t * | pContext | ) |
Clears the clipping region by filling it with the background color of the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the background color.
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 214
of file glib.c
.
References __GLIB_Context_t::backgroundColor, __GLIB_Context_t::clippingRegion, GLIB_applyClippingRegion(), GLIB_colorTranslate24bpp(), GLIB_ERROR_INVALID_ARGUMENT, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
void GLIB_colorTranslate24bpp | ( | uint32_t | color, |
uint8_t * | red, |
||
uint8_t * | green, |
||
uint8_t * | blue |
||
) |
Extracts the color components from the 32-bit color passed and puts them in the passed in 8-bits ints. The color is 24-bit RGB.
Example: color = 0x00FFFF00 -> red = 0xFF, green = 0xFF, blue = 0x00.
- Parameters
-
color
The color which is to be translated red
Pointer to a uint8_t holding the red component green
Pointer to a uint8_t holding the green component blue
Pointer to a uint8_t holding the blue component
- Returns
- None.
Definition at line 336
of file glib.c
.
Referenced by GLIB_clear(), GLIB_clearRegion(), GLIB_drawLineH(), GLIB_drawLineV(), and GLIB_drawRectFilled().
EMSTATUS GLIB_contextInit | ( | GLIB_Context_t * | pContext | ) |
Initialize the GLIB_Context_t.
The context is set to default values and gets information about the display from the display driver.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 61
of file glib.c
.
References __GLIB_Context_t::backgroundColor, Black
, __GLIB_Context_t::foregroundColor, GLIB_DEFAULT_FONT, GLIB_ERROR_INVALID_ARGUMENT, GLIB_OK, GLIB_setClippingRegion(), GLIB_setFont(), __GLIB_Context_t::pDisplayGeometry, and White
.
EMSTATUS GLIB_displaySleep | ( | void |
| ) |
Sets the display in sleep mode.
- Returns
- Returns DMD_OK on success, or else error code
Definition at line 118
of file glib.c
.
EMSTATUS GLIB_displayWakeUp | ( | void |
| ) |
Returns the display from sleep mode.
- Returns
- Returns DMD_OK on success, or else error code
Definition at line 105
of file glib.c
.
EMSTATUS GLIB_drawBitmap | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint32_t | width, |
||
uint32_t | height, |
||
const uint8_t * | picData |
||
) |
Draws a bitmap.
Sets up a bitmap that starts at x0,y0 and draws bitmap.
For monochrome displays, each 8-bit element contains 8 pixels values.
For 3-bit RGB displays, each bit in the array are one color component (red, green and blue) of the pixel, so that 3 bits represent one pixel (0xBGR). Pixel 0: Bits 2:0 (0bBGR) of byte 0 Pixel 1: Bits 5:3 (0bBGR) of byte 0 Pixel 2: Bits 7:6 (0bGR) of byte 0 and bit 0 (0bB) of byte 1 Pixel 3: Bits 3:1 (0bBGR) of byte 1 ...
For RGB displays with 8-bits per color, each pixel is represented by 24-bits, with one byte for each of the red, green and blue components. The data has to be organized like this: picData = { R, G, B, R, G, B, R, G, B ... }
The pixels are ordered by increasing x coordinate, after the last pixel of a row, the next pixel will be the first pixel on the next row.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the bitmap is drawn. x
Start x-coordinate for bitmap y
Start y-coordinate for bitmap width
Width of picture height
Height of picture picData
Bitmap data
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 66
of file glib_bitmap.c
.
References GLIB_applyClippingRegion().
EMSTATUS GLIB_drawChar | ( | GLIB_Context_t * | pContext, |
char | myChar, |
||
int32_t | x, |
||
int32_t | y, |
||
bool | opaque |
||
) |
Draws a char using the font supplied with the library.
- Parameters
-
pContext
Pointer to the GLIB_Context_t myChar
Char to be drawn x
Start x-coordinate for the char (Upper left corner) y
Start y-coordinate for the char (Upper left corner) opaque
Determines whether to show the background or color it with the background color specified by the GLIB_Context_t. If opaque == true, the background color is used.
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 52
of file glib_string.c
.
References __GLIB_Context_t::backgroundColor, __GLIB_Font_t::charSpacing, __GLIB_Font_t::class, __GLIB_Font_t::cntOfMapElements, __GLIB_Context_t::font, __GLIB_Font_t::fontHeight, __GLIB_Font_t::fontRowOffset, __GLIB_Font_t::fontWidth, GLIB_drawPixel(), GLIB_drawPixelColor(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_INVALID_CHAR, GLIB_ERROR_NOTHING_TO_DRAW, GLIB_OK, NumbersOnlyFont, __GLIB_Font_t::pFontPixMap, and __GLIB_Font_t::sizeOfMapElement.
Referenced by GLIB_drawString().
EMSTATUS GLIB_drawCircle | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius |
||
) |
Draws a circle with center at x, y, and a radius.
Draws a circle using the Midpoint Circle Algorithm. See Wikipedia for algorithm. Algorithm is optimized to use only integer arithmetic, so no floating point arithmetic is needed.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 52
of file glib_circle.c
.
References GLIB_drawPartialCircle().
EMSTATUS GLIB_drawCircleFilled | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius |
||
) |
Draws a filled circle with center at x, y, and a radius.
Draws a circle using the Midpoint Circle Algorithm and using horizontal lines. See Wikipedia for algorithm.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle
- Returns
- Returns GLIB_OK on succes. Returns GLIB_ERROR_NOTHING_TO_DRAW if none of the pixel coordinates were inside the clipping region. Returns error code otherwise.
Definition at line 151
of file glib_circle.c
.
References GLIB_drawLineH(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_OK.
EMSTATUS GLIB_drawLine | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | x2, |
||
int32_t | y2 |
||
) |
Draws a line from x1,y1 to x2, y2.
Draws a straight line using the Bresnham's Midpoint Line Algorithm. Checks for vertical and horizontal line.
- Parameters
-
pContext
Pointer to the GLIB_Context_t which holds the clipping region x1
Start x-coordinate y1
Start y-coordinate x2
End x-coordinate y2
End y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 337
of file glib_line.c
.
References GLIB_clipLine(), GLIB_drawLineH(), GLIB_drawLineV(), GLIB_drawPixel(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_OK.
Referenced by GLIB_drawPolygon().
EMSTATUS GLIB_drawLineH | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | x2 |
||
) |
Draws a horizontal line from x1, y1 to x2, y2.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the line is drawn. The line is drawn using the foreground color. x1
Start x-coordinate y1
Start y-coordinate x2
End x-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 51
of file glib_line.c
.
References __GLIB_Context_t::clippingRegion, __GLIB_Context_t::foregroundColor, GLIB_applyClippingRegion(), GLIB_colorTranslate24bpp(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, and __GLIB_Rectangle_t::yMax.
Referenced by GLIB_drawCircleFilled(), GLIB_drawLine(), GLIB_drawPolygonFilled(), and GLIB_drawRect().
EMSTATUS GLIB_drawLineV | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | y2 |
||
) |
Draws a vertical line from x1, y1 to x1, y2.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which the line is drawn. The line is drawn using the foreground color. x1
Start x-coordinate y1
Start y-coordinate y2
End y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 125
of file glib_line.c
.
References __GLIB_Context_t::clippingRegion, __GLIB_Context_t::foregroundColor, GLIB_applyClippingRegion(), GLIB_colorTranslate24bpp(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
Referenced by GLIB_drawLine(), and GLIB_drawRect().
EMSTATUS GLIB_drawPartialCircle | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius, |
||
uint8_t | bitMask |
||
) |
Draws a partial circle with center at x, y, and a radius.
Draws a partial circle using the Midpoint Circle Algorithm. Algorithm is optimized to use only integer arithmetic, so no floating point arithmetic is needed. The bitMask passed in decides which octant that should be drawn. The octants is numbered 1 to 8 in counterclockwise order.
Example: bitMask == 4 draws only pixels in 3. octant (00000100). bitMask == 5 draws only pixels in 3. and 1. octant (00000101).
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle bitMask
Bitmask which decides which octants pixels should be drawn. The LSB is 1. octant, and the MSB is 8. octant.
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 84
of file glib_circle.c
.
References GLIB_drawPartialCirclePoints(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_OK.
Referenced by GLIB_drawCircle().
EMSTATUS GLIB_drawPixel | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y |
||
) |
Draws a pixel at x, y using foregroundColor defined in the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the foreground color and clipping region x
X-coordinate y
Y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 377
of file glib.c
.
References __GLIB_Context_t::clippingRegion, __GLIB_Context_t::foregroundColor, GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_rectContainsPoint().
Referenced by GLIB_drawChar(), GLIB_drawLine(), and GLIB_drawPartialCirclePoints().
EMSTATUS GLIB_drawPixelColor | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint32_t | color |
||
) |
Draws a pixel at x, y using the color parameter.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the clipping region x
X-coordinate y
Y-coordinate color
32-bit int defining the RGB color. The 24 LSB defines the RGB color like this: RRRRRRRRGGGGGGGGBBBBBBBB. Example: Yellow = 0x00FFFF00
- Returns
- Returns DMD_OK on success, or else error code
Definition at line 412
of file glib.c
.
References __GLIB_Context_t::clippingRegion, GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_rectContainsPoint().
Referenced by GLIB_drawChar().
EMSTATUS GLIB_drawPixelRGB | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint8_t | red, |
||
uint8_t | green, |
||
uint8_t | blue |
||
) |
Draws a pixel at x, y with color defined by red, green and blue 1 byte per channel.
Example: To draw a yellow pixel at (10, 10). x = 10, y = 10, red = 0xFF, green = 0xFF, blue = 0x00
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the clipping region x
X-coordinate y
Y-coordinate red
8-bit red code green
8-bit green code blue
8-bit blue code
- Returns
- Returns DMD_OK on success, or else error code
Definition at line 456
of file glib.c
.
References __GLIB_Context_t::clippingRegion, GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_rectContainsPoint().
EMSTATUS GLIB_drawPolygon | ( | GLIB_Context_t * | pContext, |
uint32_t | numPoints, |
||
const int32_t * | polyPoints |
||
) |
Draws a polygon using Bresnham's Midpoint Line Algorithm.
This function draws a line between all points outlining the polygon. The first and last point doesn't have to be the same. The function automatically draws a line from the start point to the end point.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which the line is drawn. The lines are drawn using the foreground color. numPoints
Number of points in the polygon ( Has to be greater than 1 ) polyPoints
Pointer to array of polygon points. The points are laid out like this: polyPoints = {x1,y1,x2,y2 ... } Polypoints has to contain at least (numPoints * 2) entries
- Returns
- Returns GLIB_OK on if at least one element was drawn, or else error code
Definition at line 53
of file glib_polygon.c
.
References GLIB_drawLine(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_OK.
EMSTATUS GLIB_drawPolygonFilled | ( | GLIB_Context_t * | pContext, |
uint32_t | numPoints, |
||
const int32_t * | polyPoints |
||
) |
Draws a filled polygon using a scan line algorithm.
This function draws a line between all points outlining the polygon. The first and last point doesn't have to be the same. The function automatically draws a line from the start point to the end point.
- Parameters
-
pContext
Pointer to a GLIB_Context_t where the polygon is drawn. The polygon drawn using the foreground color. numPoints
Number of points in the polygon ( Has to be greater than 1 ) polyPoints
Pointer to array of polygon points. The points are laid out like this: polyPoints = {x1,y1,x2,y2 ... } Polypoints has to contain at least (numPoints * 2) entries
- Returns
- Returns GLIB_OK on success, otherwise a GLIB error code.
Definition at line 128
of file glib_polygon.c
.
References __GLIB_Context_t::clippingRegion, GLIB_drawLineH(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_OK, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
EMSTATUS GLIB_drawRect | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Draws a rectangle outline defined by the passed in rectangle.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the rectangle is drawn. The rectangle is drawn using the foreground color. pRect
Pointer to a rectangle structure
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 98
of file glib_rectangle.c
.
References __GLIB_Context_t::clippingRegion, GLIB_drawLineH(), GLIB_drawLineV(), GLIB_normalizeRect(), GLIB_OK, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
EMSTATUS GLIB_drawRectFilled | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Draws a filled rectangle defined by the passed in rectangle. The filled rectangle is drawn from (xMin, yMin) to (xMax, yMax), inclusive, of the rectangle passed in.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the rectangle is drawn. The rectangle is filled with the foreground color. pRect
Pointer to a rectangle structure
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 170
of file glib_rectangle.c
.
References __GLIB_Context_t::clippingRegion, __GLIB_Context_t::foregroundColor, GLIB_applyClippingRegion(), GLIB_colorTranslate24bpp(), GLIB_normalizeRect(), __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
EMSTATUS GLIB_drawString | ( | GLIB_Context_t * | pContext, |
const char * | pString, |
||
uint32_t | sLength, |
||
int32_t | x0, |
||
int32_t | y0, |
||
bool | opaque |
||
) |
Draws a string using the font supplied with the library.
- Parameters
-
pContext
Pointer to a GLIB_Context_t pString
Pointer to the string that is drawn sLength
number of characters in the string x0
Start x-coordinate for the string (Upper left corner) y0
Start y-coordinate for the string (Upper left corner) opaque
Determines whether to show the background or color it with the background color specified by the GLIB_Context_t. If opaque == 1, the background color is used.
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 180
of file glib_string.c
.
References __GLIB_Font_t::charSpacing, __GLIB_Font_t::class, __GLIB_Context_t::font, __GLIB_Font_t::fontHeight, __GLIB_Font_t::fontWidth, GLIB_drawChar(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_INVALID_CHAR, GLIB_ERROR_NOTHING_TO_DRAW, GLIB_OK, InvalidFont, and __GLIB_Font_t::lineSpacing.
void GLIB_invertBitmap | ( | GLIB_Context_t * | pContext, |
uint32_t | bitmapSize, |
||
uint8_t * | picData |
||
) |
Inverts each bit of the bitmap.
For monochrome displays, the result is an inversion of the image.
For RGB displays, the result is the negative of the input image.
- Note
- The function inverts entire bytes, meaning that any bits contained within the array that may not be part of the image will also be inverted.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the bitmap is drawn. bitmapSize
Size of the bitmap array in terms of bytes. picData
Bitmap data.
Definition at line 106
of file glib_bitmap.c
.
void GLIB_normalizeRect | ( | GLIB_Rectangle_t * | pRect | ) |
Normalize the rectangle that is passed in. Sets yMin to the minimum value of yMin and yMax. Sets yMax to the maximum value of yMin and yMax. And the same for xMin and xMax.
- Parameters
-
pRect
Pointer to a rectangle structure
- Returns
- None.
Definition at line 68
of file glib_rectangle.c
.
References __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
Referenced by GLIB_drawRect(), and GLIB_drawRectFilled().
bool GLIB_rectContainsPoint | ( | const GLIB_Rectangle_t * | pRect, |
int32_t | x, |
||
int32_t | y |
||
) |
Checks if the point passed in is in the interior of the rectangle passed in.
If the point is on the edge of the rectangle the function returns 1.
- Parameters
-
pRect
Pointer to a rectangle structure x
X-coordinate of point y
Y-coordinate of point
- Returns
- Returns false if coordinate is outside the rectangle
- Returns true otherwise
Definition at line 43
of file glib_rectangle.c
.
References __GLIB_Rectangle_t::xMax, and __GLIB_Rectangle_t::yMax.
Referenced by GLIB_drawPixel(), GLIB_drawPixelColor(), and GLIB_drawPixelRGB().
EMSTATUS GLIB_resetClippingRegion | ( | GLIB_Context_t * | pContext | ) |
Reset the GLIB_Context_t clipping region to the whole display.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 278
of file glib.c
.
References __GLIB_Context_t::clippingRegion, GLIB_ERROR_INVALID_ARGUMENT, GLIB_OK, __GLIB_Context_t::pDisplayGeometry, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
EMSTATUS GLIB_resetDisplayClippingArea | ( | GLIB_Context_t * | pContext | ) |
Reset the display driver clipping area to the whole display.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 257
of file glib.c
.
References GLIB_ERROR_INVALID_ARGUMENT, and __GLIB_Context_t::pDisplayGeometry.
Referenced by GLIB_clear().
uint32_t GLIB_rgbColor | ( | uint8_t | red, |
uint8_t | green, |
||
uint8_t | blue |
||
) |
Convert 3 uint8_t color components into a 24-bit color.
Example: red = 0xFF, green = 0xFF, blue = 0x00 -> 0x00FFFF00 = Yellow
- Parameters
-
red
Red component green
Green component blue
Blue component
- Returns
- Returns a 32-bit unsigned integer representing the color. The 8 LSB is blue, the next 8 is green and the next 8 is red. 0x00RRGGBB
Definition at line 358
of file glib.c
.
References BlueShift
, GreenShift
, and RedShift
.
EMSTATUS GLIB_setClippingRegion | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Sets the clippingRegion of the passed in GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t pRect
Pointer to a GLIB_Rectangle_t which is the clipping region to be set.
- Returns
- Returns GLIB_OK on success
- Returns GLIB_ERROR_INVALID_CLIPPINGREGION if invalid coordinates
- Returns GLIB_OUT_OF_BOUNDS if clipping region is bigger than display clipping area
Definition at line 139
of file glib.c
.
References __GLIB_Context_t::clippingRegion, GLIB_applyClippingRegion(), GLIB_ERROR_INVALID_ARGUMENT, GLIB_ERROR_INVALID_CLIPPINGREGION, GLIB_OUT_OF_BOUNDS, __GLIB_Context_t::pDisplayGeometry, __GLIB_Rectangle_t::xMax, __GLIB_Rectangle_t::xMin, __GLIB_Rectangle_t::yMax, and __GLIB_Rectangle_t::yMin.
Referenced by GLIB_contextInit().
EMSTATUS GLIB_setFont | ( | GLIB_Context_t * | pContext, |
GLIB_Font_t * | pFont |
||
) |
Set new font for the library. Note that GLIB defines a default font in glib.c. Redefine GLIB_DEFAULT_FONT to change the default font.
- Parameters
-
pContext
Pointer to the GLIB_Context_t pFont
Pointer to the new font
- Returns
- Returns GLIB_OK on success, or else error code
Definition at line 238
of file glib_string.c
.
References __GLIB_Context_t::font, GLIB_ERROR_INVALID_ARGUMENT, and GLIB_OK.
Referenced by GLIB_contextInit().