bmp.c File Reference
BMP Module.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
Definition in file
bmp.c
.
#include "
bmp.h
"
#include <stdint.h>
#include "em_types.h"
Functions |
|
| int16_t | BMP_getBitsPerPixel () |
|
Get color depth (bits per pixel)
|
|
| int32_t | BMP_getCompressionType () |
|
Get compression type.
|
|
| int32_t | BMP_getDataOffset () |
|
Get the offset, i.e. starting address, of the byte where the bitmap data can be found.
|
|
| int32_t | BMP_getFileSize () |
|
Get the fileSize in bytes.
|
|
| int32_t | BMP_getHeight () |
|
Get height of BMP image in pixels.
|
|
| int32_t | BMP_getImageDataSize () |
|
Get imageDataSize in bytes.
|
|
| int32_t | BMP_getWidth () |
|
Get width of BMP image in pixels.
|
|
| EMSTATUS | BMP_init (uint8_t *palette, uint32_t paletteSize, EMSTATUS(*fp)(uint8_t buffer[], uint32_t bufLength, uint32_t bytesToRead)) |
|
Initializes BMP Module.
|
|
| static EMSTATUS | BMP_readPaddingBytes (uint8_t paddingBytes) |
|
Help function to read in padding bytes.
|
|
| EMSTATUS | BMP_readRawData ( BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Fills buffer with raw data from BMP file.
|
|
| static EMSTATUS | BMP_readRawData24bit ( BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Help function to read 24-bit RGB BMP data.
|
|
| static EMSTATUS | BMP_readRawData8bit ( BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Help function to read 8-bit BMP data.
|
|
| static EMSTATUS | BMP_readRawDataRLE8 ( BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Help function to read 8-bit RLE BMP data.
|
|
| EMSTATUS | BMP_readRgbData (uint8_t buffer[], uint32_t bufLength, uint32_t *pixelsRead) |
|
Reads in data from BMP file and fills buffer with RGB values. This function terminates either when the buffer is full, end of row is reached or end of file is reached.
|
|
| static EMSTATUS | BMP_readRgbDataRLE8 (uint8_t buffer[], uint32_t bufLength, uint32_t *pixelsRead) |
|
Help function used by BMP_readRgbData to read in RLE8 data. This function terminates either when the buffer is full or end of row is reached.
|
|
| static EMSTATUS | BMP_readRleData ( BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Help function to read in RLE info. Use this only if you know that RLE info is coming. This function takes the markers and decode them. If no marker is present, buffer is filled with 2 bytes containing the RLE info. This function always reads in two bytes.
|
|
| EMSTATUS | BMP_reset () |
|
Makes the module ready for new bmp file. Reads in header from file, and checks if the provided bmp file is valid and supported. It reads in palette if BMP file is 8bpp. Uses function pointer set in
BMP_init()
.
|
|
Function Documentation
|
static |
Help function to read in padding bytes.
- Parameters
-
paddingBytesNumber of paddingBytes at the end of the row
- Returns
- Returns BMP_OK on success, or else error code
Definition at line
727
of file
bmp.c
.
References BMP_LOCAL_CACHE_SIZE , and BMP_OK .
Referenced by BMP_readRawData() , and BMP_readRgbData() .
|
static |
Help function to read 24-bit RGB BMP data.
- Parameters
-
dataTypeData type struct which holds information about the data returned bufferBuffer to be filled with raw data bufLengthLength of buffer
- Returns
- Returns BMP_OK on success, or else error code
Definition at line
551
of file
bmp.c
.
References __BMP_DataType::bitsPerPixel , BMP_ERROR_END_OF_FILE , BMP_OK , __BMP_DataType::compressionType , __BMP_DataType::endOfRow , __BMP_Header::height , __BMP_Header::imageDataSize , NO_COMPRESSION , __BMP_DataType::size , and __BMP_Header::width .
Referenced by BMP_readRawData() .
|
static |
Help function to read 8-bit BMP data.
- Parameters
-
dataTypeData type struct which holds information about the data returned bufferBuffer to be filled with raw data bufLengthLength of buffer
- Returns
- Returns BMP_OK on success
Definition at line
498
of file
bmp.c
.
References __BMP_DataType::bitsPerPixel , BMP_ERROR_END_OF_FILE , BMP_OK , __BMP_DataType::compressionType , __BMP_DataType::endOfRow , __BMP_Header::height , __BMP_Header::imageDataSize , __BMP_DataType::size , and __BMP_Header::width .
Referenced by BMP_readRawData() , and BMP_readRgbData() .
|
static |
Help function to read 8-bit RLE BMP data.
- Parameters
-
dataTypeData type struct which holds information about the data returned bufferBuffer to be filled with raw data bufLengthLength of buffer
- Returns
- Returns BMP_OK on success, or else error code
Definition at line
616
of file
bmp.c
.
References __BMP_DataType::bitsPerPixel , BMP_LOCAL_CACHE_SIZE , BMP_OK , BMP_readRleData() , __BMP_DataType::compressionType , __BMP_DataType::endOfRow , NO_COMPRESSION , RLE8_COMPRESSION , and __BMP_DataType::size .
Referenced by BMP_readRawData() .
|
static |
Help function used by BMP_readRgbData to read in RLE8 data. This function terminates either when the buffer is full or end of row is reached.
- Parameters
-
bufferBuffer to hold RGB values bufLengthBuffer length in bytes pixelsReadPointer to a uint32_t which holds how many bytes that are read
- Returns
- Returns BMP_OK on success, or else error code
Definition at line
366
of file
bmp.c
.
References BMP_LOCAL_CACHE_SIZE , BMP_OK , BMP_readRleData() , __BMP_Palette::data , and __BMP_DataType::endOfRow .
Referenced by BMP_readRgbData() .
|
static |
Help function to read in RLE info. Use this only if you know that RLE info is coming. This function takes the markers and decode them. If no marker is present, buffer is filled with 2 bytes containing the RLE info. This function always reads in two bytes.
- Parameters
-
dataTypeData type structure which holds endOfRow. bufferBuffer to be filled with RLE info. bufLengthLength of buffer. Has to be at least 2.
- Returns
- Returns BMP_OK on success. Returns BMP_END_OF_FILE if EOF is reached, or else error code
Definition at line
759
of file
bmp.c
.
References BMP_ERROR_END_OF_FILE , BMP_LOCAL_CACHE_SIZE , BMP_OK , and __BMP_DataType::endOfRow .
Referenced by BMP_readRawDataRLE8() , and BMP_readRgbDataRLE8() .