ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line 636
of file em_acmp.h
.
#include <
em_acmp.h
>
Field Documentation
ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
Definition at line 667
of file em_acmp.h
.
Referenced by ACMP_Init().
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line 649
of file em_acmp.h
.
Referenced by ACMP_Init().
bool ACMP_Init_TypeDef::enable |
If true, ACMP is being enabled after configuration.
Definition at line 714
of file em_acmp.h
.
Referenced by ACMP_Init().
bool ACMP_Init_TypeDef::fullBias |
Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line 639
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0 |
Hysteresis when ACMP output is 0
Definition at line 686
of file em_acmp.h
.
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1 |
Hysteresis when ACMP output is 1
Definition at line 689
of file em_acmp.h
.
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by the ACMP during warmup
Definition at line 699
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range. Adjust this setting to optimize the performance for a given input voltage range.
Definition at line 660
of file em_acmp.h
.
Referenced by ACMP_Init().
bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on falling edge
Definition at line 652
of file em_acmp.h
.
Referenced by ACMP_Init().
bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on rising edge
Definition at line 655
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource |
Select the power source for the ACMP.
Definition at line 672
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput |
VLP Input source. Select between using VADIV or VBDIV as the VLP source.
Definition at line 695
of file em_acmp.h
.
Referenced by ACMP_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_acmp.h