CAN_Init_TypeDef Struct ReferenceEMLIB > CAN
CAN initialization structure.
Definition at line
156
of file
em_can.h
.
#include <
em_can.h
>
Data Fields |
|
| uint32_t | bitrate |
| bool | enable |
| uint8_t | phaseBufferSegment1 |
| uint8_t | phaseBufferSegment2 |
| uint8_t | propagationTimeSegment |
| bool | resetMessages |
| uint8_t | synchronisationJumpWidth |
Field Documentation
| uint32_t CAN_Init_TypeDef::bitrate |
| bool CAN_Init_TypeDef::enable |
true to set the CAN Device in normal mode after init
Definition at line
158
of file
em_can.h
.
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::phaseBufferSegment1 |
| uint8_t CAN_Init_TypeDef::phaseBufferSegment2 |
| uint8_t CAN_Init_TypeDef::propagationTimeSegment |
Default Propagation Time Segment
Definition at line
167
of file
em_can.h
.
Referenced by CAN_Init() .
| bool CAN_Init_TypeDef::resetMessages |
True to reset messages during initialization
Definition at line
161
of file
em_can.h
.
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::synchronisationJumpWidth |
Default Synchronisation Jump Width
Definition at line
176
of file
em_can.h
.
Referenced by CAN_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_can.h