LESENSE_TypeDef Struct ReferenceDevices > LESENSE
LESENSE Register Declaration
Definition at line
49
of file
efm32gg11b_lesense.h
.
#include <
efm32gg11b_lesense.h
>
Data Fields |
|
| __IOM uint32_t | ALTEXCONF |
| __IOM uint32_t | BIASCTRL |
| LESENSE_BUF_TypeDef | BUF [16] |
| __IM uint32_t | BUFDATA |
| LESENSE_CH_TypeDef | CH [16] |
| __IOM uint32_t | CHEN |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IM uint32_t | CURCH |
| __IOM uint32_t | DECCTRL |
| __IOM uint32_t | DECSTATE |
| __IOM uint32_t | EVALCTRL |
| __IOM uint32_t | IDLECONF |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | PERCTRL |
| __IOM uint32_t | PRSCTRL |
| __IM uint32_t | PTR |
| uint32_t | RESERVED0 [2] |
| uint32_t | RESERVED1 [38] |
| __IOM uint32_t | ROUTEPEN |
| __IOM uint32_t | SCANRES |
| __IOM uint32_t | SENSORSTATE |
| LESENSE_ST_TypeDef | ST [32] |
| __IM uint32_t | STATUS |
| __IM uint32_t | SYNCBUSY |
| __IOM uint32_t | TIMCTRL |
Field Documentation
| __IOM uint32_t LESENSE_TypeDef::ALTEXCONF |
Alternative Excite Pin Configuration
Definition at line
67
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::BIASCTRL |
Bias Control Register
Definition at line
54
of file
efm32gg11b_lesense.h
.
| LESENSE_BUF_TypeDef LESENSE_TypeDef::BUF[16] |
Scanresult
Definition at line
79
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::BUFDATA |
Result Buffer Data Register
Definition at line
62
of file
efm32gg11b_lesense.h
.
| LESENSE_CH_TypeDef LESENSE_TypeDef::CH[16] |
Scanconfig
Definition at line
81
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CHEN |
Channel Enable Register
Definition at line
58
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CMD |
Command Register
Definition at line
57
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CTRL |
Control Register
Definition at line
50
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::CURCH |
Current Channel Index
Definition at line
63
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::DECCTRL |
Decoder Control Register
Definition at line
53
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::DECSTATE |
Current Decoder State
Definition at line
64
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::EVALCTRL |
LESENSE Evaluation Control
Definition at line
55
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IDLECONF |
GPIO Idle Phase Configuration
Definition at line
66
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IEN |
Interrupt Enable Register
Definition at line
72
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::IF |
Interrupt Flag Register
Definition at line
69
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
71
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
70
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::PERCTRL |
Peripheral Control Register
Definition at line
52
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::PRSCTRL |
PRS Control Register
Definition at line
56
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::PTR |
Result Buffer Pointers
Definition at line
61
of file
efm32gg11b_lesense.h
.
| uint32_t LESENSE_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line
68
of file
efm32gg11b_lesense.h
.
| uint32_t LESENSE_TypeDef::RESERVED1[38] |
Reserved registers
Definition at line
76
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::ROUTEPEN |
I/O Routing Register
Definition at line
74
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::SCANRES |
Scan Result Register
Definition at line
59
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::SENSORSTATE |
Decoder Input Register
Definition at line
65
of file
efm32gg11b_lesense.h
.
| LESENSE_ST_TypeDef LESENSE_TypeDef::ST[32] |
Decoding states
Definition at line
77
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::STATUS |
Status Register
Definition at line
60
of file
efm32gg11b_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
73
of file
efm32gg11b_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::TIMCTRL |
Timing Control Register
Definition at line
51
of file
efm32gg11b_lesense.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_lesense.h