SDIO_TypeDef Struct ReferenceDevices > SDIO
SDIO Register Declaration
Definition at line 49
of file efm32gg11b_sdio.h
.
#include <
efm32gg11b_sdio.h
>
Data Fields | |
__IOM uint32_t | AC12ERRSTAT |
__IM uint32_t | ADMAES |
__IOM uint32_t | ADSADDR |
__IOM uint32_t | BLKSIZE |
__IOM uint32_t | BOOTTOCTRL |
__IOM uint32_t | BUFDATPORT |
__IM uint32_t | CAPAB0 |
__IM uint32_t | CAPAB2 |
__IOM uint32_t | CFG0 |
__IOM uint32_t | CFG1 |
__IOM uint32_t | CFGPRESETVAL0 |
__IOM uint32_t | CFGPRESETVAL1 |
__IOM uint32_t | CFGPRESETVAL2 |
__IOM uint32_t | CFGPRESETVAL3 |
__IOM uint32_t | CLOCKCTRL |
__IOM uint32_t | CMDARG1 |
__IOM uint32_t | CTRL |
__IOM uint32_t | FEVTERRSTAT |
__IOM uint32_t | HOSTCTRL1 |
__IOM uint32_t | IEN |
__IOM uint32_t | IFCR |
__IOM uint32_t | IFENC |
__IM uint32_t | MAXCURCAPAB |
__IM uint32_t | PRSSTAT |
__IM uint32_t | PRSTVAL0 |
__IM uint32_t | PRSTVAL2 |
__IM uint32_t | PRSTVAL4 |
__IM uint32_t | PRSTVAL6 |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED2 [34] |
uint32_t | RESERVED3 [448] |
__IM uint32_t | RESP0 |
__IM uint32_t | RESP2 |
__IM uint32_t | RESP4 |
__IM uint32_t | RESP6 |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTELOC1 |
__IOM uint32_t | ROUTEPEN |
__IOM uint32_t | SDMASYSADDR |
__IM uint32_t | SLOTINTSTAT |
__IOM uint32_t | TFRMODE |
Field Documentation
__IOM uint32_t SDIO_TypeDef::AC12ERRSTAT |
AUTO CMD12 Error Status and Host Control2 Register
Definition at line 65
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::ADMAES |
ADMA Error Status Register
Definition at line 71
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::ADSADDR |
ADMA System Address Register
Definition at line 72
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::BLKSIZE |
Block Size and Block Count Register
Definition at line 51
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::BOOTTOCTRL |
Boot Timeout Control Register
Definition at line 78
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::BUFDATPORT |
Buffer Data Register
Definition at line 58
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::CAPAB0 |
Capabilities Register to Hold Bits 31~0
Definition at line 66
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::CAPAB2 |
Capabilities Register to Hold Bits 63~32
Definition at line 67
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFG0 |
Core Configuration 0
Definition at line 84
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFG1 |
Core Configuration 1
Definition at line 85
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFGPRESETVAL0 |
Core Configuration Preset Value 0
Definition at line 86
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFGPRESETVAL1 |
Core Configuration Preset Value 1
Definition at line 87
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFGPRESETVAL2 |
Core Configuration Preset Value 2
Definition at line 88
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CFGPRESETVAL3 |
Core Configuration Preset Value 3
Definition at line 89
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CLOCKCTRL |
Clock Control, Timeout Control and Software Register
Definition at line 61
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CMDARG1 |
SD Command Argument Register
Definition at line 52
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::CTRL |
Core Control Signals
Definition at line 83
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::FEVTERRSTAT |
Force Event Register for Auto CMD Error Status
Definition at line 70
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::HOSTCTRL1 |
Host Control1, Power, Block Gap and Wakeup-up Control Register
Definition at line 60
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::IEN |
Normal and Error Interrupt Signal Enable Register
Definition at line 64
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::IFCR |
Normal and Error Interrupt Status Register
Definition at line 62
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::IFENC |
Normal and Error Interrupt Status Enable Register
Definition at line 63
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::MAXCURCAPAB |
Maximum Current Capabilities Register
Definition at line 68
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::PRSSTAT |
Present State Register
Definition at line 59
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::PRSTVAL0 |
Preset Value for Initialization and Default Speed Mode
Definition at line 74
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::PRSTVAL2 |
Preset Value for High Speed and SDR12 Modes
Definition at line 75
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::PRSTVAL4 |
Preset Value for SDR25 and SDR50 Modes
Definition at line 76
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::PRSTVAL6 |
Preset Value for SDR104 and DDR50 Modes
Definition at line 77
of file efm32gg11b_sdio.h
.
uint32_t SDIO_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 69
of file efm32gg11b_sdio.h
.
uint32_t SDIO_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 73
of file efm32gg11b_sdio.h
.
uint32_t SDIO_TypeDef::RESERVED2[34] |
Reserved for future use
Definition at line 79
of file efm32gg11b_sdio.h
.
uint32_t SDIO_TypeDef::RESERVED3[448] |
Reserved for future use
Definition at line 82
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::RESP0 |
Response0 and Response1 Register
Definition at line 54
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::RESP2 |
Response2 and Response3 Register
Definition at line 55
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::RESP4 |
Response4 and Response5 Register
Definition at line 56
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::RESP6 |
Response6 and Response7 Register
Definition at line 57
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::ROUTELOC0 |
I/O LOCATION Register
Definition at line 90
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::ROUTELOC1 |
I/O LOCATION Register
Definition at line 91
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::ROUTEPEN |
I/O LOCATION Enable Register
Definition at line 92
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::SDMASYSADDR |
SDMA System Address Register
Definition at line 50
of file efm32gg11b_sdio.h
.
__IM uint32_t SDIO_TypeDef::SLOTINTSTAT |
Slot Interrupt Status Register
Definition at line 80
of file efm32gg11b_sdio.h
.
__IOM uint32_t SDIO_TypeDef::TFRMODE |
Transfer Mode and Command Register
Definition at line 53
of file efm32gg11b_sdio.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_sdio.h