EBI_TFTInit_TypeDef Struct ReferenceEMLIB > EBI
TFT Initialization structure
Definition at line 553
of file em_ebi.h
.
#include <
em_ebi.h
>
Field Documentation
uint32_t EBI_TFTInit_TypeDef::addressOffset |
TFT Frame Buffer address, offset to EBI bank base address
Definition at line 597
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_TFTBank_TypeDef EBI_TFTInit_TypeDef::bank |
External memory bank for driving display
Definition at line 555
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_TFTColorSrc_TypeDef EBI_TFTInit_TypeDef::colSrc |
Color source for masking and alpha blending
Definition at line 559
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::csPolarity |
TFT Polarity for Chip Select (CS) Line
Definition at line 571
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::dataenPolarity |
TFT Polarity for Data Enable (DATAEN) Line
Definition at line 575
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::dclkPeriod |
TFT DCLK period in internal cycles
Definition at line 599
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::dclkPolarity |
TFT Polarity for Data Clock (DCLK) Line
Definition at line 573
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_TFTDDMode_TypeDef EBI_TFTInit_TypeDef::driveMode |
EBI_TFTFrameBufTrigger_TypeDef EBI_TFTInit_TypeDef::fbTrigger |
Trigger for updating frame buffer pointer
Definition at line 563
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::holdCycles |
Number of cycles RGB data is held after active edge of DCLK
Definition at line 605
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::hPorchBack |
int EBI_TFTInit_TypeDef::hPorchFront |
int EBI_TFTInit_TypeDef::hPulseWidth |
Horizontal Synchronization Pulse Width
Definition at line 587
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::hsize |
EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::hsyncPolarity |
TFT Polarity for Horizontal Sync (HSYNC) Line
Definition at line 577
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_TFTInterleave_TypeDef EBI_TFTInit_TypeDef::interleave |
EBI_TFTMaskBlend_TypeDef EBI_TFTInit_TypeDef::maskBlend |
Masking and alpha blending mode
Definition at line 567
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::setupCycles |
Number of cycles RGB data is driven before active edge of DCLK
Definition at line 603
of file em_ebi.h
.
Referenced by EBI_TFTInit().
bool EBI_TFTInit_TypeDef::shiftDClk |
Drive DCLK from negative clock edge of internal clock
Definition at line 565
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::startPosition |
Starting position of External Direct Drive relative to DCLK inactive edge
Definition at line 601
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::vPorchBack |
int EBI_TFTInit_TypeDef::vPorchFront |
int EBI_TFTInit_TypeDef::vPulseWidth |
Vertical Synchronization Pulse Width
Definition at line 595
of file em_ebi.h
.
Referenced by EBI_TFTInit().
int EBI_TFTInit_TypeDef::vsize |
EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::vsyncPolarity |
TFT Polarity for Vertical Sync (VSYNC) Line
Definition at line 579
of file em_ebi.h
.
Referenced by EBI_TFTInit().
EBI_TFTWidth_TypeDef EBI_TFTInit_TypeDef::width |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_ebi.h