RTC_Init_TypeDef Struct ReferenceEMLIB > RTC

RTC initialization structure.

Definition at line 60 of file em_rtc.h.

#include <em_rtc.h>

Data Fields

bool comp0Top
 
bool debugRun
 
bool enable
 

Field Documentation

bool RTC_Init_TypeDef::comp0Top

Use compare register 0 as max count value.

Definition at line 63 of file em_rtc.h.

Referenced by RTC_Init(), and UDELAY_Calibrate().

bool RTC_Init_TypeDef::debugRun

Counter shall keep running during debug halt.

Definition at line 62 of file em_rtc.h.

Referenced by RTC_Init().

bool RTC_Init_TypeDef::enable

Start counting when init completed.

Definition at line 61 of file em_rtc.h.

Referenced by RTC_Init().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_rtc.h